请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM293 以下是所示的示例。
1. 由于邮资输入范围为0~3V、即使 OPA 第一级为24V、比较器 Vcc 仍可使用5V 吗?
2.如果比较器 Vcc 应为24V。 是否需要比较器的轨到轨输入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.