This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TL071H:TL071H:是否可以将40V 连接到 V+,将0V 连接到 V-?

Guru**** 2506985 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1282067/tl071h-tl071h-is-it-possible-to-connect-40v-to-v-and-0v-to-v-

器件型号:TL071H

我在查看 TL07xx 数据表、电源电压范围显示为±2.25V~±20V、4.5V~40V。 此时、是否可以将40V 连接到 V+、将0V 连接到 V-?