This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM2901:LM2901DR 输入电压信号相对于电源的关系

Guru**** 2510095 points
Other Parts Discussed in Thread: LM339LV

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1310106/lm2901-lm2901dr-input-voltage-signal-in-relation-to-power-supply

器件型号:LM2901
主题中讨论的其他器件:LM339LV

您好专家:

目前该项目计划将 LM2901DR 用作比较器、如果电源电压 VCC 提供单个+5V 电源、IN+是0.5V 基准电压的固定输入、 IN-是否为来自外部输入的电压信号、如果该电压信号高于5V (例如6V)、比较器是否能够正常工作? 如果输入电压为4.5V、是否可以正常使用? 谢谢。