This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA4170-Q1:电路

Guru**** 2782635 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1336552/opa4170-q1-circuit

器件型号:OPA4170-Q1

你(们)好。

我想设计一个具有单个输出引脚的运算放大器电路。

输入:-0V 至5V

输出范围:--10V 至+10V

 在0V 时、输入输出将是-10V、而5V 输入输出将是+10V