This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMP7704-SP:5962R1920601VXC -图纸容差问题

Guru**** 1456330 points
Other Parts Discussed in Thread: LMP7704-SP
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1351723/lmp7704-sp-5962r1920601vxc---tolerances-on-drawing-question

器件型号:LMP7704-SP

您好!

我目前正在使用器件5962R1920601VXC (或 LMP7704-SP)进行设计。

从数据表中可以看出、给定的尺寸为0.43mm MAX (从器件底部到引线)和25mm MAX (引线尖端到引线尖端)。

您的团队能否提供这些维度的最低价值观?

如果从 DLA 陆地和海事图纸中得到帮助、这些尺寸将会是"A1"和"E3"尺寸。

谢谢!