This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA4202:电容负载

Guru**** 2974170 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1450214/opa4202-capacitive-loads

器件型号:OPA4202

工具与软件:

您好!

我想设置下面的电路、其中输入是交流信号、幅值在40mV 到5V 之间、频率在30Hz 到3kHz 之间。

我想知道电容 C11和 C12是否我将它们更改为20uF、电路仍然会稳定?