This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM2432:使用 USB dfu-util 负载 FW 时、如何判断 AM243x MCU 是否转换了 HS-SE?

Guru**** 2595805 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1489883/am2432-when-using-usb-dfu-util-load-fw-how-to-tell-whether-the-am243x-mcu-is-hs-se-converted-or-not

器件型号:AM2432

工具与软件:

您好、TI 团队:  


在为 UART 引导模式用例使用 Keywriter 时、我们一直在利用 UART 控制台上报告的 SoC ID。 但当我们进入 USB 引导模式时、该信息将不再可用。  

是否有办法允许我们在 USB 引导模式下获得与 UART 引导模式情况类似的相同 SoC ID 输出?


谢谢!  
Hong

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    请参阅以下日志、了解如何通过 USB DFU 检索 SoC ID:

    ❯ dfu-util -a SocId -U socid.bin
    dfu-util 0.11
                                                                                                                                                                                            
    Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
    Copyright 2010-2021 Tormod Volden and Stefan Schmidt
    This program is Free Software and has ABSOLUTELY NO WARRANTY
    Please report bugs to sourceforge.net/.../
                                                                                                                                                                                            
    Opening DFU capable USB device...
    Device ID 0451:6165
    Device DFU version 0110
    Claiming USB DFU Interface...
    Setting Alternate Interface #1 ...
    Determining device status...
    DFU state(2) = dfuIDLE, status(0) = No error condition is present
    DFU mode device DFU version 0110
    Device returned transfer size 512
    Copying data from DFU device to PC
    Upload  [=========================] 100%          200 bytes
    Upload done.
    Received a total of 200 bytes
    ❯ xxd -c 1000 -p socid.bin > socid.txt
    ❯ python3 uart_boot_socid.py -d am64x -f socid.txt
    socid.txt
    -----------------------
    SoC ID Header Info:
    -----------------------
    NumBlocks            : 2
    -----------------------
    SoC ID Public ROM Info:
    -----------------------
    SubBlockId           : 1
    SubBlockSize         : 26
    DeviceName           : am64x
    DeviceType           : HSFS
    DMSC ROM Version     : [0, 2, 0, 0]
    R5 ROM Version       : [0, 2, 0, 0]
    -----------------------
    SoC ID Secure ROM Info:
    -----------------------
    Sec SubBlockId       : 2
    Sec SubBlockSize     : 166
    Sec Prime            : 0
    Sec Key Revision     : 0
    Sec Key Count        : 2
    Sec TI MPK Hash      : b018658ad99dc903c8c9bfb27b12751099920a042ad1dfea7b7ba57369f15546de285edde6a7b39a8bdc40a27b237f8fb1e57f245e80b929c1e28b024aa2ecc6
    Sec Cust MPK Hash    : ad0bc40b000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000
    Sec Unique ID        : 00d3ad583d3f6d57081296eee39054dae86e31c717b9049a204d4139e4ad69df

    此致、

    Prashant