This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSPM0G3507:无法使用 GPIO 将 MCU 从 standby0 唤醒至 run0。

Guru**** 2933630 points

Other Parts Discussed in Thread: SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1548923/mspm0g3507-unable-to-wakeup-mcu-from-standby0-to-run0-using-a-gpio

器件型号:MSPM0G3507
主题:SysConfig 中讨论的其他器件

工具/软件:

您好:

我想使用 GPIO 唤醒 MCU、 我已经配置了 GPIO PA12 对于中的唤醒功能 其中概述了 SysConfig 添加到工程。

/**
 * These arguments were used when this file was generated. They will be automatically applied on subsequent loads
 * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
 * @cliArgs --device "MSPM0G350X" --part "Default" --package "LQFP-64(PM)" --product "mspm0_sdk@2.05.01.01"
 * @v2CliArgs --device "MSPM0G3507" --package "LQFP-64(PM)" --product "mspm0_sdk@2.05.01.01"
 * @versions {"tool":"1.24.0+4110"}
 */

/**
 * Import the modules used in this configuration.
 */
const Board  = scripting.addModule("/ti/driverlib/Board");
const GPIO   = scripting.addModule("/ti/driverlib/GPIO", {}, false);
const GPIO1  = GPIO.addInstance();
const GPIO2  = GPIO.addInstance();
const RTC    = scripting.addModule("/ti/driverlib/RTC");
const SYSCTL = scripting.addModule("/ti/driverlib/SYSCTL");

/**
 * Write custom configuration values to the imported modules.
 */

GPIO1.$name                                 = "GPIO_LEDS";
GPIO1.associatedPins.create(2);
GPIO1.associatedPins[0].assignedPort        = "PORTA";
GPIO1.associatedPins[0].internalResistor    = "PULL_UP";
GPIO1.associatedPins[0].$name               = "USER_LED_1";
GPIO1.associatedPins[0].launchPadShortcut   = "LED1En";
GPIO1.associatedPins[1].assignedPort        = "PORTA";
GPIO1.associatedPins[1].assignedPortSegment = "Lower";
GPIO1.associatedPins[1].$name               = "USER_TEST";
GPIO1.associatedPins[1].internalResistor    = "PULL_UP";
GPIO1.associatedPins[1].pin.$assign         = "PA15";

GPIO2.$name                              = "WakeUp";
GPIO2.port                               = "PORTA";
GPIO2.portSegment                        = "Lower";
GPIO2.associatedPins[0].$name            = "PIN_0";
GPIO2.associatedPins[0].direction        = "INPUT";
GPIO2.associatedPins[0].interruptEn      = true;
GPIO2.associatedPins[0].internalResistor = "PULL_DOWN";
GPIO2.associatedPins[0].fastWakeEn       = true;
GPIO2.associatedPins[0].polarity         = "RISE";
GPIO2.associatedPins[0].pin.$assign      = "PA12";

RTC.intervalAlarmEvent = "HOURCHANGE";
RTC.calDOW             = "1";
RTC.calMin             = 32;
RTC.calHour            = 10;
RTC.calYear            = 2021;
RTC.calMonth           = "4";
RTC.calDOM             = 5;
RTC.calAlarm1Min       = 33;
RTC.calAlarm1Hour      = 10;
RTC.calAlarm1DOW       = "1";
RTC.calAlarm1DOM       = 5;
RTC.calSec             = 58;
RTC.enPerAlarm1        = true;
RTC.enabledInterrupts  = ["PRESCALER1"];

SYSCTL.validateClkStatus = true;
SYSCTL.clockTreeEn       = true;
SYSCTL.enableSleepOnExit = true;
SYSCTL.SYSOSC_Freq       = 4000000;
SYSCTL.powerPolicy       = "STANDBY0";

/**
 * Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
 * version of the tool will not impact the pinmux you originally saw.  These lines can be completely deleted in order to
 * re-solve from scratch.
 */
Board.peripheral.$suggestSolution            = "DEBUGSS";
Board.peripheral.swclkPin.$suggestSolution   = "PA20";
Board.peripheral.swdioPin.$suggestSolution   = "PA19";
GPIO1.associatedPins[0].pin.$suggestSolution = "PA0";
RTC.peripheral.$suggestSolution              = "RTC";


请告诉我执行上述操作所需的校正。



应届毕业生、

Abhijeet D.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、  

    让我从我这边来测试一下、稍后再回复你。

    此致、
    彼得

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    HII Peter

    确定。

    应届毕业生、

    Abhijeet D.