This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-MSPM0G3507:[MSPM0G3507] CAN 消息未被 MSMP0G3507 评估板确认

Guru**** 2966990 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1553380/lp-mspm0g3507-mspm0g3507-can-messages-are-not-acknowledged-by-msmp0g3507-evalboard

器件型号:LP-MSPM0G3507


工具/软件:

您好团队:

我面临的问题是、MSMP0G3507 评估板未接收/未确认 CAN Rx 消息。

我已确保 CAN 已初始化并启用中断、如下所示:

  /*初始化 CAN */
  SYSCFG_DL_MCAN0_init ();
  DL_MCAN_TXBufTransIntrEnable (MCAN0_INST、0U、1U);
  DL_MCAN_TXBufTransIntrEnable (MCAN0_INST、1U、1U);
我也将 CanTrcv 连接到电路板。
谢谢!
Prashanth.