This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1290NCPDT:如果 FMPRE0 为 0x00000000、则芯片在通过 SWD 接口连接后无法发送启用暂停的命令。

Guru**** 2556760 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1567533/tm4c1290ncpdt-if-fmpre0-is-0x00000000-the-chip-fails-to-send-the-halt-enabled-command-when-connected-via-the-swd-interface

器件型号:TM4C1290NCPDT


工具/软件:

 如果 FMPRE0 为 0x00000000、则当通过 SWD 接口连接时、芯片无法发送启用暂停的命令。