This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C123GH6PM:将程序下载到启动板时,它既不运行,也不调试

Guru**** 2766615 points

Other Parts Discussed in Thread: EK-TM4C123GXL

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1070649/tm4c123gh6pm-when-downloading-a-program-into-de-launchpad-it-does-not-run-nor-it-debugs

部件号:TM4C123GH6PM
“线程”中讨论的其它部件:EK-TM4C123GXL

你好  

我基本上是在尝试运行 CAN 总线示例,我已经验证了引脚是否正确,并且连接被设置为“Stellaris”。

当我尝试下载到启动板时,一切似乎都正常工作,我甚至得到了暂停和停止按钮,但似乎无法调试。

下面是我尝试运行的代码以及连接配置。 请大家提供反馈,我对 ARM 处理器领域有点陌生。

此外,我还在使用 CCS 11.1

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_can.h"
#include "driverlib/can.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/fpu.h"
#include "driverlib/can.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include <rom.h>
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "grlib/grlib.h"
#include "utils/uartstdio.h"
#include "driverlib/interrupt.h"
#include "inc/tm4c123gh6pm.h"

//Volatile variables
volatile uint32_t g_ui32RXMsgCount = 0;         //Counter for interrupts so no data gets lost
volatile uint32_t g_ui32TXMsgCount = 0;         //Counter for interrupts so no data gets lost
volatile bool g_bRXFlag = 0;                    //Flag to indicate data has been received
volatile uint32_t g_ui32ErrFlag = 0;            //Global variable to keep track of the error so they are processed

//CAN objects for data tx and rx
tCANMsgObject g_sCAN0RxMessage;
tCANMsgObject g_sCAN0TxMessage;

//Message identifiers and objects
//RXID is set to 0 so all messages are received
#define CAN0RXID                0
#define RXOBJECT                1
#define CAN0TXID                2
#define TXOBJECT                2

//Variables to hold characters being sent / received
uint8_t g_ui8TXMsgData;
uint8_t g_ui8RXMsgData;

//CAN 0 Interrupt handler. Checks for the cause of the interrupt, and mantains
//a count of all messages that have been transmitted/received
void CAN0IntHandler(void)
{
    uint32_t ui32Status;
    //Read the interrupt status to find the cause of the interrupt
    //CAN_INT_STS_CAUSE register values
    //0x0000        = No interrupt pending
    //0x0001-0x0020 = Number of message object that cause the interrupt
    //0x8000        = Status interrupt
    //all others numbers are reserved and have no meaning in this system

    //Read the interrupt cause
    ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);

    //If this was a status interrupt acknowledge it by reading the CAN
    //status register
    if(ui32Status == CAN_INT_INTID_STATUS)
    {
        //Read the controller status. This will return a field of status
        //error bits that can indicate various errors. Refer to the
        //API documentation for details about the error status bits.
        //Just by reading the status will clear the interrupt.
        ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);

        //Add ERROR flags to list of current errors. To be handled
        //later, because it would take too much time here in the interrupt.
        g_ui32ErrFlag |= ui32Status;
    }
    //Check if the cause is message object RXOBJECT, which we are using
    //to receive messages
    else if(ui32Status == RXOBJECT)
    {
        //Getting to this point means that the RX interrupt occurred
        //on message object RXOBJECT, and the message reception is complete.
        //Clear the message interrupt.
        CANIntClear(CAN0_BASE, RXOBJECT);
        //Increment a counter to keep track of how many messages have been
        //received. In real application this could be used to set flags to
        //indicate when a message is received
        g_ui32RXMsgCount++;
        //Set flag to indicate received message is pending
        g_bRXFlag = true;
        //Since a message was received, clear any error flags.
        //This is done because before the message is received it triggers
        //a Status interrupt for RX complete. By clearing the flag here
        //we prevent unnecessary error handling from happening
        g_ui32ErrFlag = 0;
    }
    //Check if the cause is message object TXOBJECT, which we are using
    //for transmitting messages
    else if(ui32Status == TXOBJECT)
    {
        //Getting to this point means that the TX interrupt occurred on
        //message object TXOBJECT, and the message reception is complete
        //Clear the message object interrupt.
        CANIntClear(CAN0_BASE, TXOBJECT);
        //Increment a counter to keep track of how many messages have been transmitted
        //In real applications this could be used to set flags to indicate when a message
        // is transmitted
        g_ui32TXMsgCount++;
        //Since a message was transmitted, clear any error flags.
        //This is done because before the message is transmitted it
        //triggers a Status interrupt for TX complete. By clearing the flag
        //here we prevent unnecessary error handling from happening
        g_ui32ErrFlag = 0;
    }
    else
    {
        //this code should never execute
        return;
    }
}

void ConfigureUART(void)
{
    //Enable the GPIO peripheral used by UART.
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    //Enable UART0
    SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    //Configure GPIO pins for UART mode
    GPIOPinConfigure(GPIO_PA0_U0RX);
    GPIOPinConfigure(GPIO_PA1_U0TX);
    GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    //Use internal 16MHz oscillator as the UART clock source
    UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    //Initialize the UART for console I/O
    UARTStdioConfig(0, 115200, SysCtlClockGet());
}

//Setup CAN0 to both send and receive at 500KHz
void InitCAN0(void)
{
    //For this example CAN0 is used with RX and TX on port E4 and E5
    //GPIO port E needs to be enabled so these pins can be used
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    //Configure the GPIO muxing to select CAN0 functions for these pins
    //this step selects which alternate function is available for these
    //pins
    GPIOPinConfigure(GPIO_PE4_CAN0RX);
    GPIOPinConfigure(GPIO_PE5_CAN0TX);
    //Enable the alternate function on the GPIO pins. The above step selects
    //which alternate function is available. This step actually enables
    //the alternate function instead of GPPIO for these pins
    GPIOPinTypeCAN(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    //The GPIO port and pins have been set up for CAN. THe CAN
    //peripheral must be enabled
    SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
    //Initialize CAN Controller
    CANInit(CAN0_BASE);
    //Setup the bit rate for the CAN Bus. This function sets up the
    //CAN bus timing for a nominal configuration. You can achieve
    //more control over the can bus timing by using the function
    //CANBitTimingSet() instead of this one, if needed.
    //For this example, the CAN bus is set to 500kHz
    CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
    //Enable interrupts on the CAN peripheral. This example uses
    //static allocation of interrupt handlers which means the name of
    //the handler is in the vector table of startup code
    CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    //Enable the CAN interrupt on the processor NVIC
    IntEnable(INT_CAN0);
    //Enable the CAN for operation
    CANEnable(CAN0_BASE);
    //Initialize a message object to be used for receiving CAN messages
    //with any CAN ID. In order to receive any CAN ID, the ID and mask
    //must be both set to 0, and the ID filter enabled
    g_sCAN0RxMessage.ui32MsgID = CAN0RXID;
    g_sCAN0RxMessage.ui32MsgIDMask = 0;
    g_sCAN0RxMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER;
    g_sCAN0RxMessage.ui32MsgLen = sizeof(g_ui8RXMsgData);
    //Now load the message object into the CAN peripheral. Once loaded
    //the CAN will receive any message on the bus, and an interrupt will occur.
    //Use message object RXOBJECT for receiving messages (this is not the
    //same as the CAN ID which can be any value in this example)
    CANMessageSet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, MSG_OBJ_TYPE_RX);
    //Initialize the message object that will be used for sending CAN
    //messages. The message will by 1 bytes that will contain the
    //character received from the other controller. Initially it will be set to 0
    g_ui8TXMsgData = 0;
    g_sCAN0TxMessage.ui32MsgID = CAN0TXID;
    g_sCAN0TxMessage.ui32MsgIDMask = 0;
    g_sCAN0TxMessage.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
    g_sCAN0TxMessage.ui32MsgLen = sizeof(g_ui8TXMsgData);
    g_sCAN0TxMessage.pui8MsgData = (uint8_t *)&g_ui8TXMsgData;
}

//CAN error handling. When a message a message is received if there is an error it is
//saved to g_ui32ErrFlag, the Error Flag set. Bellow the flags are checked
//and cleared. It is left up to the user to add handling functionality if
//so desired
void CANErrorHandler(void)
{
    //CAN controller has entered a Bus off state
    if(g_ui32ErrFlag & CAN_STATUS_BUS_OFF)
    {
        UARTprintf("ERROR: CAN STATUS BUS OFF\n");
        //clear CAN_STATUS_BUS_OFF Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_BUS_OFF);
    }
    //CAN controller error level has reached warning level
    if(g_ui32ErrFlag & CAN_STATUS_EWARN)
    {
        UARTprintf("ERROR: TOO MUCH ERRORS\n");
        //clear CAN_STATUS_EWARN Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_EWARN);
    }
    //CAN controller error level has reached error pasive level
    if(g_ui32ErrFlag & CAN_STATUS_EPASS)
    {
        //Clear CAN_STATUS_EPASS Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_EPASS);
    }
    //A message was received successfully since the last read of this status
    if(g_ui32ErrFlag & CAN_STATUS_RXOK)
    {
        //Clear CAN_STATUS_RXOK Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_RXOK);
    }
    // A message was transmitted successfully since the last read of this status
    if(g_ui32ErrFlag & CAN_STATUS_TXOK)
    {
        //Clear CAN_STATUS_TXOK Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_TXOK);
    }
    //This is the mask for the last error code field
    if(g_ui32ErrFlag & CAN_STATUS_LEC_MSK)
    {
        //Clear CAN_STATUS_LEC_MSK Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_MSK);
    }
    //A bit stuffing has occurred
    if(g_ui32ErrFlag & CAN_STATUS_LEC_STUFF)
    {
        //Clear CAN_STATUS_LEC_STUFF Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_STUFF);
    }
    //A formatting error has occurred
    if(g_ui32ErrFlag & CAN_STATUS_LEC_FORM)
    {
        //Clear CAN_STATUS_LEC_FORM Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_FORM);
    }
    //An acknowledge error has occurred
    if(g_ui32ErrFlag & CAN_STATUS_LEC_ACK)
    {
        //Clear CAN_STATUS_LEC_ACK Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_ACK);
    }
    //A bus remained a bit level of 1 for longer than is allowed
    if(g_ui32ErrFlag & CAN_STATUS_LEC_BIT1)
    {
        //Clear CAN_STATUS_LEC_BIT1 Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_BIT1);
    }
    //The bus remained a but level of 0 for longer than is allowed
    if(g_ui32ErrFlag & CAN_STATUS_LEC_BIT0)
    {
        //Clear CAN_STATUS_LEC_BIT0 Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_BIT0);
    }
    //A CRC error has occurred
    if(g_ui32ErrFlag & CAN_STATUS_LEC_CRC)
    {
        //Important error to handle
        //Clear CAN_STATUS_LEC_CRC Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_CRC);
    }
    //This is the mask for the CAN Last Error Code (LEC)
    if(g_ui32ErrFlag & CAN_STATUS_LEC_MASK)
    {
        //Clear CAN_STATUS_LEC_MASK Flag
        g_ui32ErrFlag &= ~(CAN_STATUS_LEC_MASK);
    }
    //At this point the error Flag container should be 0, make sure it is
    if(g_ui32ErrFlag !=0)
    {
        UARTprintf("Unhandled ERROR: %x \n",g_ui32ErrFlag);
        g_ui32ErrFlag &= 0x00;
    }
}

int main(void)
{
    volatile uint32_t ui32Loop;             //Declare dummy variable
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);

    while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOG))
    {
    }

    //GPIODirModeSet(GPIO_PORTF_BASE, 0x04, GPIO_DIR_MODE_OUT);
    GPIOPinTypeGPIOOutput(GPIO_PORTG_BASE, GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
    GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3, 1);

    //Enable lazy stacking for interrupts handlers. This allows floating-point
    //instructions to be used within interrupt handlers, but at the expense
    //of extra stack usage
    //FPULazyStackingEnable();
    //Set the clocking to run directly from the crystal
    SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);
    //SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL| SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);    //Set 80Mhz
    //SysCtlClockSet(SYSCTL_OSC_INT | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_320);
    //Initialize the UART
    ConfigureUART();
    //Initialize CAN0
    InitCAN0();
    while(1)
    {
        //If this condition is true this means the RX interrupt occurred
        //and there is a message ready to be read from the CAN
        if(g_bRXFlag)
        {
            //Reuse the same message object that was used earlier to configure the CAN
            //for receiving messages. A buffer for storing the received data must also
            //be provided, so set the buffer pointer within the message
            //object
            g_sCAN0RxMessage.pui8MsgData = (uint8_t *) &g_ui8RXMsgData;
            //Read the message from the CAN. Message object RXOBJECT is used
            //(which is not the same thing as CAN ID). The interrupt clearing
            //flag is not set because this interrupt was already cleared in the
            //interrupt handler
            CANMessageGet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, 0);
            //Clear the pending message flag so that the interrupt handler can
            //set it again when the next message arrives.
            g_bRXFlag = 0;
            //Check to see if there is an indication that some messages were lost
            if(g_sCAN0RxMessage.ui32Flags & MSG_OBJ_DATA_LOST)
            {
                UARTprintf("\nCAN message loss detected\n");
            }
            //print the received char to the UART Terminal
            //UARTprintf("%c", g_ui8RXMsgData);
        }
        else
        {
            //Error handling
            if(g_ui32ErrFlag != 0)
                CANErrorHandler();

            while(UARTCharsAvail(UART0_BASE))
            {
                // Read the next character from the UART terminal
                g_ui8TXMsgData = UARTCharGetNonBlocking(UART0_BASE);
                char txdata = g_ui8TXMsgData;
                UARTprintf("Sent data: ", txdata);
                // Send the CAN message using object number TXOBJECT (not the
                // same thing as CAN ID, which is also TXOBJECT in this
                // example).  This function will cause the message to be
                // transmitted right away
                CANMessageSet(CAN0_BASE, TXOBJECT, &g_sCAN0TxMessage, MSG_OBJ_TYPE_TX);
            }
            g_ui8TXMsgData = 0x33;
            CANMessageSet(CAN0_BASE, TXOBJECT, &g_sCAN0TxMessage, MSG_OBJ_TYPE_TX);

        }
    }

	return 0;
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

     看起来调试器尚未连接到目标。 请查看下面的屏幕截图。 它说它正在运行。 这意味着它没有连接。 您可以尝试两种方法。  

     1.单击调试按钮(以红色圆圈显示),它将构建您的项目并连接到目标。 连接后,您将调试代码。

     2.您可以右键单击 Stellaris 整周调试 InteFace_0 (在屏幕截图中以蓝色下划线表示),然后选择“连接目标”

     任何一种方式都将连接到目标。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    很抱歉耽误你的回答。

    我尝试右键单击并单击连接目标,我收到了此消息

    CORTEX_M4_0: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    

    我没有断点,仍然无法调试或连接到目标。

    尽管加载了程序,但我的程序根本没有执行。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

     为什么不从 C:\ti\TiaWare_C_Series-2.2.0.295\examples\boards\EK-tm4c123gxl\blingky 的简单盲项目开始。 这已经是一个完全构建的 CCS 项目。 如果尚未打开 CCS 并将此项目导入工作空间,请将其导入。 导入后,只需单击“闪烁”即可突出显示为活动项目。 您将看到[Active - Debugge](活动-调试)。 之后,您只需单击“调试”按钮。 它将构建项目(如果有任何文件已更新),连接到目标,您应该准备好运行和调试程序。 放置一些断点,看看是否可以调试这个简单的程序。  

    请参阅下面首先突出显示“闪烁”的部分,然后单击调试按钮。  

    另请参阅这些 CCS 培训视频。  

    https://training.ti.com/tiva-c-series-launchpad-workshop-chapter-02?context=1148217-1141458

    https://training.ti.com/getting-started-code-composer-studio-v7