请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
您好,
您是否知道 按钮擦除整个闪存后删除的步骤操作 IC,如下图所示?
谢谢

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您是否知道 按钮擦除整个闪存后删除的步骤操作 IC,如下图所示?
谢谢

工具团队确认了我的假设。 “擦除整个闪存”按钮将生成 DPActiveDebugSession.Expression.Evaluate ("MassEras()") ,其执行方式如下:
hotmenu MassErase()
{
GEL_TextOut("Initializing.\n", "MassErase()");
_isMassErase = 1;
// Disconnect from target. This must be done for each module in the device debug sub-system hierarchy.
DisconnectIfConnected(); // Cortex
GEL_EvalOnTarget("<parent>", "DisconnectIfConnected()", 1); // DAP (Cortex' parent)
GEL_EvalOnTarget("<parent>", "GEL_EvalOnTarget(\"<parent>\",\"DisconnectIfConnected()\", 1)", 1); // Icepick (DAP's parent)
// Do board reset
GEL_TextOut("Issuing Board Reset.\n", "MassErase()");
GEL_AdvancedReset("Board Reset");
// Reconnect to Icepick
GEL_EvalOnTarget("<parent>", "GEL_EvalOnTarget(\"<parent>\",\"ConnectIfDisconnected()\", 1)", 1);
// Issue mass erase from Icepick and disconnect
GEL_EvalOnTarget("<parent>", "GEL_EvalOnTarget(\"<parent>\",\"IP_CC26xx_CHIPERASE = 1\", 1)", 1);
GEL_EvalOnTarget("<parent>", "GEL_EvalOnTarget(\"<parent>\",\"DisconnectIfConnected()\", 1)", 1);
// Workaround on engineering devices. Disconnect and reconnect for chip erase to take effect.
ConnectIfDisconnected();
DisconnectIfConnected();
_isMassErase = 0;
GEL_TextOut("Mass erase complete.\n", "MassErase()");
}
IP_CC26xx_CHIPERASE 寄存器是由 XDS 驱动程序定义的虚拟寄存器,向其写入1将导致 WUC TAP 中的 XDS 探测器设置 CHICE_ERAK_REQ。
此致,
瑞安