This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS570LS3137:MCU 自行重置

Guru**** 2964200 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1079041/tms570ls3137-mcu-resets-himself

部件号:TMS570LS3137

您好,

我想将我的项目配置为在闪存的第0列气缸组中有一个“备份主程序”和“引导加载程序”,在闪存的第1列气缸组中有一个可更新的主程序。 但是,尝试实施时,MCU 会在每次执行 RTI 中断时自行重置。 我附上下面的 bl_link.cmd 代码。

/* Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/
 *
 *
 *  Redistribution and use in source and binary forms, with or without
 *  modification, are permitted provided that the following conditions
 *  are met:
 *
 *    Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 *    Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the
 *    distribution.
 *
 *    Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*                                                                            */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN (0) */
/* USER CODE END */


/*----------------------------------------------------------------------------*/
/* Linker Settings                                                            */
--retain="*(.intvecs)"

/* USER CODE BEGIN (1) */

/* USER CODE END */

/*----------------------------------------------------------------------------*/
/* Memory Map                                                                 */

MEMORY
{

    VECTORS (X)  : origin=0x00000000 length=0x00000020
    FLASH0  (RX) : origin=0x00000020 length=0x0017FFE0
    FLASH1  (RX) : origin=0x00180000 length=0x07E82000
    SRAM  (RW) : origin=0x08002000 length=0x00002000
    STACK   (RW) : origin=0x08004000 length=0x00002000


//    VECTORS    (X)   : origin=0x00000000 length=0x00000020    vfill = 0xffffffff
//    FLASH0     (RX)  : origin=0x00000020 length=0x00010000    vfill = 0xffffffff
//    FLASH1     (RX)  : origin=0x00010020 length=0x07FF1FE0    vfill = 0xffffffff
//    SRAM       (RWX)  : origin=0x08002000 length=0x00002000
//    STACK      (RW)  : origin=0x08004000 length=0x00002000

/* USER CODE BEGIN (2) */
#if 1
    ECC_VEC  (R) : origin=(0xf0400000 + (start(VECTORS) >> 3))
                   length=(size(VECTORS) >> 3)
                   ECC={algorithm=algoL2R5F021, input_range=VECTORS}

    ECC_FLA0 (R) : origin=(0xf0400000 + (start(FLASH0)  >> 3))
                   length=(size(FLASH0)  >> 3)
                   ECC={algorithm=algoL2R5F021, input_range=FLASH0 }

    ECC_FLA1 (R) : origin=(0xf0400000 + (start(FLASH1)  >> 3))
                   length=(size(FLASH1)  >> 3)
                   ECC={algorithm=algoL2R5F021, input_range=FLASH1 }
#endif
/* USER CODE END */

}

/* USER CODE BEGIN (3) */
ECC
{
    algoL2R5F021 : address_mask = 0xfffffff8 /* Address Bits 31:3 */
                   hamming_mask = R4         /* Use R4/R5 build in Mask */
                   parity_mask  = 0x0c       /* Set which ECC bits are Even and Odd parity */
                   mirroring    = F021       /* RM57Lx and TMS570LCx are build in F021 */
}
/* USER CODE END */


/*----------------------------------------------------------------------------*/
/* Section Configuration                                                      */

SECTIONS
{
   .intvecs : {} > VECTORS


   flashAPI:
   {
     .\source\Fapi_UserDefinedFunctions.obj (.text)
     .\source\bl_flash.obj (.text)
     //--library= "c:\ti\Hercules\F021 Flash API\02.01.01\F021_API_CortexR4_BE_V3D16.lib"  (.text)
     --library="F021_API_CortexR4_BE_V3D16.lib"  (.text)
   } palign=8 load = FLASH0, run = SRAM, LOAD_START(apiLoadStart), RUN_START(apiRunStart), SIZE(apiLoadSize)

   .text  : {} > FLASH0 /*Initialized executable code and constants*/
   .const : {} load=FLASH0 , run = SRAM, LOAD_START(constLoadStart), RUN_START(constRunStart), SIZE(constLoadSize)

//  ; .cinit : {} > FLASH0 /*Initialized global and static variables*/
// ;  .pinit : {} > FLASH0
// ;  .data  : {} > SRAM
//  ; .bss   : {} > SRAM   /*Uninitialized Global and static variables */
//  ; .sysmem  : {} > SRAM


//  ;  .intvecs : {} > VECTORS
//   ; .text    : {} > FLASH0 | FLASH1
//    ;.const   : {} > FLASH0 | FLASH1

    .cinit   : {} > FLASH0
    .pinit   : {} > FLASH0
    .bss     : {} > SRAM
    .data    : {} > SRAM
	.sysmem  : {} > SRAM
/* USER CODE BEGIN (4) */
/* USER CODE END */
}

/* USER CODE BEGIN (5) */
/* USER CODE END */


/*----------------------------------------------------------------------------*/
/* Misc                                                                       */

/* USER CODE BEGIN (6) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/

谢谢,此致,

莱安德罗

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好, 莱安德罗,

    很抱歉,我不能完全理解您的问题。 是否要将应用程序的引导加载程序和 main()编程到闪存库0和闪存库1,后者是闪存库0中代码的备份?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    QJ 您好,

    很抱歉,也许我解释错误。  我们希望使用引导加载程序和无法更新的 main()程序(备份)的第一个版本来刷新 bank 0。 另一方面,通过 CAN 接口,我们希望使用 bootloader 刷新带有 main()更新版本的气缸组1。  

    Bank 0:bootloader + Backup main()(无法通过 CAN 更新)

    第1列气缸组:可更新的 main() (可通过 CAN 更新)

    谢谢,此致,

    莱安德罗

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    QJ 您好,

    我们发现了一些可能对解决此问题很重要的东西。

    /*----------------------------------------------------------------------------*/
    /* Linker Settings                                                            */
    --retain="*(.intvecs)"
    
    /*----------------------------------------------------------------------------*/
    /* Memory Map                                                                 */
    
    MEMORY
    {
        VECTORS    (X)   : origin=0x00000000 length=0x00000020    vfill = 0xffffffff
        FLASH0     (RX)  : origin=0x00000020 length=0x00010000    vfill = 0xffffffff
        FLASH1     (RX)  : origin=0x00010020 length=0x07FF1FE0    vfill = 0xffffffff
        SRAM       (RWX)  : origin=0x08002000 length=0x00002000
        STACK      (RW)  : origin=0x08004000 length=0x00002000
    
    #if 1
        ECC_VEC  (R) : origin=(0xf0400000 + (start(VECTORS) >> 3))
                       length=(size(VECTORS) >> 3)
                       ECC={algorithm=algoL2R5F021, input_range=VECTORS}
    
        ECC_FLA0 (R) : origin=(0xf0400000 + (start(FLASH0)  >> 3))
                       length=(size(FLASH0)  >> 3)
                       ECC={algorithm=algoL2R5F021, input_range=FLASH0 }
    
        ECC_FLA1 (R) : origin=(0xf0400000 + (start(FLASH1)  >> 3))
                       length=(size(FLASH1)  >> 3)
                       ECC={algorithm=algoL2R5F021, input_range=FLASH1 }
    #endif
    
    ECC
    {
        algoL2R5F021 : address_mask = 0xfffffff8 /* Address Bits 31:3 */
                       hamming_mask = R4         /* Use R4/R5 build in Mask */
                       parity_mask  = 0x0c       /* Set which ECC bits are Even and Odd parity */
                       mirroring    = F021       /* RM57Lx and TMS570LCx are build in F021 */
    }
    
    /* Section Configuration */
    
    SECTIONS
    {
       .intvecs : {} > VECTORS
    
       flashAPI:
       {
         .\source\Fapi_UserDefinedFunctions.obj (.text)
         .\source\bl_flash.obj (.text)
         //--library= "c:\ti\Hercules\F021 Flash API\02.01.01\F021_API_CortexR4_BE_V3D16.lib"  (.text)
         --library="F021_API_CortexR4_BE_V3D16.lib"  (.text)
       } palign=8 load = FLASH0, run = SRAM, LOAD_START(apiLoadStart), RUN_START(apiRunStart), SIZE(apiLoadSize)
    
       .text  : {} > FLASH0 /*Initialized executable code and constants*/
       //.const : {} load=FLASH0, run = SRAM, LOAD_START(constLoadStart), RUN_START(constRunStart), SIZE(constLoadSize)
    
    	.const : {} > FLASH0
        .cinit   : {} > FLASH0
        .pinit   : {} > FLASH0
        .bss     : {} > SRAM
        .data    : {} > SRAM
    	.sysmem  : {} > SRAM
    }
    

    我们评论了以下几行:

    .const : {} load=FLASH0, run = SRAM, LOAD_START(constLoadStart), RUN_START(constRunStart), SIZE(constLoadSize)

    而且设备不会自行重置。 这可能是 RTI 的问题吗?

    谢谢,此致,

    莱安德罗

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好, 莱安德罗,

    由于 要擦除和编程的闪存扇区位于第1列气缸组,因此您不必从 SRAM 执行闪存 API。  

    const:{} load=FLASH0, run = SRAM,load_start(connstLoadStart),run_start(connstRunStart),size(connstLoadSize)--> 将 const (闪存扇区定义)复制到 SRAM。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    QJ 您好,

    非常感谢您的回复。 我们将尝试使用此配置。 我们会告诉您它是否运行良好。

    此致,

    莱安德罗