This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C129XNCZAD:TM4C129XNCZAD 入门

Guru**** 2542740 points
Other Parts Discussed in Thread: TM4C129XNCZAD, EK-TM4C1294XL

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1081896/tm4c129xnczad-getting-started-with-tm4c129xnczad

部件号:TM4C129XNCZAD
“线程”中讨论的其它部件: EK-TM4C1294XL

大家好,我只是从 TM4C129XNCZAD 开始,我尝试将一个端口引脚闪烁一秒钟以开始,有谁能引导我这样做,谁能给我提供代码以开始。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Nagaraj,

     如果您尚未下载 TivaWare,请从 https://www.ti.com/tool/SW-TM4C 下载 TivaWare。 TiaWare 是一款软件开发套件(SDK), 它提供了工程师评估和开发 TM4C 设备系列应用所需的所有组件。 下载 SDK 后,您可以在 C:\ti\TivaWare_C_Series-2.2.0.295\Examples\boards\EK-tm4c1294xl 下找到许多示例。 您可以从“闪烁”,“投影0”和“您好”示例开始。 一个盲目的例子可以很简单,如下所示。  

    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_memmap.h"
    #include "driverlib/debug.h"
    #include "driverlib/gpio.h"
    #include "driverlib/sysctl.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>Blinky (blinky)</h1>
    //!
    //! A very simple example that blinks the on-board LED using direct register
    //! access.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
        while(1);
    }
    #endif
    
    //*****************************************************************************
    //
    // Blink the on-board LED.
    //
    //*****************************************************************************
    int
    main(void)
    {
        volatile uint32_t ui32Loop;
    
        //
        // Enable the GPIO port that is used for the on-board LED.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
    
        //
        // Check if the peripheral access is enabled.
        //
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPION))
        {
        }
    
        //
        // Enable the GPIO pin for the LED (PN0).  Set the direction as output, and
        // enable the GPIO pin for digital function.
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
    
        //
        // Loop forever.
        //
        while(1)
        {
            //
            // Turn on the LED.
            //
            GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
    
            //
            // Delay for a bit.
            //
            for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
            {
            }
    
            //
            // Turn off the LED.
            //
            GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0x0);
    
            //
            // Delay for a bit.
            //
            for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
            {
            }
        }
    }

    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_types.h"
    #include "inc/hw_memmap.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/gpio.h"
    
    //*****************************************************************************
    //
    // Define pin to LED mapping.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>Project Zero (project0)</h1>
    //!
    //! This example demonstrates the use of TivaWare to setup the clocks and
    //! toggle GPIO pins to make the LED blink. This is a good place to start
    //! understanding your launchpad and the tools that can be used to program it.
    //
    //*****************************************************************************
    
    #define USER_LED1  GPIO_PIN_0
    #define USER_LED2  GPIO_PIN_1
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // Main 'C' Language entry point.  Toggle an LED using TivaWare.
    //
    //*****************************************************************************
    int
    main(void)
    {
        uint32_t ui32SysClock;
    
        //
        // Run from the PLL at 120 MHz.
        // Note: SYSCTL_CFG_VCO_240 is a new setting provided in TivaWare 2.2.x and
        // later to better reflect the actual VCO speed due to SYSCTL#22.
        //
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                           SYSCTL_OSC_MAIN |
                                           SYSCTL_USE_PLL |
                                           SYSCTL_CFG_VCO_240), 120000000);
    
        //
        // Enable and wait for the port to be ready for access
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPION))
        {
        }
        
        //
        // Configure the GPIO port for the LED operation.
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, (USER_LED1|USER_LED2));
    
        //
        // Loop Forever
        //
        while(1)
        {
            //
            // Turn on the LED
            //
            GPIOPinWrite(GPIO_PORTN_BASE, (USER_LED1|USER_LED2), USER_LED1);
    
            //
            // Delay for a bit
            //
            SysCtlDelay(ui32SysClock/6);
    
            //
            // Turn on the LED
            //
            GPIOPinWrite(GPIO_PORTN_BASE, (USER_LED1|USER_LED2), USER_LED2);
    
            //
            // Delay for a bit
            //
            SysCtlDelay(ui32SysClock/6);
        }
    }

      

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢查尔斯的支持我正在尝试打开端口针脚高度,但端口针脚高度不高,请帮我解决这个问题。我在邮件中附上了我的代码片段

    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_memmap.h"
    #include "driverlib/debug.h"
    #include "driverlib/gpio.h"
    #include "driverlib/sysctl.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>Blinky (blinky)</h1>
    //!
    //! A very simple example that blinks the on-board LED using direct register
    //! access.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
        while(1);
    }
    #endif
    
    //*****************************************************************************
    //
    // Blink the on-board LED.
    //
    //*****************************************************************************
    int
    main(void)
    {
        volatile uint32_t ui32Loop;
    
        //
        // Enable the GPIO port that is used for the on-board LED.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
    
        //
        // Check if the peripheral access is enabled.
        //
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPION))
        {
        }
    
        //
        // Enable the GPIO pin for the LED (PN0).  Set the direction as output, and
        // enable the GPIO pin for digital function.
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_4);
        GPIOPinTypeGPIOOutput(GPIO_PORTE_BASE, GPIO_PIN_6);
    
        //
        // Loop forever.
        //
        while(1)
        {
            //
            // Turn on the LED.
            //
            GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, GPIO_PIN_4);
            GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_6, GPIO_PIN_6);
    
    
        }
    }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

     如果要打开连接到 PF4或 PE6的 LED 指示灯,则需要先启用这两个端口。 目前您仅启用 PN。 如果您尝试访问未首先启用的 portF 和 Porte,则会中止。 您需要添加以下代码。  

    //
    //启用用于板载 LED 的 GPIO 端口。
    //
    SysPeripheralEnable (sysctl_Periph_GPIOF);

    SysPeripheralEnable (sysctl_Periph_GPIOE);

    //
    //检查是否启用了外围设备访问。
    //
    While (!SystlPeripheralReady (sysctl_Periph_GPIOF))

    }

    While (!SystlPeripheralReady (sysctl_Periph_GPIOE))

    }

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢查尔斯,我现在指示灯闪烁了,我附上了我的代码片段以供参考,谢谢。  

    int main(void)
    {
        volatile uint32_t ui32Loop;
    
        //
        // Enable the GPIO port that is used for the on-board LED.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
    
        //
        // Check if the peripheral access is enabled.
        //
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPION))
        {
        }
    
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    
    
    
        //
        // Check if the peripheral access is enabled.
        //
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOF))
        {
        }
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE))
        {
        }
    
        //
        // Enable the GPIO pin for the LED (PN0).  Set the direction as output, and
        // enable the GPIO pin for digital function.
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_4);
        GPIOPinTypeGPIOOutput(GPIO_PORTE_BASE, GPIO_PIN_6);
    
        //
        // Loop forever.
        //
        while(1)
        {
            //
            // Turn on the LED.
            //
            GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, GPIO_PIN_4);
            GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_6, GPIO_PIN_6);
    
    
            //
            // Delay for a bit.
            //
            for(ui32Loop = 0; ui32Loop < 2000000; ui32Loop++)
            {
            }
    
            //
            // Turn off the LED.
            //
            GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, 0x0);
    
            //
            // Delay for a bit.
            //
            for(ui32Loop = 0; ui32Loop < 2000000; ui32Loop++)
            {
            }
        }
    
    	return 0;
    }