This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SW-EK-LM4F120XL:I2C配置功能

Guru**** 670100 points
Other Parts Discussed in Thread: EK-TM4C123GXL
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1098490/sw-ek-lm4f120xl-i2c-configuration-function

部件号:SW-EK-LM4F120XL
主题中讨论的其他部件:EK-LM4F120XLTM4C123EK-TM4C123GXL

我已经设置了一个功能,以便配置LM4F120H5QR微控制器与外部传感器(HMC5883L)之间的I2C通信。

我使用了lm4f120h5qr.h中的寄存器定义

它看起来是否正常?

文件:///C/Users/Peter/Documents/Afgangsprojet/EK-LM4F120XL_Launchpad/lm4f120h5qr.h

void I2C_Config(void)
{
    SYSCTL_RCGCI2C_R |= SYSCTL_RCGCI2C_R0; // Set bit 0/R0 in the Inter-Integrated Circuit Run Mode Clock Gating Control (RCGCI2C) register,
    //in order to enable and provide a clock to I2C module 0 in Run mode.

    SYSCTL_RCGCGPIO_R |= SYSCTL_RCGCGPIO_R1; // Set bit 1/R1 to enable and provide a clock to GPIO Port B in Run mode,
    //in the General-Purpose Input/Output Run Mode Clock Gating Control (RCGCGPIO) register.

    GPIO_PORTB_AHB_AFSEL_R |= 0xC; // Set PB2 & PB3 to enable the appropriate pins for their alternate function,
    //in the GPIO Alternate Function Select (GPIOAFSEL) register.

    GPIO_PORTB_AHB_ODR_R |= 0x8; // Set PB3 (I2C0SDA) for open-drain operation,
    //in the GPIO Open Drain Select (GPIOODR) register.

    GPIO_PORTB_AHB_PCTL_R |= 0x00003300; // Set the bit field PMC0 to 0011 in the GPIO Port Control (GPIOPCTL) register, in order to enable the
    //appropriate pins for their alternate function.

    I2C0_MASTER_MCR_R = 0x00000010; // Initialize the I2C Master by writing the I2C Master Configuration (I2CMCR) register with a value of 0x0000.0010.

    I2C0_MASTER_MTPR_R = 0x00000027; // Set the desired SCL clock speed by writing the I2C Master Timer Period (I2CMTPR) register with the equation:
    //TPR = (System Clock/(2*(SCL_LP + SCL_HP)*SCL_CLK))-1
    //SCL_LP & SCL_HP are fixed at 6 & 4 respectively, SCL_CLK is the desired clock speed of the I2C clock(100 Kbps, 400 Kbps & 1 Mbps)
    //and TPR is the Timer Period register value (range of 1 to 127).
}