This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM2634:AM2634:下载应用程序映像*appimage大小问题与UART uniflash

Guru**** 2589280 points
Other Parts Discussed in Thread: UNIFLASH

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1100577/am2634-am2634-downloading-application-image-appimage-size-issue-with-uart-uniflash

部件号:AM2634
主题中讨论的其他部分:UNIFLAASH

大家好

我们尝试通过8.2 SDK在客户主板上使用UART0进行uniflash

AM263x MCU+ SDK:闪存工具(TI.com)

我们可以 通过python UART_uniflaslash.py成功下载*.appimage (21.0772万字节),

>python uart_uniflash.py -p COM28 --cfg=default_sbl_qspi.cfg

Parsing config file ...
Parsing config file ... SUCCESS. Found 3 command(s) !!!

Executing command 1 of 3 ...
Found flash writer ... sending sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
Sent flashwriter sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage of size 49534 bytes in 7.06s.

Executing command 2 of 3 ...
Command arguments : --file=../../am263x_zcu_sbl/Debug/am263x_zcu_sbl.tiimage --operation=flash --flash-offset=0x0
Sent ../../am263x_zcu_sbl/Debug/am263x_zcu_sbl.tiimage of size 124942 bytes in 15.17s.
[STATUS] SUCCESS !!!

Executing command 3 of 3 ...
Command arguments : --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000
Sent ../../am263x_zcu/Release/am263x_zcu.appimage of size 210772 bytes in 22.64s.
[STATUS] SUCCESS !!!

All commands from config file are executed !!!

我们无法完成 python UART_uniflaslash.py的*.appimage (75.6319万字节)下载,

C:\GIT_HH\TI_AM263x_new\evw\tools\boot>python uart_uniflash.py -p COM28 --cfg=C:\GIT_HH\TI_AM263x_new\evw\tools\boot\sbl_prebuilt\am263x-cc\default_sbl_qspi_zcu.cfg

Parsing config file ...
Parsing config file ... SUCCESS. Found 3 command(s) !!!

Executing command 1 of 3 ...
Found flash writer ... sending sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
Sent flashwriter sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage of size 49534 bytes in 7.69s.

Executing command 2 of 3 ...
Command arguments : --file=sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
Sent sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage of size 56206 bytes in 8.65s.
[STATUS] SUCCESS !!!

Executing command 3 of 3 ...
Command arguments : --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000
Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 756317bytes [01:13, 10725.90bytes/s]recv error: getc timeout in start sequence
Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 756319bytes [01:25, 10725.90bytes/s]expected sequence 2, got (seq1=1, seq2=1), receiving next block, will NAK.
recv error: purge, requesting retransmission (NAK)
Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 756319bytes [01:30, 10725.90bytes/s]
[ERROR] XMODEM recv failed, no response OR incorrect response from EVM OR cancelled by user,
        Power cycle EVM and run this script again !!!

 对uniflash *。appiamge有任何大小限制?
请帮助我们解决此问题

巴西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jay:  

    请核实您的陈述。 我认为可能会出现打字错误,让我觉得事情不清楚:  

    [quote.userid="48.7798万" url="~/support/micromicrosofters/arm-based micromicromicromicrosofters-group/arm-based micromicromicromicromicromicromicromicrosofters/110.0577万/am2634-am2634-am2634-download-application-image-appimage-size-issue-issue-with -UART-unifart-group-unifth-un-un-group-un-bie-lash2634 -UART-unifart-group-unifth-un-un-group-un-bie-lash ;2634;我们2634我们可以下载*.77pybleas/pybleas/micromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicromicrosoft/ps/f-d/~下载*.77py/ be-f-f-f-f-f-f-f-f-f-f-d/ byte-f-d/ byte-f-d/ byte-f-download-f-lash基于pybe-f-f-f  

    是否只是appimage字节大小差异似乎存在问题?  您可以通过闪存写入程序使用的两个cfg文件发送吗?  

    谢谢!

    -Randy

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jay:

    我听说1 MB 有应用程序图像大小限制,但756 KB 远未达到。 您可以尝试以下两种方法:

    1.更换UART的USB电缆(PC到J26),然后重试。

    2.使用SBL_JTAG_uniflash将应用程序映像写入QSPI闪存的0x8万。 如果这起作用,则问题在于UART通信。

    此致,

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Randy

    cfg文件相同

    #-----------------------------------------------------------------------------#
    #                                                                             #
    #      DEFAULT CONFIGURATION FILE TO BE USED WITH THE FLASHWRITER SCRIPT      # 
    #                                                                             #
    #-----------------------------------------------------------------------------#
    #
    # By default this config file, 
    # - points to pre-built flash writer, bootloader for this EVM
    # - The application image points to relative path of the ipc echo application image for this EVM
    #   - Make sure this application is built before running this script
    # - You can customized this config file to point to your own bootloader and/or application images
    # - You can use --operation=flashverify if you just want to verify the flash contents and not flash the file.
    #
    
    # First point to sbl_uart_uniflash binary, which function's as a server to flash one or more files
    --flash-writer=sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
    
    # Now send one or more files to flash or flashverify as needed. The order of sending files does not matter
    
    # When sending bootloader make sure to flash at offset 0x0. ROM expects bootloader at offset 0x0
    --file=sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
    
    # When sending application image, make sure to flash at offset 0x80000 (default) or to whatever offset your bootloader is configured for
    #--file=../../am263x_zcu/Debug/am263x_zcu.appimage --operation=flash --flash-offset=0x80000
    --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000

    只是appimage字节大小差异似乎是个问题

    我们尝试在同一个项目中创建不同大小的应用程序  

    (1)发送大小为62.7796万字节的*。appimage,单位为61.79秒。
    [status]成功!!!

    Parsing config file ...
    Parsing config file ... SUCCESS. Found 3 command(s) !!!
    
    Executing command 1 of 3 ...
    Found flash writer ... sending sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
    Sent flashwriter sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage of size 49534 bytes in 5.65s.
    
    Executing command 2 of 3 ...
    Command arguments : --file=sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
    Sent sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage of size 56206 bytes in 8.66s.
    [STATUS] SUCCESS !!!
    
    Executing command 3 of 3 ...
    Command arguments : --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000
    Sent ../../am263x_zcu/Release/am263x_zcu.appimage of size 627796 bytes in 61.79s.
    [STATUS] SUCCESS !!!
    
    All commands from config file are executed !!!

    (2)正在发送../../am263x_zcu/Release/am263x_zcu.appimage:63.9011万字节[01:0210727.11字节/s]recv错误:启动序列中的getc超时

    Parsing config file ...
    Parsing config file ... SUCCESS. Found 3 command(s) !!!
    
    Executing command 1 of 3 ...
    Found flash writer ... sending sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
    Sent flashwriter sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage of size 49534 bytes in 5.09s.
    
    Executing command 2 of 3 ...
    Command arguments : --file=sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
    Sent sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage of size 56206 bytes in 8.66s.
    [STATUS] SUCCESS !!!
    
    Executing command 3 of 3 ...
    Command arguments : --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000
    Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 639011bytes [01:02, 10727.11bytes/s]recv error: getc timeout in start sequence
    Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 639013bytes [01:12, 10727.11bytes/s]expected sequence 2, got (seq1=1, seq2=1), receiving next block, will NAK.
    recv error: purge, requesting retransmission (NAK)
    Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 639013bytes [01:12, 10727.11bytes/s]
    [ERROR] XMODEM recv failed, no response OR incorrect response from EVM OR cancelled by user,
            Power cycle EVM and run this script again !!!

    巴西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好Ming

    1.我们用于UART连接UART0的USB电缆, UART (PC到J26)的含义是什么?

    UART2634 -UART-unif589/4077589#4077589]UART (2634 (引述407.7589万引述J26407.7589万J26)

    2.2634 /4077589#4077589"]2.</s>2634 407.7589万407.7589万使用SBL_JTAG_uniflash将应用程序映像写入QSPI闪存的0x8万。 如果此操作有效,则问题在于UART通信。[/QUOT]

    2.我们尝试使用SBL_JTAG_uniflash将应用程序映像写入QSPI闪存的0x8万。 验证闪存中的文件是否验证成功!!

    但是我们重新启动主板时QSPI启动失败,UART日志输出什么都没有

    如何通过SBL_JTAG_uniflash刷新SBL图像和*appimage?  

    [Cortex_R5_0]  
     
     ==================
     JTAG Uniflash Menu
     ==================
     
     1: Erase Complete Flash
     2: Write File to Flash and Verify
     3: Verify file in Flash
     
     x: Exit
     
     Enter Choice: 2
    
     Enter file name along with path to write or verify : C:\GIT_HH\TI_AM263x_new\evw\am263x_zcu\Release\am263x_zcu.appimage
     Enter flash offset (in hex format) : 0x80000
     Enter below command in CCS scripting console to load the file data to memory.
     AFTER the file load is done, enter '1' to continue ...
    
     loadRaw(0x70040020, 0, "C:/GIT_HH/TI_AM263x_new/evw/am263x_zcu/Release/am263x_zcu.appimage", 32, false);
    1
     [FLASH WRITER] Flashing success!!... 
     
     
     ==================
     JTAG Uniflash Menu
     ==================
     
     1: Erase Complete Flash
     2: Write File to Flash and Verify
     3: Verify file in Flash
     
     x: Exit
     
     Enter Choice: 3
    
     Enter file name along with path to write or verify : C:\GIT_HH\TI_AM263x_new\evw\am263x_zcu\Release\am263x_zcu.appimage
     Enter flash offset (in hex format) : 0x80000
     Enter below command in CCS scripting console to load the file data to memory.
     AFTER the file load is done, enter '1' to continue ...
    
     loadRaw(0x70040020, 0, "C:/GIT_HH/TI_AM263x_new/evw/am263x_zcu/Release/am263x_zcu.appimage", 32, false);
    1
     [FLASH WRITER] Verifying success!!... 
     
     
     ==================
     JTAG Uniflash Menu
     ==================
     
     1: Erase Complete Flash
     2: Write File to Flash and Verify
     3: Verify file in Flash
     
     x: Exit
     

    巴西

    [/quote]
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jay:

    对不起,我混合了AM263x CC和AM243x EVM。 正确,JTAG和UART使用相同的USB电缆用于AM263x CC。 请忽略我在上一篇文章中关于USB电缆的描述。

    为了编写SBL QSPI和应用程序图像,您需要调用SBL_JTAG_uniflash两次。 第一次执行整个闪存擦除,并在闪存地址0x0万处写入SBL_QSPI,然后第二次,不要擦除闪存,只需在闪存中写入0x8万处的应用程序映像。  

    在这两个运行中,请确保在输入"1"以继续之前使用CCS脚本(loadRaw)加载SBL_QSPI和应用程序映像。

    此致,

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好Ming

    我们尝试编写SBL QSPI和应用程序映像,将SBL_JTAG_uniflash调用两次, QSPI引导成功。

    (1)加载原始 appimage时,在脚本控制台中显示1万毫秒后超时,但正在验证成功!!!...

    (2) SBL_JTAG_UNIFLAASH *应用图像(75.6319万byte)正常,SBL_UART_UNIFLAASH有什么问题?

    2.2634 /4077589#4077589"]2.</s>2634 407.7589万407.7589万使用SBL_JTAG_uniflash将应用程序映像写入QSPI闪存的0x8万。 如果此操作有效,则问题在于UART通信。[/QUOT]

    巴西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jay:

    它与SBL_JTAG_uniflash无关,是CCS加载应用程序图像错误。 您的板载XDS-110设置似乎有一些问题。 请检查您的目标配置文件(CCXML)中的“JTAG TCLK频率”。 我的外观如下(1MHz):

    我在加载大应用程序图像文件时没有问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好Ming

    2634 -UART-unifXds/4079452#4079452"]在2634在主2634主板407.9452万板上407.9452万上的一些设置似乎有问题。 请检查您的目标配置文件(CCXML)中的“JTAG TCLK频率”。 我的外观如下(1MHz):[/QUOT]

    我们使用XDS200连接AM263X目标 ,目标配置文件(CCXML),如下所示  

     并且可以加载SBL_UART_JTAG.OUT程序,如下所示

    [quote userid="1.5702万" url="~/support/micromicrosofters/arm-based micromicromicrosofters-group/arm-based micromicromicromicromicrosofters/f/arm-based micromicromicromicromicrosofters-forum/110.0577万/am2634-am2634-am2634-download-application-image-size-issue-with -UART-uniflash2634 -UART-uniflash [/4079452#4079452"]2634 [/4079452#4079452"]大2634大图片407.9452万图片加407.9452万加载应用程序没有问题[/appfile问题]

    您意味着使用SBL UNIFUART LASH加载大应用程序图像文件(>752kb)是否正常?

    如何使用BL UART UNIFLAASH在主板上调试此问题 ?

    巴西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jay:

    我在这里有点困惑。 在4天前的帖子中(1)您提到了第二次使用SBL_JTAG_uniflash时appimage (752 KB)的loadraw超时。 我认为这是由于JTAG TCLK设置过高造成的。 现在您说您的appimage的loadraw是正常的。 这是否意味着您可以使用SBL_JTAG_uniflash? 例如,您可以使用SBL_JTAG_uniflash将SBL_QSPI (0x0万)和应用程序映像(0x8万)闪存到闪存中? 如果是这样,则应用程序应在闪存引导模式下工作。 接下来是SBL_UART_uniflash调试,因为SBL_JTAG_uniflash和SBL_UART_unflash之间的唯一区别是UART通信。

    顺便说一下,我确实尝试过加载原始appimage (620 KB)。 当JTAG TCLK使用MCU+ SDK 08.02 .00.30 上的SBL_JTAG_UNFLASH (带有板载XDS-110)设置为1MHz时,此功能有效。

    此致,

    明  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好Ming

    1)2634 /4081035#4081035#4081035"]1)您2634您提到408.1035万提到的408.1035万的JTAG_SB1g_timed408.1035万JTAG_SB1g_timed out时间使用752 KB (第二次映像时的映像 我认为这是由于JTAG TCLK设置过高造成的。 现在您说您的appimage的loadraw是正常的。 这是否意味着您可以使用SBL_JTAG_uniflash? 例如,您可以使用SBL_JTAG_uniflash将SBL_QSPI (0x0万)和应用程序映像(0x8万)闪存到闪存中? 如果是这样,则应用程序应在闪存引导模式下工作。 [/引述]

    (1)是, 当SBL_JTAG_uniflash loadraw appimage在脚本控制台中显示1万ms后超时,但 SBL_JTAG_uniflash正在验证成功!!...  =>因此我们 的应用 程序appimage (752 KB) 在闪存引导模式下使用 SBL_JTAG_uniflash可以正常工作  
    (2)接下来是SBL_UART_uniflash调试, 请告知我们如何解决此问题。

    巴西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jay:

    我将从SBL_UART_uniflash的UART通信和缓冲区排列开始。 请在SBL_UART_uniflash中添加一些调试日志信息,以检查错误发生的位置。 这可能是UART通信相关问题,如接收错误。 或者可能是接收缓冲区太小或与数据缓冲区/代码段重叠等

    同时,我将向软件开发团队报告错误,以获得进一步的建议。

    谢谢!