This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1230E6PM:1周后出现错误

Guru**** 2952440 points

Other Parts Discussed in Thread: TM4C1230E6PM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1097952/tm4c1230e6pm-bug-to-canbus-after-1-week

部件号:TM4C1230E6PM

您好,

我用10毫秒的CAN询问时间做了3次功能测试,系统工作了一个星期,然后我有了CAN总线框架,但没有传输。

我使用TM4C1230E6PM。

这是CANBUS配置

/**
 * @fn static void vd_srv_COM_Init(void)
 * @brief Activate interrupt CAN FIFO0 RX 
 * @param none
 * @return none
 */
void vd_srv_COM_Init(void)
{
    u32_UiCanBus = CAN0_BASE;
    /* Enable Rx interrupt */
    CANDisable(u32_UiCanBus);
    CANIntDisable(u32_UiCanBus, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    switch (u32_UiCanBus)
    {
    case CAN0_BASE:
        IntDisable(INT_CAN0);
        break;
    default:
        break;
    }
    IntDisable(INT_CAN0);
    CANInit(u32_UiCanBus);
    CANBitRateSet(u32_UiCanBus, SysCtlClockGet(), 250000);
    CANIntEnable(u32_UiCanBus, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    switch (u32_UiCanBus)
        {
        case CAN0_BASE:
            IntEnable(INT_CAN0);
            IntPrioritySet(INT_CAN0, 10);
            break;
        default:
            break;
        }
    CANEnable(u32_UiCanBus);
    g_sCANMsgObjectRx1.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
                                 );
    g_sCANMsgObjectRx1.pui8MsgData = u8_CanRxData;
    g_sCANMsgObjectRx1.ui32MsgID = 0x20;
    g_sCANMsgObjectRx1.ui32MsgIDMask = 0;
    g_sCANMsgObjectRx1.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
                             );
    g_sCANMsgObjectRx1.ui32MsgLen = 8;
    CANMessageSet(u32_UiCanBus, 1, &g_sCANMsgObjectRx1, MSG_OBJ_TYPE_RX);
    g_sCANMsgObjectRx1.ui32MsgLen = 7;
    CANMessageSet(u32_UiCanBus, 2, &g_sCANMsgObjectRx1, MSG_OBJ_TYPE_RX);
    g_sCANMsgObjectRx1.ui32MsgLen = 8;
    g_sCANMsgObjectRx1.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER | MSG_OBJ_REMOTE_FRAME
                                 );
    CANMessageSet(u32_UiCanBus, 3, &g_sCANMsgObjectRx1, MSG_OBJ_TYPE_RX_REMOTE);
}

这是带有传输的代码

static void vd_srv_com_WriteCanData8Octet(uint32_t u32_UiCanBus)
{
    uint16_t u16_CalculData = U16_NULL;
    int16_t i16_CalculCurrent = 0;
    /* Construit la trame � envoyer */

    g_sCANMsgObjectTx1.ui32MsgID = g_sCANMsgObjectRx1.ui32MsgID;
    g_sCANMsgObjectTx1.ui32MsgIDMask = 0;
    g_sCANMsgObjectTx1.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
    g_sCANMsgObjectTx1.ui32MsgLen = NB_DATA_LECTURE_8OCTET;

    /* S'il n'y � pas de d�faut dans le lecture de la tension alors */
    /* la tension prends la valeur de la jauge */
    if ( (u16_srv_SNS_GetVoltage() > 0) && ( u16_srv_SNS_GetVoltage() < 0xFFFF))
    {
        u16_CalculData = u16_srv_SNS_GetVoltage() / COEFF_MES;
    }
    else
    {
        u16_CalculData = u16_srv_MEASANA_GetVBattInMv() / COEFF_MES;
    }

    u8_CanTxData[0] = (u16_CalculData & FILTRE_POIDS_FORT) >> DECALAGE_8BIT;
    u8_CanTxData[1] = u16_CalculData & FILTRE_POIDS_FAIBLE;
    u8_CanTxData[2] = (uint8_t)(i8_srv_MEASANA_GetTempBattInDeg() + OFFSET_TEMP);

    u16_CalculData = u16_srv_MEASANA_GetIchargeInMa() / COEFF_MES;
    u8_CanTxData[3] = u16_CalculData & FILTRE_POIDS_FAIBLE;
    if (u16_srv_MEASANA_GetIoutInMa() < U16_SEUIL_SELECT_CURRENT)
    {
    	i16_CalculCurrent = i16_srv_SNS_GetCurrent() - (int16_t)(u16_srv_MEASANA_GetIchargeInMa());
        if (i16_CalculCurrent > 0)
        {
        	u16_CalculData = U16_NULL;
        }
        else
        {
        	u16_CalculData = (uint16_t)(-1 * i16_CalculCurrent);
        	u16_CalculData = u16_CalculData / COEFF_MES;
        }
    }
    else
    {
    	u16_CalculData = u16_srv_MEASANA_GetIoutInMa() / COEFF_MES;
    }
    u8_CanTxData[4] = u16_CalculData & FILTRE_POIDS_FAIBLE;;
    u8_CanTxData[5] = (uint8_t)(u16_srv_REGISTER_GetValue(ADD_REG_PARCBATTERIESOUSPARC)) & 0x0F;
    u8_CanTxData[5] |= ((uint8_t)(u16_srv_REGISTER_GetValue(ADD_REG_PARCBATTERIEPARC)) & 0x0F) << 4;
    u8_CanTxData[6] = (uint8_t)(u16_srv_REGISTER_GetValue(ADD_REG_STATUS));
    u8_CanTxData[7] = u8_srv_SNS_GetRsoc();

    /* Envoie de la trame CAN */
    g_sCANMsgObjectTx1.pui8MsgData = u8_CanTxData;
            CANMessageSet(u32_UiCanBus, 4, &g_sCANMsgObjectTx1, MSG_OBJ_TYPE_TX);
            while(!g_bMsgObj4Sent)
            {
            }
            g_bMsgObj4Sent = 0;
}

中断可以

/**
 * @fn void vd_app_scheduler_Update(void)
 * @brief Update scheduler counter and variable
 * @param none
 * @return none
 */
void CAN0_Handler(void)
{
 uint32_t ui32Status;

         //
         // Read the CAN interrupt status to find the cause of the interrupt
         //
         ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);

         //
         // If the cause is a controller status interrupt, then get the status
         //
         if(ui32Status == CAN_INT_INTID_STATUS)
         {
             //
             // Read the controller status.  This will return a field of status
             // error bits that can indicate various errors.  Error processing
             // is not done in this example for simplicity.  Refer to the
             // API documentation for details about the error status bits.
             // The act of reading this status will clear the interrupt.  If the
             // CAN peripheral is not connected to a CAN bus with other CAN devices
             // present, then errors will occur and will be indicated in the
             // controller status.
             //
             ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);

             //
             // Set a flag to indicate some errors may have occurred.
             //

             g_bErrFlag = 1;
             g_bMsgObj3Sent = 1;
             g_bMsgObj4Sent = 1;
             u8_FlagErrorCan = 1;
             u8_FlagRx = 1;
             CANIntClear(CAN0_BASE, 0);
             CANIntClear(CAN0_BASE, 1);
             CANIntClear(CAN0_BASE, 2);
             CANIntClear(CAN0_BASE, 3);
             CANIntClear(CAN0_BASE, 4);
             if (ui32Status & 0xE7)
             {
                 vd_srv_COM_Init();
             }

         }

         //
         // Check if the cause is message object 1, which is used for sending
         // message 1.
         //
         else if(ui32Status == 1)
         {
             u8_FlagRx = 1;

             //
             // Getting to this point means that the TX interrupt occurred on
             // message object 1, and the message TX is complete.  Clear the
             // message object interrupt.
             //
             CANIntClear(CAN0_BASE, 1);

             //
             // Increment a counter to keep track of how many messages have been
             // sent.  In a real application this could be used to set flags to
             // indicate when a message is sent.
             //
             g_ui32Msg1Count++;

             //
             // Since the message was sent, clear any error flags.
             //
             g_bErrFlag = 0;
           //  vd_srv_COM_ReceptInt(CAN0_BASE);
         }

         //
         // Check if the cause is message object 2, which is used for sending
         // message 2.
         //
         else if(ui32Status == 2)
         {
             u8_FlagRx = 1;

             //
             // Getting to this point means that the TX interrupt occurred on
             // message object 1, and the message TX is complete.  Clear the
             // message object interrupt.
             //
             CANIntClear(CAN0_BASE, 2);

             //
             // Increment a counter to keep track of how many messages have been
             // sent.  In a real application this could be used to set flags to
             // indicate when a message is sent.
             //
             g_ui32Msg1Count++;

             //
             // Since the message was sent, clear any error flags.
             //
             g_bErrFlag = 0;
            // vd_srv_COM_ReceptInt(CAN0_BASE);
         }

         //
         // Check if the cause is message object 3, which is used for sending
         // messages 3 and 4.
         //
         else if(ui32Status == 3)
         {
             u8_FlagRx = 1;

             //
             // Getting to this point means that the TX interrupt occurred on
             // message object 1, and the message TX is complete.  Clear the
             // message object interrupt.
             //
             CANIntClear(CAN0_BASE, 3);

             //
             // Increment a counter to keep track of how many messages have been
             // sent.  In a real application this could be used to set flags to
             // indicate when a message is sent.
             //
             g_ui32Msg1Count++;

             //
             // Since the message was sent, clear any error flags.
             //
             g_bErrFlag = 0;
             //vd_srv_COM_ReceptInt(CAN0_BASE);
         }

         //
         // Otherwise, something unexpected caused the interrupt.  This should
         // never happen.
         //
         else if(ui32Status == 4)
         {
             CANIntClear(CAN0_BASE, 4);

             //
             // Increment a counter to keep track of how many messages have been
             // sent.  In a real application this could be used to set flags to
             // indicate when a message is sent.
             //
             g_ui32Msg1Count++;
             g_bMsgObj3Sent = 1;
             g_bMsgObj4Sent = 1;
             //
             // Since the message was sent, clear any error flags.
             //
             g_bErrFlag = 0;
         }
         else
         {
             g_bMsgObj3Sent = 1;
             g_bMsgObj4Sent = 1;
             u8_FlagErrorCan = 1;
             CANIntClear(CAN0_BASE, 0);
         }

}

此致,

Ludovic Micou

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

     当停止发送帧时是否出现任何错误? 请检查以下两个寄存器,您看到了什么? 希望它能为您提供一些关于发生了什么的线索。 您可以在另一个主板上重复同样的问题吗? 老实说,这种问题已经存在一周,因此不容易调试。 我没有理由认为这是软件问题,如果它工作了一个多星期。 。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

    我没有另一个板。调试程序连接在板中以检查故障。 当故障出现时,我可以知道寄存器的状态。

    此致,

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    只是一个大猜测- 我看到全局 g_bMsgObj4Sent在传输函数和中断处理程序中被访问。 它是否被宣布为易失性?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    它不被声明为易失性

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的,我还没有真正研究过你的代码,但是中断是否有可能改变一个全局,就像其他人在使用它一样?
    将中断时访问的所有全局变量设置为易失性可能更安全,以便编译器/优化器知道该值可以随时更改。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

     我没有听到你的回复。 我假设您已解决了问题。 我现在将关闭此线程。 如果您有任何更新,只需写回此帖子,该主题将重新打开。