您好!
我想使用 SCI 和 DMA 与外部 IC 通信、即写入 IC 和从 IC 读取。
当我 启用 SCI 回送时、我能够写入数据并读回相同的数据。
下面是代码
/** @file HL_sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
#include "HL_system.h"
#include "HL_sci.h"
#include "HL_sys_pmu.h"
#include "HL_sys_dma.h"
#include "HL_sys_vim.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define size 20U
#define SCI2_TX_ADDR ((uint32_t)(&(sciREG2->TD)) + 3)
#define SCI2_RX_ADDR ((uint32_t)(&(sciREG2->RD)) + 3)
#define DMA_SCI2_TX_CH DMA_REQ41
#define DMA_SCI2_RX_CH DMA_REQ40
#define SCI_SET_TX_DMA (1<<16)
#define SCI_SET_RX_DMA (1<<17)
#define SCI_SET_RX_DMA_ALL (1<<18)
/* dma control packet configuration stack */
uint32 DMA_Comp_Flag;
uint32 DMA_TX_Counter;
uint32 DMA_RX_Counter;
#pragma SET_DATA_SECTION(".sharedRAM")
uint8 TX_Data[size] = {0};
uint8 RX_Data[size] = {0};
#pragma SET_DATA_SECTION()
int main(void);
void DMA_Init(void);
void scidmaInit();
void scidmaSend();
void scidmaReceive();
void Update_DMA_Comp_Flag(uint32 channel);
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
uint32 IDLECOUNT = 0;
_enable_IRQ_interrupt_();
sciInit();
sciEnableLoopback(sciREG2, Digital_Lbk);
/* Enable DMA */
dmaEnable();
/* Init SCI2 for DMA transfers */
DMA_Init();
/* Enable Interrupt after reception of data */
dmaEnableInterrupt(DMA_CH0, BTC, DMA_INTA);
scidmaSend();
dmaEnableInterrupt(DMA_CH1, BTC, DMA_INTA);
scidmaReceive();
/* Wait for the DMA interrupt ISR to set the Flag */
while(DMA_Comp_Flag != 0x55AAD09E){
IDLECOUNT++;
}
while (1);
/* USER CODE END */
//return 0;
}
/* USER CODE BEGIN (4) */
void DMA_Init(void)
{
/* Init SCI3 for DMA transfers */
scidmaInit();
}
/** @fn void scidmaInit(short mode)
* @brief Initialize the SCI and DMA to tranfer SCI data via DMA
* @note This function configures the SCI to trigger a DMA request when the SCI TX is complete.
*/
void scidmaInit()
{
dmaReqAssign(DMA_CH0, DMA_SCI2_TX_CH);
dmaReqAssign(DMA_CH1, DMA_SCI2_RX_CH);
/* Reset the Flag */
DMA_Comp_Flag = 0x55AAD09E;
/* Channel 40 - Enable the VIM channel in HalCoGen to include dmaBTCAInterrupt function */
vimChannelMap(40, 40, &dmaBTCAInterrupt);
/* Enable VIM DMA BTCA interrupt to CPU on SCI2 transfer complete */
vimEnableInterrupt(40, SYS_IRQ);
} /* scidmaInit */
/** @fn void scidmaSend(char *source_address, short mode)
* @brief Initialize the SCI and DMA to tranfer SCI data via DMA
* @note This function configures the SCI to trigger a DMA request when the SCI TX is complete.
*
* This function configures the DMA in single buffer or multibuffer mode.
* In single buffer mode (0) the DMA moves each Byte to the SCI tranmit register when request is set.
* In multi buffer mode (1) the DMA moves 4 Bytes to the SCI transmit buffer when the request is set.
*/
void scidmaSend()
{
g_dmaCTRL g_dmaCTRLPKT;
int i;
for(i=0; i<size; i++)
{
TX_Data[i] = i + 1;
}
/* Wait for the DMA to complete any existing transfers */
while(DMA_Comp_Flag != 0x55AAD09E);
/* Reset the Flag to not Done*/
DMA_Comp_Flag = ~0x55AAD09E;
/* - Populate dma control packets structure */
g_dmaCTRLPKT.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT.ELCNT = 1; /* element count */
g_dmaCTRLPKT.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.ELSOFFSET = 0; /* element source offset */
g_dmaCTRLPKT.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.FRSOFFSET = 0; /* frame source offset */
g_dmaCTRLPKT.PORTASGN = PORTA_READ_PORTB_WRITE; /* PORTA_READ_PORTB_WRITE */
g_dmaCTRLPKT.RDSIZE = ACCESS_8_BIT; /* read size */
g_dmaCTRLPKT.WRSIZE = ACCESS_8_BIT; /* write size */
g_dmaCTRLPKT.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT.ADDMODEWR = ADDR_FIXED; /* address mode write */
g_dmaCTRLPKT.AUTOINIT = AUTOINIT_OFF; /* autoinit */
g_dmaCTRLPKT.SADD = (uint32)TX_Data;
g_dmaCTRLPKT.DADD = SCI2_TX_ADDR;
g_dmaCTRLPKT.FRCNT = size;
/* - setting dma control packets for transmit */
dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT);
/* - setting the dma channel to trigger on h/w request */
dmaSetChEnable(DMA_CH0, DMA_HW);
/* Enable TX DMA */
sciREG2->SETINT = SCI_SET_TX_DMA;
} /* scidmaSend */
/** @fn void scidmaReceive(char *source_address)
*/
void scidmaReceive()
{
g_dmaCTRL g_dmaCTRLPKT;
/* Wait for the DMA to complete any existing transfers */
while(DMA_Comp_Flag != 0x55AAD09E);
/* Reset the Flag to not Done*/
DMA_Comp_Flag = ~0x55AAD09E;
/* - Populate dma control packets structure */
g_dmaCTRLPKT.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT.ELCNT = 1; /* element count */
g_dmaCTRLPKT.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.ELSOFFSET = 0; /* element source offset */
g_dmaCTRLPKT.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.FRSOFFSET = 0; /* frame source offset */
g_dmaCTRLPKT.PORTASGN = PORTB_READ_PORTA_WRITE; /* PORTB_READ_PORTA_WRITE */
g_dmaCTRLPKT.RDSIZE = ACCESS_8_BIT; /* read size */
g_dmaCTRLPKT.WRSIZE = ACCESS_8_BIT; /* write size */
g_dmaCTRLPKT.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT.ADDMODERD = ADDR_FIXED; /* address mode read */
g_dmaCTRLPKT.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT.AUTOINIT = AUTOINIT_OFF; /* autoinit */
g_dmaCTRLPKT.SADD = SCI2_RX_ADDR;
g_dmaCTRLPKT.DADD = (uint32)RX_Data;
g_dmaCTRLPKT.FRCNT = size;
/* - setting dma control packets for transmit */
dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT);
/* - setting the dma channel to trigger on h/w request */
dmaSetChEnable(DMA_CH1, DMA_HW);
sciEnableNotification(sciREG2, SCI_RX_INT);
/* Enable RX DMA */
sciREG2->SETINT |= SCI_SET_RX_DMA;
} /* scidmaReceive */
/** @fn void Update_DMA_Comp_Flag()
* @brief Switch the DMA complete flag to done and disable the SCI2 TX DMA interrupt
* @note This function needs to be called by dmaGroupANotification in notification.c
*/
void Update_DMA_Comp_Flag(uint32 channel)
{
/* Set the Flag to Done*/
DMA_Comp_Flag = 0x55AAD09E;
if(channel == DMA_CH0)
{
/* Disable TX DMA Interrupt */
sciREG2->CLEARINT = SCI_SET_TX_DMA;
DMA_TX_Counter++;
}
else if(channel == DMA_CH1)
{
/* Disable RX DMA Interrupt */
sciREG2->CLEARINT = SCI_SET_RX_DMA;
DMA_RX_Counter++;
}
}
/* USER CODE END */
但是、当我在没有回送的情况下回读时、这种情况不起作用。
在示例中、我也可以看到"SCI 回送被使用"或"Tx 和 Rx 在不同的硬件 SCI 单元上完成"。
无法同时使用相同的硬件进行发送和接收??
此致