This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS570LS3137:使用 OpenOCD 进行调试

Guru**** 2569105 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1106954/tms570ls3137-debugging-with-openocd

器件型号:TMS570LS3137

您好!

我正在尝试使用 OpenOCD 调试我的应用、但我在执行此任务时遇到了很多问题。 我使用 JLink Base 作为调试器、下面是 OpenOCD 配置文件:

set DAP_TAPID 0x0B8A002F
set JRC_TAPID 0x0B8A002F

source [find interface/jlink.cfg]
transport select jtag
source [find target/ti_tms570.cfg]

reset_config trst_only

JFlash 在连接到目标以及读取/写入闪存方面没有问题、但 OpenOCD 不允许调试我的应用、输出如下:

Open On-Chip Debugger 0.11.0+dev-00571-g254883597 (2022-02-17-13:22)
Licensed under GNU GPL v2
For bug reports, read
	openocd.org/.../bugs.html
Info : TI BE-32 quirks mode is enabled
trst_only separate trst_push_pull

Info : J-Link V10 compiled Nov  2 2021 12:14:50
Info : Hardware version: 10.10
Info : VTarget = 3.328 V
Info : clock speed 1500 kHz
Info : JTAG tap: tms570.jrc tap/device found: 0x4b8a002f (mfg: 0x017 (Texas Instruments), part: 0xb8a0, ver: 0x4)
Info : JTAG tap: tms570.cpu enabled
Warn : Debug base address for target tms570.cpu has bit 31 set to 0. Access to debug registers will likely fail!
Please fix the target configuration.
Info : tms570.cpu: hardware has 6 breakpoints, 2 watchpoints
Info : starting gdb server for tms570.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : JTAG tap: tms570.jrc tap/device found: 0x4b8a002f (mfg: 0x017 (Texas Instruments), part: 0xb8a0, ver: 0x4)
Info : JTAG tap: tms570.cpu enabled
Warn : Debug base address for target tms570.cpu has bit 31 set to 0. Access to debug registers will likely fail!
Please fix the target configuration.
Warn : tms570.cpu: ran after reset and before halt ...
Error: timed out while waiting for target halted
TARGET: tms570.cpu - Not halted
GDB Server stopped, exit code 1

您是否知道如何配置 OpenOCD 以便能够调试 TMS570应用?

此致、

Bartek