This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1294KCPDT:看门狗计时器-复位

Guru**** 2943350 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1053783/tm4c1294kcpdt-watchdog-timer---reset

器件型号:TM4C1294KCPDT

您好!

  我需要通过看门狗计时器每1秒检查一次程序执行情况。假设程序卡在上面,但 我需要等待200ms,然后 必须重置 控制器。我已经浏览了 TI 提供的看门狗示例代码。

 从这一点我知道,每隔1秒就会调用一次中断,这样看门狗定时器就会复位,但控制器不会复位。 在该中断函数内有标志、标志不会变为真。看门狗计时器将在2秒后复位微 cotroller。我对吗?

//*****************************************************************************
//
// watchdog.c - Watchdog timer example.
//
// Copyright (c) 2013-2014 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/watchdog.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"


//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Watchdog (watchdog)</h1>
//!
//! This example application demonstrates the use of the watchdog as a simple
//! heartbeat for the system.  If the watchdog is not periodically fed, it will
//! reset the system.  Each time the watchdog is fed, the LED is inverted so
//! that it is easy to see that it is being fed, which occurs once every
//! second.  To stop the watchdog being fed and, hence, cause a system reset,
//! press the SW1 button.
//
//*****************************************************************************

//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;

//*****************************************************************************
//
// Flag to tell the watchdog interrupt handler whether or not to clear the
// interrupt (feed the watchdog).
//
//*****************************************************************************
volatile bool g_bFeedWatchdog = true;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// The interrupt handler for the watchdog.  This feeds the dog (so that the
// processor does not get reset) and winks the LED connected to GPIO B3.
//
//*****************************************************************************
void
WatchdogIntHandler(void)
{
    //
    // If we have been told to stop feeding the watchdog, return immediately
    // without clearing the interrupt.  This will cause the system to reset
    // next time the watchdog interrupt fires.
    //
    if(!g_bFeedWatchdog)
    {
        return;
    }
    //
    // Clear the watchdog interrupt.
    //
    ROM_WatchdogIntClear(WATCHDOG0_BASE);

    //
    // Invert the GPIO PN0 value.
    //
    ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0,
                     (ROM_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_0) ^
                                     GPIO_PIN_0));
}

//*****************************************************************************
//
// This function is called when the SW1 button is pressed.
//
//*****************************************************************************
static int32_t
SW1ButtonPressed(void)
{
    //
    // Set the flag that tells the interrupt handler not to clear the
    // watchdog interrupt.
    //
    g_bFeedWatchdog = false;
    return(0);
}

//*****************************************************************************
//
// This example demonstrates the use of the watchdog timer.
//
//*****************************************************************************
int
main(void)
{
    //
    // Set the clocking to run directly from the crystal at 120MHz.
    //
    g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                             SYSCTL_OSC_MAIN |
                                             SYSCTL_USE_PLL |
                                             SYSCTL_CFG_VCO_480), 120000000);
   //
   // Initialize the buttons driver.
   //
   //  ButtonsInit();
    //
    // Enable the peripherals used by this example.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_WDOG0);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);

    //
    // Enable processor interrupts.
    //
    ROM_IntMasterEnable();

    //
    // Set GPIO PN0 as an output.  This drives an LED on the board that will
    // toggle when a watchdog interrupt is processed.
    //
    ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
    ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);

    //
    // Enable the watchdog interrupt.
    //
    ROM_IntEnable(INT_WATCHDOG);

    //
    // Set the period of the watchdog timer to 1 second.
    //
    ROM_WatchdogReloadSet(WATCHDOG0_BASE, g_ui32SysClock);

    //
    // Enable reset generation from the watchdog timer.
    //
    ROM_WatchdogResetEnable(WATCHDOG0_BASE);

    //
    // Enable the watchdog timer.
    //
    ROM_WatchdogEnable(WATCHDOG0_BASE);

    //
    // Loop forever while the LED winks as watchdog interrupts are handled.
    //
    while(1)
    {
        //
        // Poll for the select button pressed
        //
         uint8_t ui8Buttons = ButtonsPoll(0, 0);
         if(ui8Buttons & USR_SW1)
        {
            SW1ButtonPressed();
            while(1)
            {
            }
        }
    }
}

谢谢、

Rani

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Rani、

    [引用 userid="473476" URL"~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1053783/tm4c1294kcpdt-watchdog-timer---reset 中的内容] 我了解到,每次调用 interupt 后,看门狗计时器都会重置,但控制器不会重置。 在该中断函数内有标志、标志不会变为真。看门狗计时器将在2秒后复位微控制器。我是否正确?[/QUERP]

    是的、没错。 第二个中断将触发复位。 第一 个超时通过设置中断标志来触发看门狗中断。 如果在 下一次超时发生时该中断标志未被清除、则超时将触发系统复位。

    此致、

    Ralph Jacobi