This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SW-TM4C:TM4C1294KCPDT 芯片的 UDP TX 问题

Guru**** 2567795 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1047358/sw-tm4c-udp-tx-problem-with-tm4c1294kcpdt-chip

器件型号:SW-TM4C
我联系了客户支持中心、他们要求我将其发布在这里。 
今年早些时候、用于 C 系列的 TivaWare 软件(使用版本2.1.4.178)中出现 UDP 传输问题、 
但在版本2.2.0.295中似乎也没有对其进行修正。

此症状是由于数据碎片超过 MTU 大小而导致的。 
具体而言、CRC 错误发生在数据接收端、数据似乎已部分损坏。 

我猜问题是下面的功能。 

(路径:third_parti\lwip-1.4.1\ports\Tiva-tm4c129\netif\Tiva-tm4c129.c)
static err_t
tivaif_transmit(struct netif *psNetif, struct pbuf *p)
{
  tStellarisIF *pIF;
  tDescriptor *pDesc;
  struct pbuf *pBuf;
  uint32_t ui32NumChained, ui32NumDescs;
  bool bFirst;
  SYS_ARCH_DECL_PROTECT(lev);

  LWIP_DEBUGF(NETIF_DEBUG, ("tivaif_transmit 0x%08x, len %d\n", p,
              p->tot_len));

  /**
   * This entire function must run within a "critical section" to preserve
   * the integrity of the transmit pbuf queue.
   */
  SYS_ARCH_PROTECT(lev);

  /* Update our transmit attempt counter. */
  DRIVER_STATS_INC(TXCount);

  /**
   * Increase the reference count on the packet provided so that we can
   * hold on to it until we are finished transmitting its content.
   */
  pbuf_ref(p);

  /**
   * Determine whether all buffers passed are within SRAM and, if not, copy
   * the pbuf into SRAM-resident buffers so that the Ethernet DMA can access
   * the data.
   */
  p = tivaif_check_pbuf(p);

  /* Make sure we still have a valid buffer (it may have been copied) */
  if(!p)
  {
      LINK_STATS_INC(link.memerr);
      SYS_ARCH_UNPROTECT(lev);
      return(ERR_MEM);
  }

  /* Get our state data from the netif structure we were passed. */
  pIF = (tStellarisIF *)psNetif->state;

  /* Make sure that the transmit descriptors are not all in use */
  pDesc = &(pIF->pTxDescList->pDescriptors[pIF->pTxDescList->ui32Write]);
  if(pDesc->pBuf)
  {
      /**
       * The current write descriptor has a pbuf attached to it so this
       * implies that the ring is full. Reject this transmit request with a
       * memory error since we can't satisfy it just now.
       */
      pbuf_free(p);
      LINK_STATS_INC(link.memerr);
      DRIVER_STATS_INC(TXNoDescCount);
      SYS_ARCH_UNPROTECT(lev);
      return (ERR_MEM);
  }

  /* How many pbufs are in the chain passed? */
  ui32NumChained = (uint32_t)pbuf_clen(p);

  /* How many free transmit descriptors do we have? */
  ui32NumDescs = (pIF->pTxDescList->ui32Read > pIF->pTxDescList->ui32Write) ?
          (pIF->pTxDescList->ui32Read - pIF->pTxDescList->ui32Write) :
          ((NUM_TX_DESCRIPTORS - pIF->pTxDescList->ui32Write) +
           pIF->pTxDescList->ui32Read);

  /* Do we have enough free descriptors to send the whole packet? */
  if(ui32NumDescs < ui32NumChained)
  {
      /* No - we can't transmit this whole packet so return an error. */
      pbuf_free(p);
      LINK_STATS_INC(link.memerr);
      DRIVER_STATS_INC(TXNoDescCount);
      SYS_ARCH_UNPROTECT(lev);
      return (ERR_MEM);
  }

  /* Tag the first descriptor as the start of the packet. */
  bFirst = true;
  pDesc->Desc.ui32CtrlStatus = DES0_TX_CTRL_FIRST_SEG;

  /* Here, we know we can send the packet so write it to the descriptors */
  pBuf = p;

  while(ui32NumChained)
  {
      /* Get a pointer to the descriptor we will write next. */
      pDesc = &(pIF->pTxDescList->pDescriptors[pIF->pTxDescList->ui32Write]);

      /* Fill in the buffer pointer and length */
      pDesc->Desc.ui32Count = (uint32_t)pBuf->len;
      pDesc->Desc.pvBuffer1 = pBuf->payload;

      /* Tag the first descriptor as the start of the packet. */
      if(bFirst)
      {
          bFirst = false;
          pDesc->Desc.ui32CtrlStatus = DES0_TX_CTRL_FIRST_SEG;
      }
      else
      {
          pDesc->Desc.ui32CtrlStatus = 0;
      }

      pDesc->Desc.ui32CtrlStatus |= (DES0_TX_CTRL_IP_ALL_CKHSUMS |
                                     DES0_TX_CTRL_CHAINED);

      /* Decrement our descriptor counter, move on to the next buffer in the
       * pbuf chain. */
      ui32NumChained--;
      pBuf = pBuf->next;

      /* Update the descriptor list write index. */
      pIF->pTxDescList->ui32Write++;
      if(pIF->pTxDescList->ui32Write == NUM_TX_DESCRIPTORS)
      {
          pIF->pTxDescList->ui32Write = 0;
      }

      /* If this is the last descriptor, mark it as the end of the packet. */
      if(!ui32NumChained)
      {
          pDesc->Desc.ui32CtrlStatus |= (DES0_TX_CTRL_LAST_SEG |
                                         DES0_TX_CTRL_INTERRUPT);

          /* Tag the descriptor with the original pbuf pointer. */
          pDesc->pBuf = p;
      }
      else
      {
          /* Set the lsb of the pbuf pointer.  We use this as a signal that
           * we should not free the pbuf when we are walking the descriptor
           * list while processing the transmit interrupt.  We only free the
           * pbuf when processing the last descriptor used to transmit its
           * chain.
           */
          pDesc->pBuf = (struct pbuf *)((uint32_t)p + 1);
      }

      DRIVER_STATS_INC(TXBufQueuedCount);

      /* Hand the descriptor over to the hardware. */
      pDesc->Desc.ui32CtrlStatus |= DES0_TX_CTRL_OWN;
  }

  /* Tell the transmitter to start (in case it had stopped). */
  EMACTxDMAPollDemand(EMAC0_BASE);

  /* Update lwIP statistics */
  LINK_STATS_INC(link.xmit);

  SYS_ARCH_UNPROTECT(lev);

  return(ERR_OK);
}

我们修改了以下函数并确认了正常运行。
更正后的行为103和110。
static err_t
if_transmit(struct netif *psNetif, struct pbuf *p)
{
  tStellarisIF *pIF;
  tDescriptor *pDesc;
  struct pbuf *pBuf;
  uint32_t ui32NumChained, ui32NumDescs;
  bool bFirst;
  SYS_ARCH_DECL_PROTECT(lev);

  LWIP_DEBUGF(NETIF_DEBUG, ("tivaif_transmit 0x%08x, len %d\n", p,
              p->tot_len));

  /**
   * This entire function must run within a "critical section" to preserve
   * the integrity of the transmit pbuf queue.
   */
  SYS_ARCH_PROTECT(lev);

  /* Update our transmit attempt counter. */
  DRIVER_STATS_INC(TXCount);

  /**
   * Increase the reference count on the packet provided so that we can
   * hold on to it until we are finished transmitting its content.
   */
  pbuf_ref(p);

  /**
   * Determine whether all buffers passed are within SRAM and, if not, copy
   * the pbuf into SRAM-resident buffers so that the Ethernet DMA can access
   * the data.
   */
  p = tivaif_check_pbuf(p);

  /* Make sure we still have a valid buffer (it may have been copied) */
  if(!p)
  {
      LINK_STATS_INC(link.memerr);
      SYS_ARCH_UNPROTECT(lev);
      return(ERR_MEM);
  }

  /* Get our state data from the netif structure we were passed. */
  pIF = (tStellarisIF *)psNetif->state;

  /* Make sure that the transmit descriptors are not all in use */
  pDesc = &(pIF->pTxDescList->pDescriptors[pIF->pTxDescList->ui32Write]);
  if(pDesc->pBuf)
  {
      /**
       * The current write descriptor has a pbuf attached to it so this
       * implies that the ring is full. Reject this transmit request with a
       * memory error since we can't satisfy it just now.
       */
      pbuf_free(p);
      LINK_STATS_INC(link.memerr);
      DRIVER_STATS_INC(TXNoDescCount);
      SYS_ARCH_UNPROTECT(lev);
      return (ERR_MEM);
  }

  /* How many pbufs are in the chain passed? */
  ui32NumChained = (uint32_t)pbuf_clen(p);

  /* How many free transmit descriptors do we have? */
  ui32NumDescs = (pIF->pTxDescList->ui32Read > pIF->pTxDescList->ui32Write) ?
          (pIF->pTxDescList->ui32Read - pIF->pTxDescList->ui32Write) :
          ((NUM_TX_DESCRIPTORS - pIF->pTxDescList->ui32Write) +
           pIF->pTxDescList->ui32Read);

  /* Do we have enough free descriptors to send the whole packet? */
  if(ui32NumDescs < ui32NumChained)
  {
      /* No - we can't transmit this whole packet so return an error. */
      pbuf_free(p);
      LINK_STATS_INC(link.memerr);
      DRIVER_STATS_INC(TXNoDescCount);
      SYS_ARCH_UNPROTECT(lev);
      return (ERR_MEM);
  }

  /* Tag the first descriptor as the start of the packet. */
  bFirst = true;
  pDesc->Desc.ui32CtrlStatus = DES0_TX_CTRL_FIRST_SEG;

  /* Here, we know we can send the packet so write it to the descriptors */
  pBuf = p;

  while(ui32NumChained)
  {
      /* Get a pointer to the descriptor we will write next. */
      pDesc = &(pIF->pTxDescList->pDescriptors[pIF->pTxDescList->ui32Write]);

      /* Fill in the buffer pointer and length */
      pDesc->Desc.ui32Count = (uint32_t)pBuf->len;
      pDesc->Desc.pvBuffer1 = pBuf->payload;

      /* Tag the first descriptor as the start of the packet. */
      if(bFirst)
      {
          bFirst = false;
          pDesc->Desc.ui32CtrlStatus = (DES0_TX_CTRL_FIRST_SEG | DES0_TX_CTRL_IP_ALL_CKHSUMS);
      }
      else
      {
          pDesc->Desc.ui32CtrlStatus = 0;
      }

      pDesc->Desc.ui32CtrlStatus |= (//DES0_TX_CTRL_IP_ALL_CKHSUMS |
                                     DES0_TX_CTRL_CHAINED);

      /* Decrement our descriptor counter, move on to the next buffer in the
       * pbuf chain. */
      ui32NumChained--;
      pBuf = pBuf->next;

      /* Update the descriptor list write index. */
      pIF->pTxDescList->ui32Write++;
      if(pIF->pTxDescList->ui32Write == NUM_TX_DESCRIPTORS)
      {
          pIF->pTxDescList->ui32Write = 0;
      }

      /* If this is the last descriptor, mark it as the end of the packet. */
      if(!ui32NumChained)
      {
          pDesc->Desc.ui32CtrlStatus |= (DES0_TX_CTRL_LAST_SEG |
                                         DES0_TX_CTRL_INTERRUPT);

          /* Tag the descriptor with the original pbuf pointer. */
          pDesc->pBuf = p;
      }
      else
      {
          /* Set the lsb of the pbuf pointer.  We use this as a signal that
           * we should not free the pbuf when we are walking the descriptor
           * list while processing the transmit interrupt.  We only free the
           * pbuf when processing the last descriptor used to transmit its
           * chain.
           */
          pDesc->pBuf = (struct pbuf *)((uint32_t)p + 1);
      }

      DRIVER_STATS_INC(TXBufQueuedCount);

      /* Hand the descriptor over to the hardware. */
      pDesc->Desc.ui32CtrlStatus |= DES0_TX_CTRL_OWN;
  }

  /* Tell the transmitter to start (in case it had stopped). */
  EMACTxDMAPollDemand(EMAC0_BASE);

  /* Update lwIP statistics */
  LINK_STATS_INC(link.xmit);

  SYS_ARCH_UNPROTECT(lev);

  return(ERR_OK);
}



芯片仅实现了 UDP、因此未测试其他协议。

请审查可行性。

感谢您的支持。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="502452" URL"~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1047358/sw-tm4c-udp-tx-problem-with-tm4c1294kcpdt-chip "]具体而言,数据接收端会出现 CRC 错误,数据似乎部分损坏。

    我尚未研究过您的代码更改、但问题似乎与我在 MSP432E401Y 中描述的类似:simplelink_msp432e4_sdk_4_20_00_12中的 NDK 无法发送碎片化的 UDP 数据包、但可以接收这些数据包。

    虽然引用的线程用于运行简单 NDK 的 MSP432E 器件、而不是运行 LWIP 的 TM4C129、但两个器件共享相同的以太网外设、因此以太网驱动程序中可能存在一些重叠。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    查看 Wireshark 捕获、我认为相同的症状是正确的。

    即使在第一个片段之后放置 CRC 也是一个问题。

    与其他芯片一样、TI SDK 似乎存在总体问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Sung-hyun:

     我认为我理解您在做什么、我同意。 在 TivaWare 驱动程序中、无论 描述符是否为数据包起始、DES0_TX_CTRL_IP_All_CKHSUMS 标志的 CIC 字段都会写入所有描述符。 但是、根据数据表、CIC 仅在描述符是数据包开头时有效。 更改代码后 、DES0_TX_CTRL_IP_All_CKHSUMS 仅在 设置 DES0_TX_CTRL_FIRST_SEG 时应用于数据包开头。 我认为、通过修改、您将不再看到任何数据损坏。 这是正确的理解吗? 再次感谢您找到问题、我将为该帖子添加书签、以便在其他人遇到相同问题时供将来参考。  

    CIC:校验和插入控制
    这些位控制着以太网帧中校验和的插入、这些帧通过 IPv4封装 TCP、UDP 或 ICMP
    或 IPv6。 当第一段控制位(TDES0[28])被置位时、该域有效。
    ■0x0 =不执行任何操作。 校验和引擎被绕过。
    ■0x1 =插入 IPv4报头校验和。 使用此值在帧时插入 IPv4标头校验和
    封装 IPv4数据报。
    ■0x2 =插入 TCP/UDP/ICMP 校验和。 校验和在 TCP、UDP 或 ICMP 段上计算
    仅当 TCP、UDP 或 ICMP 伪报头校验和出现在相应的中时
    输入帧的校验和字段。 如果是封装的数据报,则还会插入 IPv4报头校验和
    符合 IPv4。
    ■0x3 =插入在该引擎中完全计算的 TCP/UDP/ICMP 校验和。 TCP、UDP 或 ICMP
    伪报头包含在校验和计算中、以及输入帧的相应校验和字段中
    全零值。 如果封装的数据报符合,还会插入 IPv4标头校验和
    IPv4。
    校验和引擎检测 TCP、UDP 或 ICMP 段是否封装在 IPv4或 IPv6和中
    相应地处理其数据。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢你的答复。
    您的理解是正确的。
    将来是否可以针对相关问题修改版本?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Sung-hyun:

     近期内、没有计划发布另一个 TivaWare 版本。 但是 、我会注意到您报告的问题 、并将其包含在未来的 TivaWare 版本中。 同时、请为您的应用使用您修改的代码来解决此问题。  

    [编辑:2021年10月25日12:晚上11点]我已提交内部 TT 以跟踪此问题。