This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1294NCPDT:TM4C129DNCPDT:FATSD 和 FATSDRAW

Guru**** 2612065 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1038635/tm4c1294ncpdt-tm4c129dncpdt-fatsd-and-fatsdraw

器件型号:TM4C1294NCPDT

你(们)好

我很难在 TI 文档和 FATFS 网站上找到参考资料、以解释 FATSD 和 FASTDRAW 之间的区别。

 基于的 fatsdusbcopy?

谢谢

R.  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Richard、

    我也不确定-我认为这不是 TivaWare 的一部分。 如果它是用于 Tiva-C 的 TI-RTOS 的一部分、我们不参与构建、提供的产品是我无法回答的问题。 虽然我不知道是谁将其引导至哪个位置。

    就以下方面而言:

    [引用 userid="114962" URL"~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1038635/tm4c1294ncpdt-tm4c129dncpdt-fatsd-and-fatsdraw "] 基于以下内容的 fatsdusbcopy?

    我可以看到、它使用 USBMSCHFatFs 驱动程序、该驱动程序似乎仅使用标准 FatFs:

     *  The USBMSCHFatFs header file should be included in an application as follows:
     *  @code
     *  #include <ti/drivers/USBMSCHFatFs.h>
     *  @endcode
     *
     *  # Operation #
     *
     *  The USBMSCHFatFs driver is a driver designed to hook into FatFs. It
     *  implements a set of functions that FatFs needs to call to perform basic
     *  block data transfers.
     *
     *  This driver is designed to work with the USB Library. Because it is running
     *  in host mode, we need to add protection when accessing the USB Library. A
     *  gate was added to prevent the task servicing the USB library to preempt any
     *  other task accessing the USB Library.
     *
     *  Once the driver has been opened, the application may used the FatFs APIs or
     *  the standard C runtime file I/O calls (fopen, fclose, etc...). Once the
     *  driver has been closed, ensure the application does NOT make any file I/O
     *  calls.
     *
     *  ## Opening the driver #
     *
     *  @code
     *  USBMSCHFatFs_Handle      handle;
     *  USBMSCHFatFs_Params      params;
     *
     *  USBMSCHFatFs_Params_init(&params);
     *  params.servicePriority  = somePriority;
     *  handle = USBMSCHFatFs_open(someUSBMSCHFatFs_configIndexValue, &params);
     *  if (!handle) {
     *      System_printf("USBMSCHFatFs did not open");
     *  }
     *  @endcode
     *
     *  # Implementation #
     *
     *  This module serves as the main interface for TI-RTOS
     *  applications. Its purpose is to redirect the module's APIs to specific
     *  peripheral implementations which are specified using a pointer to a
     *  USBMSCHFatFs_FxnTable.
     *
     *  The USBMSCHFatFs driver interface module is joined (at link
     *  time) to a NULL-terminated array of USBMSCHFatFs_Config data structures
     *  named *USBMSCHFatFs_config*. *USBMSCHFatFs_config* is implemented in the
     *  application with each entry being an instance of a USBMSCHFatFs peripheral.
     *  Each entry in *USBMSCHFatFs_config* contains a:
     *  - (USBMSCHFatFs_FxnTable *) to a set of functions that implement a
     *    USBMSCHFatFs peripheral
     *  - (void *) data object that is associated with the USBMSCHFatFs_FxnTable
     *  - (void *) hardware attributes that are associated to the
     *    USBMSCHFatFs_FxnTable

    此致、

    Ralph Jacobi

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    FATFS 使用 stdio.h 文件命令、其中 FATFSRAW 访问 TI 演示代码中的 FATFS 命令而不是 stdio.h。 此问题与 FATFS 无关  

     USBMSCHFatFS 使用 stdio 文件命令而不是 FATFS 直接命令。  

    不知道做这件事有什么优点和缺点。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Richard、

    很遗憾、我也没有-我只是没有 SD 卡或 FATFS 方面的经验、我从未研究过 SD 卡的 TI-RTOS 演示。

    很抱歉、我在这里没有能力提供帮助...

    此致、

    Ralph Jacobi