This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] EK-TM4C123GXL:I2C 从设备

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1006883/ek-tm4c123gxl-i2c-slave

器件型号:EK-TM4C123GXL

您好!

我已将 TM4C123G 上的 PB2/I2C0SCL、PB3/I2C0SDA 连接 到另一个 CPU。

我将 TM4C123G 配置为 i2c 从器件重新路由至演示代码 SLAVE_Receive_int.c

我使用 i2cdetect 工具来发现 TM4C123G、但没有回复。

我应该做什么正确的配置? 谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    该示例使用环回模式。 我不知道您的 i2cdetect 工具有什么作用、但该示例不会响应外部主器件。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢、Bob。

    您知道如何修改示例、然后主器件可以检测到该示例吗?

    i2cdetect 工具是 Linux 中的开源代码。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尝试此代码;

    //*****************************************************************************
    //
    // slave_receive_int.c - Example demonstrating a simple I2C master message
    //                       transmission using a slave interrupt when data is
    //                       received.
    //
    // Copyright (c) 2010-2020 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    // 
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the  
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // 
    // This is part of revision 2.2.0.295 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_i2c.h"
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "driverlib/gpio.h"
    #include "driverlib/i2c.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup i2c_examples_list
    //! <h1>Slave Receive Interrupt (slave_receive_int)</h1>
    //!
    //! This example shows how to configure a receive interrupt on the slave
    //! module.  This includes setting up the I2C0 module for loopback mode as well
    //! as configuring the master and slave modules.  Loopback mode internally
    //! connects the master and slave data and clock lines together.  The address
    //! of the slave module is set to a value so it can receive data from the
    //! master.
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - I2C0 peripheral
    //! - GPIO Port B peripheral (for I2C0 pins)
    //! - I2C0SCL - PB2
    //! - I2C0SDA - PB3
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of I2C.
    //! - UART0 peripheral
    //! - GPIO Port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - INT_I2C0 - I2C0SlaveIntHandler
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Set the address for slave module. This is a 7-bit address sent in the
    // following format:
    //                      [A6:A5:A4:A3:A2:A1:A0:RS]
    //
    // A zero in the R/S position of the first byte means that the master
    // transmits (sends) data to the selected slave, and a one in this position
    // means that the master receives data from the slave.
    //
    //*****************************************************************************
    #define SLAVE_ADDRESS           0x3C
    
    //*****************************************************************************
    //
    // Global variable to hold the I2C data that has been received.
    //
    //*****************************************************************************
    static uint32_t g_ui32DataRx;
    
    //*****************************************************************************
    //
    // This is a flag that gets set in the interrupt handler to indicate that an
    // interrupt occurred.
    //
    //*****************************************************************************
    volatile static bool g_bIntFlag = false;
    
    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    //
    //*****************************************************************************
    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);
    
        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    
        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, 16000000);
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for the for I2C0 data slave interrupt.
    //
    //*****************************************************************************
    void
    I2C0SlaveIntHandler(void)
    {
        //
        // Clear the I2C0 interrupt flag.
        //
        I2CSlaveIntClear(I2C0_BASE);
    
        //
        // Read the data from the slave.
        //
        g_ui32DataRx = I2CSlaveDataGet(I2C0_BASE);
    
        //
        // Set a flag to indicate that the interrupt occurred.
        //
        g_bIntFlag = true;
    }
    
    //*****************************************************************************
    //
    // Configure the I2C0 master and slave and connect them using loopback mode.
    //
    //*****************************************************************************
    int
    main(void)
    {
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
        defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        uint32_t ui32SysClock;
    #endif
        uint32_t ui32DataTx;
    
        //
        // Set the clocking to run directly from the external crystal/oscillator.
        // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
        // crystal on your board.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
        defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                           SYSCTL_OSC_MAIN |
                                           SYSCTL_USE_PLL), 25000000);
    #else
        SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                       SYSCTL_XTAL_16MHZ);
    #endif
    
        //
        // The I2C0 peripheral must be enabled before use.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
    
        //
        // For this example I2C0 is used with PortB[3:2].  The actual port and
        // pins used may be different on your part, consult the data sheet for
        // more information.  GPIO port B needs to be enabled so these pins can
        // be used.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    
        //
        // Configure the pin muxing for I2C0 functions on port B2 and B3.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PB2_I2C0SCL);
        GPIOPinConfigure(GPIO_PB3_I2C0SDA);
    
        //
        // Select the I2C function for these pins.  This function will also
        // configure the GPIO pins pins for I2C operation, setting them to
        // open-drain operation with weak pull-ups.  Consult the data sheet
        // to see which functions are allocated per pin.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
        GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
    
        //
        // Enable loopback mode.  Loopback mode is a built in feature that helps
        // for debug the I2Cx module.  It internally connects the I2C master and
        // slave terminals, which effectively lets you send data as a master and
        // receive data as a slave.  NOTE: For external I2C operation you will need
        // to use external pull-ups that are faster than the internal pull-ups.
        // Refer to the datasheet for more information.
        //
        // Comment out this line to allow i2cdetect to detect the slave
        //HWREG(I2C0_BASE + I2C_O_MCR) |= 0x01;
    
        //
        // Enable the I2C0 interrupt on the processor (NVIC).
        //
        IntRegister(INT_I2C0, I2C0SlaveIntHandler);
        IntEnable(INT_I2C0);
    
        //
        // Configure and turn on the I2C0 slave interrupt.  The I2CSlaveIntEnableEx()
        // gives you the ability to only enable specific interrupts.  For this case
        // we are only interrupting when the slave device receives data.
        //
        I2CSlaveIntEnableEx(I2C0_BASE, I2C_SLAVE_INT_DATA);
    
        //
        // Enable and initialize the I2C0 master module.  Use the system clock for
        // the I2C0 module.  The last parameter sets the I2C data transfer rate.
        // If false the data rate is set to 100kbps and if true the data rate will
        // be set to 400kbps.  For this example we will use a data rate of 100kbps.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
        defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        I2CMasterInitExpClk(I2C0_BASE, ui32SysClock, false);
    #else
        I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
    #endif
    
        //
        // Enable the I2C0 slave module.
        //
        I2CSlaveEnable(I2C0_BASE);
    
        //
        // Set the slave address to SLAVE_ADDRESS.  In loopback mode, it's an
        // arbitrary 7-bit number (set in a macro above) that is sent to the
        // I2CMasterSlaveAddrSet function.
        //
        I2CSlaveInit(I2C0_BASE, SLAVE_ADDRESS);
    
        //
        // Tell the master module what address it will place on the bus when
        // communicating with the slave.  Set the address to SLAVE_ADDRESS
        // (as set in the slave module).  The receive parameter is set to false
        // which indicates the I2C Master is initiating a writes to the slave.  If
        // true, that would indicate that the I2C Master is initiating reads from
        // the slave.
        //
        I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
    
        //
        // Set up the serial console to use for displaying messages.  This is just
        // for this example program and is not needed for proper I2C operation.
        //
        InitConsole();
    
        //
        // Enable interrupts to the processor.
        //
        IntMasterEnable();
    
        //
        // Display the example setup on the console.
        //
        UARTprintf("I2C Slave Interrupt Example ->");
        UARTprintf("\n   Module = I2C0");
        UARTprintf("\n   Mode = Receive interrupt on the Slave module");
        UARTprintf("\n   Rate = 100kbps\n\n");
    
        //
        // Initialize the data to send.
        //
        ui32DataTx = 'I';
    
        //
        // Indicate the direction of the data.
        //
        UARTprintf("Transferring from: Master -> Slave\n");
    
        //
        // Display the data that I2C0 is transferring.
        //
        UARTprintf("  Sending: '%c'", ui32DataTx);
    
        //
        // Place the data to be sent in the data register.
        //
        I2CMasterDataPut(I2C0_BASE, ui32DataTx);
    
        //
        // Initiate send of single piece of data from the master.  Since the
        // loopback mode is enabled, the Master and Slave units are connected
        // allowing us to receive the same data that we sent out.
        //
        I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
    
        //
        // Wait for interrupt to occur.
        //
        while(!g_bIntFlag)
        {
        }
    
        //
        // Display that interrupt was received.
        //
        UARTprintf("\n  Slave Interrupt Received!\n");
    
        //
        // Display the data that the slave has received.
        //
        UARTprintf("  Received: '%c'\n\n", g_ui32DataRx);
    
        //
        // Loop forever.
        //
        while(1)
        {
        }
    }
    

    我所做的更改是:

    1.在第115行的变量 g_bIntFlag 中添加了 volatile 关键字

    2.注释掉了在第261行启用环回模式的 HWREG 写入

    3.在第263行添加了对 IntRegister 的调用。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢。 Bob。

    这很有用、我将与我们的硬件团队一起验证它。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Bob:

    当从主器件发出 i2cdette/i2cset 时、该演示效果良好。

    但当 i2cget 时、它会出现读取失败的问题。

    如何读取? 我应该在 MCU 中添加一些寄存器吗?

    谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    该示例不会将数据发送回主器件。 该示例是一个从器件接收示例。  

    要响应主器件的读取请求、必须将数据放入 数据寄存器中。 通过调用 TivaWare 函数 I2CSlaveDataPut ()来执行此操作。