This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL2-TMS57012:错误-1170 @ 0x0

Guru**** 2587925 points
Other Parts Discussed in Thread: TMS570LS1224

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/999295/launchxl2-tms57012-error--1170-0x0

器件型号:LAUNCHXL2-TMS57012
主题中讨论的其他器件:TMS570LS1224

大家好、我有一个 Hercules TMS570LS1224、目标是新的、是我第一次使用它

我尝试连接时收到以下错误消息:

"CortexR4:连接到目标时出错:(错误-1170 @ 0x0)无法访问 DAP。 重置设备、然后重试此操作。 如果错误仍然存在,请确认配置,重新打开电路板电源,和/或尝试更可靠的 JTAG 设置(例如,较低的 TCLK)。(仿真包9.3.0.00042)

谢谢