This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 编译器/TMS570LS3137:ARM_15.12.3.LTS

Guru**** 2587365 points
Other Parts Discussed in Thread: CCSTUDIO, TMS570LS3137

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/585252/compiler-tms570ls3137-arm_15-12-3-lts

器件型号:TMS570LS3137
主题中讨论的其他器件:CCStudio

工具/软件:TI C/C++编译器

您好!

我将面临 GEL 脚本和 Java 脚本。

InvokeCSS.js

//将 DSS 软件包导入我们的命名空间,以便在键入时保存
importPackage (Packages.com.ti.debug.engine.scripting);
importPackage (Packages.com.ti.ccstudio.scripting.environment);
importPackage (Packages.java.lang);

//修改这些变量以匹配您的环境。 使用正斜杠
VAR ccs6InstallDir ="C:/ti/ccsv6;
VAR RTWorksDir ="/ccs_temp";
VAR TargetCCXMLfile = RTWorksDir +"/TMS570LS3137.ccxml";
VAR programToLoad = RTWorksDir +"/Test.out";
var logfile = RTWorksDir +"/log.xml";

//创建我们的脚本环境对象-这是主要入口点
//进入任何脚本和工厂,以创建其他可脚本服务器和会话
VAR 脚本= ScriptingEnvironment.instance();

//在当前目录中创建日志文件以记录脚本执行
script.traceBegin (logfile、ccs6InstallDir +"/ccs_base/scripting/examples/DebugServerExamples/DefaultStylesheet.xsl");

//设置控制台和日志的跟踪级别
script.traceSetConsoleLevel (TraceLevel 信息);
script.traceSetFileLevel (TraceLevel。all);

script.traceWrite ("开始脚本会话");

//获取调试服务器并启动调试会话
var debugServer = script.getServer ("DebugServer.1");
debugServer.setConfig("D:/RTRT/TestRealTime/targets/CCS61_TMS570LS3137/cmd/TMS570LS3137.ccxml");
debugServer.setConfig(TargetCCXMLfile);

/var debugSession=debugServer.openSession(".*");
/var debugSession=debugServer.openSession("Texas Instruments XDS100v2 USB Debug Probe/CortexR4");
var debugSession=debugServer.openSession("Blackhawk USB560-M 仿真器,20引脚 JTAG 电缆/CortexR4");

script.traceWrite ("连接目标");

//连接到 CPU
debugSession.target.connect();

script.traceWrite ("目标已连接");

//debugSession.expression.evaluate ('GEL_LoadGel ("ccs_temp/tms570ls3137.gel"));

debugSession.expression.evaluate ('GEL_LoadGel ("C:/ti/ccsv6/ccs_base/emulation/gel/tms570ls3137.gel)"');

//加载程序
script.traceWrite ("加载程序");

debugSession.memory.loadProgram (programToLoad);

script.traceWrite ("从 GEL 执行程序");

debugSession.expression.evaluate ("load_BP_report_file");

var privClose = debugSession.symbol.getAddress ("priv_close");

var ccs6End = false;

while (!ccs6End)

  if (debugSession.memory.readRegister ("PC")!=专用)
  {
    Thread.Sleep (2000);
  }
  其他
  {
    ccs6End = true;
  }

//Thread.Sleep (15000);

debugSession.breakpoint.add("exit.c",85);

script.traceWrite ("退出断点集");

//运行目标
debugSession.target.run();

script.traceWrite ("目标正在运行");

//全部完成
debugServer.stop();
debugServer.stop();

script.traceWrite ("结束脚本会话");

//停止记录并退出。
script.traceEnd();

根据我们的要求修改 GEL 文件(字体为粗体):

TMS570LS3137.GEL

/*                                                                           *//
/*(c) Texas Instruments 2006-2011、保留所有权利。                      *
/*                                                                           *//
/*                                                                           *//
/*文件:           TMS570LS3137.GEL                                       *
/*版本:       1.0                                                      */
/*                                                                           *//
/*注意:此 GEL 文件作为示例提供,可用于       */
TMS570LS3137      微控制器的//软件开发。 之前 */
/*      用法建议检查文件是否提供           了*/
/*      功能预期。                                              *
/*                                                                           *//
/*                                                                           *//

/*------------------ *
/*定义-内存映射说明符                                       */
#define FLASH  0
#define RAM    1.
define nEMIF  0
#define EMIF   1.

/*------------------ *
/*定义-文本格式指定符                                      */
#define 黑色  0
#define blue   1.
#define RED    2.

/*------------------ *
/*定义-内存开关                                               */
#define 已启动0
#define COMPl  1.

/*------------------ *
/*全局变量-默认内存映射                                     */
unsigned int MemoryMap =闪存;

/*------------------ *
/*全局变量-内存开关                                          */
unsigned int MemSwitchState = compl;

/*------------------ *
/*函数- startup()                                                      */
/*                                                                           *//
startup(){

}/* startup()*/

/*------------------ *
/*函数- OnResetDetected ()                                              */
/*                                                                           *//
OnResetDetected (){

   if (MemSwitchState == compl){
   
       memmap (闪存、EMIF);
       MemoryMap =闪存;
       GEL_TextOut ("\t 由于系统复位、闪存@地址0x0的内存映射设置\n"、、、、 );
   }
   
   if (MemSwitchState ==已启动)
    
       MemSwitchState == compl;
   }
/*------------------ *
/*函数- OnTargetConnect()                                              */
/*                                                                           *//
OnTargetConnect()

   if (MemoryMap ==闪存){
       memmap (闪存、EMIF);
       GEL_TextOut ("\t 闪存@地址0x0"、、、、、、的内存映射设置 );
   }    
   if (MemoryMap == RAM){
       memmap (RAM、EMIF);
       GEL_TextOut ("\tRAM 的内存映射设置@地址0x0。"、、、、 );
       GEL_TextOut ("\t 仅用于调试!"、、、、 );
   }   
}/* OnTargetConnect()*/

/******** /
menuitem "load TestRT Program";

INT RTRT_Mode = 0;

热菜单 load_BP_report_file (int nErrorCode、int bSymbolsOnly)

 int BREAKPTS_SET = 0;
 int 计数器= 0;  

 //GEL_Reset ();
 //GEL_Restart ();
 RTRTRT_Mode = 0;
 GEL_TextOut ("清除断点 priv_writeln \n");
 GEL_HWBreakPtDel (priv_writeln);
 GEL_TextOut ("清除断点 priv_close \n");
 GEL_HWBreakPtDel (priv_close);
 GEL_HWBreakPtReset ();
 //GEL_System ("del c:\\temp\\rtr.dat");
 //GEL_System ("del c:\\temp\\tempfile.txt");
 if (!BREAKPTS_SET)
 {
  GEL_TextOut ("设置断点\n");
  GEL_HWBreakPtAdd (priv_writeln);
  GEL_TextOut ("为 priv_writeln 设置断点\n");
  GEL_HWBreakPtAdd (priv_close);
  GEL_TextOut ("为 priv_close\n"设置断点);

  GEL_TextOut ("b -%x\n"、、、、 sizeof (atl_buffer));                                                        

  BREAKPTS_SET = 1;
  GEL_Run();
  RTRT_Mode = 1;  
  GEL_TextOut ("RTRT 模式设置为1\n");
   }
}  
 
OnHalt()

 GEL_TextOut ("OnHalt called n");
 GEL_TextOut ("PC -%x\n"、、、、 PC);
 //GEL_Run ();

 if (RTRT_Mode = 1)
 {
  if (pc ==priv_writeln)                                                      
  {    
   Int A;
   a= sizeof (atl_buffer);
   GEL_TextOut ("a -%x\n"、、、、 a);                                                        
        GEL_MemorySave (atl_buffer、0、a、"log.dat");   
        GEL_System ("type log.dat >>c:/temp/RTRT.dat);
   GEL_Run();
  }
  否则 if (PC =priv_close)
  {
   GEL_TextOut ("\nTestRT:程序正常执行\n");
   GEL_System ("echo Execution _Complete > c:/temp/tempFile.txt);
   GEL_Halt();
   RTRTRT_Mode = 0;
   
  }
  其他
  {
     GEL_Run();
  }

  
  }
 

热菜单 clear_RAM_buffer()

   /* 清除"atl_buffer"的 RAM 缓冲器*/
   GEL_MemoryFill (atl_buffer、0、0x0C00、0x00);
 GEL_TextOut ("RAM 缓冲器已清除\n");

hotmenu load_report_file()

   /*打开窗口以查看 RIO (结果)文件*/
         //GEL_OpenWindow ("TestRT Rio Data Window"、0);   
   
   /* RIO (结果)文件的内容*/
   /*数据的大小为6K,即6144字节("atl_buffer"的大小)*/
        // GEL_MemorySave (atl_buffer、1、sizeof (atl_buffer)、"c:/temp/Test.spt、1、1);
         GEL_TargetTextOut (ATL_buffer、0、6144、0、"TestRT Rio Data Window"、1);
                                                                         

hotmenu save_report_file (int nErrorCode、int bSymbolsOnly)

    Int A;

    a= sizeof (atl_buffer);
     GEL_MemorySave (atl_buffer、0、a、"log.dat");
   GEL_System ("type log.dat >> D:/MSS_TDR/temp/RTRT.dat");

/************* /

/*------------------ *
/*函数- memmap (memSel、extMem)                                         */
/*                                                                           *//
memmap (memSel、extMem){

   GEL_MapOff ();
   GEL_MapReset();  

   /*闪存/RAM 定义*/
   if (memSel ==闪存){

       /*闪存定义*/
       GEL_MapAdd (0x00000000、0、0x00300000、1、0); /*内部闪存()    */
       GEL_MapAddStr (0xF0400000、0、0x00060000、"R|AS2"、0); /*内部闪存 ECC   */        
       GEL_MapAdd (0x08000000、0、0x00040000、1、1); /*内部 RAM         */
       GEL_MapAdd (0x08400000、0、0x00040000、1、1); /*内部 RAM ECC     */
       GEL_MapAdd (0x20000000、0、0x00300000、1、0); /*镜像闪存       */        
       GEL_MapAdd (0xFE000000、0、0x01000000、1、1); /* CRC/PSA              */
   }

   if (memSel == RAM){

       /* RAM 定义*/
       GEL_MapAdd (0x00000000、0、0x00040000、1、1); /*内部 RAM         */
       GEL_MapAdd (0x00400000、0、0x00040000、1、1); /*内部 RAM ECC     */
       GEL_MapAdd (0x08000000、0、0x00300000、1、0); /*内部闪存()    */
       GEL_MapAddStr (0xF0400000、0、0x00060000、"R|AS2"、0); /*内部闪存 ECC   */        
       GEL_MapAdd (0x20000000、0、0x00300000、1、0); /*镜像闪存       */        
       GEL_MapAdd (0xFE000000、0、0x01000000、1、1); /* CRC/PSA              */
   }

   if (extMem =EMIF){

       GEL_MapAdd (0x60000000、0、0x10000000、1、1); /*外部异步存储器      */
       GEL_MapAdd (0x80000000、0、0x08000000、1、1); /*外部同步 SDRAM 内存      */
   }

 /*其它与闪存相关的内存*/
 GEL_MapAdd (0xF0200000、0、0x00010000、1、0); /* EEPROM      */
 GEL_MapAddStr (0xF0100000、0、0x00002000、"R|AS2"、0); /* EEPROM ECC     */
 GEL_MapAdd (0xF0000000、0、0x00004000、1、0); /*客户 OTP      */
 GEL_MapAddStr (0xF0040000、0、0x00000800、"R|AS2"、0); /*客户 OTP ECC   */
 GEL_MapAdd (0xF000E000、0、0x00001000、1、0); /*客户 OTP、EEPROM    */
 GEL_MapAddStr (0xF0041C00、0、0x00000400、"R|AS2"、0); /*客户 OTP、EEPROM ECC   */

 
   /*外设寄存器定义*/
   GEL_MapAdd (0xFFF7FC00、0、0x00000200、1、1); /* SPI5      - PS00        */
   GEL_MapAdd (0xFFF7FA00、0、0x00000200、1、1); /* SPI4      - PS01        */
   GEL_MapAdd (0xFFF7F800、0、0x00000200、1、1); /* SPI3      - PS01        */
   GEL_MapAdd (0xFFF7F600、0、0x00000200、1、1); /* SPI2      - PS02        */
   GEL_MapAdd (0xFFF7F400、0、0x00000200、1、1); /* MIBSPI1   - PS02        */
   GEL_MapAdd (0xFFF7E400、0、0x00000100、1、1); /* LIN       - PS06        */
   GEL_MapAdd (0xFFF7E500、0、0x00000100、1、1); /* SCI       - PS06        */
   GEL_MapAdd (0xFFF7E000、0、0x00000200、1、1); /* DCAN3     - PS07        */
   GEL_MapAdd (0xFFF7DE00、0、0x00000200、1、1); /* DCAN2     - PS08        */
   GEL_MapAdd (0xFFF7DC00、0、0x00000200、1、1); /* DCAN1     - PS08        */
   GEL_MapAdd (0xFFF7C800、0、0x00000800、1、1); /* Flexray   - PS12+PS13   */
   GEL_MapAdd (0xFFF7A000、0、0x00000200、1、1); /* Flexray TU - PS23        */
   GEL_MapAdd (0xFFF7D400、0、0x00000100、1、1); /* I2C       - PS10        */
   GEL_MapAdd (0xFFF7C200、0、0x00000200、1、1); /* MIBADC2   - PS15        */
   GEL_MapAdd (0xFFF7C000、0、0x00000200、1、1); /* MIBADC1   - PS15        */
   GEL_MapAdd (0xFFF7BC00、0、0x00000100、1、1); /* GIO       - PS16        */
   GEL_MapAdd (0xFFF7B800、0、0x00000100、1、1); /* NHET1     - PS17        */
   GEL_MapAdd (0xFFF7B900、0、0x00000100、1、1); /* NHET2     - PS17        */
   GEL_MapAdd (0xFFF7A400、0、0x00000100、1、1); /* HET TU    - PS22        */
   GEL_MapAdd (0xFFF7A500、0、0x00000100、1、1); /* HET TU2-PS22            */

   
   /*外设存储器*/
   GEL_MapAdd (0xFC520000、0、0x00002000、1、1); /* CPPI、以太网 RAM - PS05 */
   GEL_MapAdd (0xFF0A0000、0、0x00020000、1、1); /* MibSPI5 RAM   - PS05    */
   GEL_MapAdd (0xFF0C0000、0、0x00020000、1、1); /* MibSPI3 RAM   - PS06    */
   GEL_MapAdd (0xFF0E0000、0、0x00020000、1、1); /* MibSPI1 RAM   - PS07    */
   GEL_MapAdd (0xFF1A0000、0、0x00020000、1、1); /* CAN3 RAM      - PS13    */
   GEL_MapAdd (0xFF1C0000、0、0x00020000、1、1); /* CAN2 RAM      - PS14    */
   GEL_MapAdd (0xFF1E0000、0、0x00020000、1、1); /* CAN1 RAM      - PS15    */
   GEL_MapAdd (0xFF3A0000、0、0x00020000、1、1); /* MIBADC2 RAM   - PS29    */
   GEL_MapAdd (0xFF3E0000、0、0x00020000、1、1); /* MIBADC1 RAM   - PS31    */
   GEL_MapAdd (0xFF440000、0、0x00020000、1、1); /* NHET2 RAM      - PS34    */
   GEL_MapAdd (0xFF460000、0、0x00020000、1、1); /* NHET1 RAM      - PS35    */
   GEL_MapAdd (0xFF4C0000、0、0x00020000、1、1); /* HET2 TU RAM    - PS38    */
   GEL_MapAdd (0xFF4E0000、0、0x00020000、1、1); /* HET1 TU RAM    - PS39    */
   GEL_MapAdd (0xFF50000、0、0x00020000、1、1); /* Flexray TU RAM - PS40    */

   /*系统外设寄存器*/
   GEL_MapAdd (0xFE000000、0、0x01000000、1、1); /* CRC                      */
   GEL_MapAdd (0xFFA00000、0、0x00001000、1、1); /* CoreSight 调试 ROM      *
   GEL_MapAdd (0xFFA01000、0、0x00001000、1、1); /* R4调试寄存器        */
   GEL_MapAdd (0xFFA02000、0、0x00001000、1、1); /* ETM-R4寄存器          */
   GEL_MapAdd (0xFFA03000、0、0x00001000、1、1); /* CoreSight TPIU 寄存器  */
   GEL_MapAdd (0xFFA04000、0、0x00001000、1、1); /* POM 寄存器             */
   GEL_MapAdd (0xFFF80000、0、0x00001000、1、1); /* DMA RAM                  */
   GEL_MapAdd (0xFFF82000、0、0x00001000、1、1); /* VIM RAM                  */
   GEL_MapAdd (0xFFF83000、0、0x00001000、1、1); /* RTP RAM                  */
   GEL_MapAdd (0xFFF87000、0、0x00001000、1、1); /*闪存包装程序寄存器   */
   GEL_MapAdd (0xFFF8C000、0、0x00001000、1、1); /*熔丝组控制器    */
   GEL_MapAdd (0xFFFFFF0000、0、0x00000200、1、1); /*电源管理寄存器*/
   GEL_MapAdd (0xFFFFFFE000、0、0x00000100、1、1); /* PCR 寄存器             */
   GEL_MapAdd (0xFFFFFFE100、0、0x00000100、1、1); /*系统2寄存器        */
   GEL_MapAdd (0xFFFFFFE400、0、0x00000200、1、1); /* PBIST                    */
   GEL_MapAdd (0xFFFFFFE600、0、0x00000100、1、1); /* STC                      */    
   GEL_MapAdd (0xFFFFFFEA00、0、0x00000200、1、1); /* IOMM                     */    
   GEL_MapAdd (0xFFFFFFEC00、0、0x00000100、1、1); /* DCC1                     */    
   GEL_MapAdd (0xFFFFFF000、0、0x00000400、1、1); /* DMA                      */
   GEL_MapAdd (0xFFFFFF400、0、0x00000100、1、1); /* DCC2                      */    
   GEL_MapAdd (0xFFFFFF500、0、0x00000100、1、1); /* ESM                      */
 GEL_MapAdd (0xFFFFFF600、0、0x00000100、1、1); /* CCMR4                    */
 GEL_MapAdd (0xFFFFFF700、0、0x00000100、1、1); /* DMM                      */
 GEL_MapAdd (0xFFFFFF800、0、0x00000100、1、1); /* RAM ECC 偶             数*/
 GEL_MapAdd (0xFFFFFF900、0、0x00000100、1、1); /* RAM ECC 奇数              */
 GEL_MapAdd (0xFFFFFF00、0、0x00000100、1、1); /* RTP                      */
   GEL_MapAdd (0xFFFFFF00、0、0x00000100、1、1); /* RTI 寄存器             */
   GEL_MapAdd (0xFFFFFFFD00、0、0x00000100、1、1); /* VIM 奇偶校验               */
   GEL_MapAdd (0xFFFFFF00、0、0x00000100、1、1); /* VIM 寄存器             */
   GEL_MapAdd (0xFFFFFF00、0、0x00000100、1、1); /*系统寄存器          */
   
   /* EMIF/以太网寄存器*/
   GEL_MapAdd (0xFCFFE800、0、0x00000100、1、1); /* EMIF                     */
   GEL_MapAdd (0xFCF78000、0、0x00000400、1、1); /* CPGMAC 从属设备             */
   GEL_MapAdd (0xFCF78800、0、0x00000100、1、1); /* CPGMACSS 包装程序         */
   GEL_MapAdd (0xFCF78900、0、0x00000100、1、1); /*以太网 MDIO            */
   
   GEL_MapOn();

}/*函数- memmap (memSel、extMem)*/

/*------------------ *
/*函数- swap_mem (memSel)                                               */
/*                                                                           *//
swap_mem (memSel){
   
   GEL_TextOut ("注意:\n\t 将切换设备的闪存/RAM 存储器地址。");
   GEL_TextOut ("\tat 此例程的末尾将重置器件。");
   GEL_TextOut ("\t 这可能会导致弹出消息、指出错误!");
   GEL_TextOut ("\tJust 在消息出现后重新连接。");

   MemSwitchState =已启动;
   
   if (memSel == RAM){

       memmap (RAM、EMIF);
       MemoryMap = RAM;
       *(int *) 0xffffffffc4 = 0x050505;
       *(int *) 0xffffffcc = 0x00000001;
       *(int *) 0xffffffcc = 0x00000000;
   }

   if (memSel ==闪存){

       memmap (闪存、EMIF);
       MemoryMap =闪存;
       *(int *) 0xffffffffc4 = 0x0A0A0A0A;
       *(int *) 0xffffffcc = 0x00000001;
       *(int *) 0xffffffcc = 0x00000000;
   }
   
   MemSwitchState = compl;
   
   GEL_TextOut ("\t 内存交换完成。");
   GEL_TextOut ("\TIN case 弹出消息、已重新连接到器件。");
   
   
}/* swap_mem (memSel)*/

/*------------------ *
/*菜单项-"TMS570LS3137内存映射设置"                               */
/*                                                                           *//
菜单项"TMS570LS3137内存映射设置";

   热菜单 CCS_MemMap_flash_at_0x0 (){

       memmap (闪存、EMIF);
       GEL_TextOut ("\t 闪存@地址0x0"、、、、、、的内存映射设置 );
       
   }

   热菜单 CCS_MemMap_RAM_at_0x0 (){
   
       memmap (RAM、EMIF);
       GEL_TextOut ("\tRAM 的内存映射设置@地址0x0。"、、、、 );
       GEL_TextOut ("\t 仅用于调试!"、、、、 );

   }

/*------------------ *
/*菜单项-"TMS570LS3137内存开关"                                  */
/*                                                                           *//
菜单项"TMS570LS3137内存开关";

   热菜单 Target_Flash_TO_0x0 (){

       swap_mem (FLASH);
   }

   热菜单 Target_RAM_TO_0x0 (){
   
       swap_mem (RAM);
   }

我的错误日志文件"CortexR4:GEL 输出:PC - 0x00005A20 "无法通过 GEL 文件读取:

CortexR4:GEL 输出:清除断点 priv_writeln

CortexR4:GEL 输出:PC - 0x00005A20

CortexR4:GEL 输出:清除断点 priv_close

CortexR4:GEL 输出:设置断点

CortexR4:GEL 输出:为 priv_writeln 设置断点

CortexR4:GEL 输出:为 priv_close 设置断点

CortexR4:GEL 输出:B - 0x00000C00

CortexR4:GEL 输出:RTRT 模式被设定为1
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0
CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
CortexR4:GEL 输出:OnHalt 被调用

CortexR4:GEL 输出:PC - 0x000000C0

CortexR4:GEL 输出:A - 0x00000C00
CortexR4:GEL_System:键入 log.dat >> c:/temp/RTRT.dat
CortexR4:GEL_System:
严重:无法读取寄存器 PC:执行状态阻止访问
严重:评估"PC"时出错:无法读取寄存器 PC:执行状态阻止访问
org.moilla.javascript:WrappedException:wrapped com.ti.ccstudio。scripting.environment.ScriptingException:Error evaling "PC":Could not read register PC: execution state prevented access (D:\RTRTRT\TestRealTime\Targets\CCS61_TMS570LS3137\cmd:InvokeCCS.js#61)
 在 org.mozilla.javascript:context.throwAsScriptRuntimeEx (context.java:1693)

 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好!

    在修改 GEL 文件之前是否存在任何问题(Java 脚本和 GEL 脚本)?

    此致、