This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/EK-TM4C123GXL:EK-TM4C123GXL

Guru**** 2590120 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/572874/ccs-ek-tm4c123gxl-ek-tm4c123gxl

器件型号:EK-TM4C123GXL

工具/软件:Code Composer Studio

您好!  

我不熟悉 Tiva 并从事一个个人项目、该项目需要同时测量6个电路的频率。 我的电路由 PWM 输入(我还需要测量该输入)以及生成频率(最大1000Hz)的5个电路运行。 我需要在两次后续测量之间提供15秒的时间延迟。 它必须是表格格式、因为我需要记录输出频率、它将运行100次迭代。
我无法构建同时测量6个可用频率的代码。 有人可以帮我解决这个问题吗?