This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMDS243GPEVM:尝试刷写应用程序时出错

Guru**** 2556080 points
Other Parts Discussed in Thread: UNIFLASH

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1179294/tmds243gpevm-error-when-trying-to-flash-an-application

器件型号:TMDS243GPEVM

大家好、

我正在尝试 刷写 以太网/IP 适配器示例 并得到以下错误:

[INFO] Parsing config file ... SUCCESS. Found 3 command(s) !!!

[INFO] Executing command 1 of 3 ...
[INFO] Found flash writer ... sending K:/Pool/decicher/ti/mcu_plus_sdk_am243x_08_03_00_18/tools/boot/sbl_prebuilt/am243x-lp/sbl_uart.release.tiimage
[INFO] Sent flashwriter K:/Pool/decicher/ti/mcu_plus_sdk_am243x_08_03_00_18/tools/boot/sbl_prebuilt/am243x-lp/sbl_uart.release.tiimage of size 257820 bytes in 26.14s.

[INFO] Executing command 2 of 3 ...
[INFO] Command arguments : --file=K:/Pool/decicher/ti/mcu_plus_sdk_am243x_08_03_00_18/tools/boot/sbl_prebuilt/am243x-lp/sbl_ospi.release.tiimage --operation=flash --flash-offset=0x0000
Sent K:/Pool/decicher/ti/mcu_plus_sdk_am243x_08_03_00_18/tools/boot/sbl_prebuilt/am243x-lp/sbl_ospi.release.tiimage of size 297589 bytes in 31.21s.
[ERROR] Incorrect magic number in Response Header !!!
[INFO] Executing command 3 of 3 ...
[INFO] Command arguments : --file=C:/Users/decicher/workspace_v12/ethernetip_adapter_mii_demo_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Release/ethernetip_adapter_mii_demo_am243x-evm_r5fss0-0_freertos_ti-arm-clang.appimage --operation=flash --flash-offset=0x80000

或通过终端:

PS K:\Pool\decicher\ti\mcu_plus_sdk_am243x_08_03_00_18\tools\boot> python uart_uniflash.py -p COM6 --cfg=C:/Users/decicher/Desktop/FLASH_sbl_ospi.cfg

Parsing config file ...
Parsing config file ... SUCCESS. Found 3 command(s) !!!

Executing command 1 of 3 ...
Found flash writer ... sending sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage
Sent flashwriter sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage of size 291781 bytes in 28.06s.

Executing command 2 of 3 ...
Command arguments : --file=sbl_prebuilt/am243x-lp/sbl_ospi.release.tiimage --operation=flash --flash-offset=0x0
Sending sbl_prebuilt/am243x-lp/sbl_ospi.release.tiimage:   0%|             | 2/297621 [01:50<9102:17:30, 110.10s/bytes]
[ERROR] XMODEM send failed, no response OR incorrect response from EVM OR cancelled by user,
Power cycle EVM and run this script again !!!

有什么想法我做了什么错?

BR

Erik

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Erik、

    在 GUI 中、您应该放入的第一个文件应为"SBL_prebuilt/am243x-LP/SBL_UART_uniflash.release.tiimage"。 您使用的是"SBL_UART.release.tiimage"

    此致、

    Ming