This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS570LC4357-EP:tms570lc4357-EP

Guru**** 2784315 points

Other Parts Discussed in Thread: TMS570LC4357-EP, HALCOGEN

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1179203/tms570lc4357-ep-tms570lc4357-ep

器件型号:TMS570LC4357-EP
主题中讨论的其他器件: HALCOGEN

大家好、TI 社区。 我目前正在使用 Hercules 硬件开发套件(TMS570LC4357-EP)

我无法使用 SPI 协议从外部硬件(数据密钥)读取数据、但我测试了 HALCogen 软件中提供的 MibSPI 示例代码(包括环回和 DMA)、并看到了内部寄存器之间的数据传输、这种传输方式非常完美。


我使用下面列出的 SPI 引脚组合连接外部硬件(数据密钥):

J-10 SPI2扩展连接器-

CLK 的引脚64

CS0-引脚63

SOMI 的引脚59

SIMO 的引脚61

我已经尝试过下面附加的示例 SPI 代码、数据传输在内部工作得非常完美。 但是、我需要使用之前指定的 SPI2引脚排列来接收来自外部硬件(数据密钥)的数据的代码、在这种排列中、我的 HDK 用作主器件、而外部硬件(数据密钥)用作从器件。

/** @file HL_sys_main.c 
*   @brief Application main file
*   @date 11-Dec-2018
*   @version 04.07.01
*
*   This file contains an empty main function,
*   which can be used for the application.
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com  
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* USER CODE END */

/* Include Files */

#include "HL_sys_common.h"

/* USER CODE BEGIN (1) */
#include "HL_sys_core.h"
#include "HL_sys_dma.h"
#include "HL_spi.h"
//#include "HL_sci.h"

//#include <ra_dbg_level.h>
//#include <ra_stdio.h>
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
#define WITH_DMA    0
#define LOOP_BACK   1

#define D_SIZE        128

#define SPI_MASTER    spiREG3

#define MASTER_SPI_TX_ADDR ((uint32_t)(&(spiREG3->DAT1)) + 2)
#define MASTER_SPI_RX_ADDR  ((uint32_t)(&(spiREG3->BUF))  + 2)

uint16 tx_data[D_SIZE] = {0};
uint16 rx_data[D_SIZE] = {0};

unsigned int MASTER_SPI_DMA_FTCFlag  = 0;
unsigned int MASTER_SPI_DMA_HBCFlag  = 0;
unsigned int MASTER_SPI_DMA_BTCFlag  = 0;

g_dmaCTRL g_dmaCTRLPKT_RX, g_dmaCTRLPKT_TX;

static void loadDataPattern       (uint32 psize, uint16* pptr);

#if (WITH_DMA)
static void dmaConfigCtrlTxPacket (uint32 sadd,  uint32 dadd, uint16 ElmntCnt, uint16 FrameCnt);
static void dmaConfigCtrlRxPacket (uint32 sadd,  uint32 dadd, uint16 ElmntCnt, uint16 FrameCnt);
#endif

/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */

    _enable_IRQ_interrupt_();

    loadDataPattern(D_SIZE,&tx_data[0]);

    spiInit();
#if (LOOP_BACK)
    spiEnableLoopback(SPI_MASTER, Analog_Lbk);
#endif

#if (WITH_DMA)

    /* - setting the dma channel to trigger on h/w request */
    dmaSetChEnable(DMA_CH0, DMA_HW);
    dmaSetChEnable(DMA_CH1, DMA_HW);

    dmaReqAssign(DMA_CH0, DMA_REQ14);     //SPI3 RX
    dmaReqAssign(DMA_CH1, DMA_REQ15);    //SPI3 TX

    dmaConfigCtrlRxPacket(MASTER_SPI_RX_ADDR, (uint32)rx_data, 1, D_SIZE); //TBC
    dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT_RX);

    /* - setting dma control packets */
    dmaConfigCtrlTxPacket((uint32)tx_data, MASTER_SPI_TX_ADDR, 1, D_SIZE); //TBC
    dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT_TX);

    dmaEnable();

    SPI_MASTER->INT0 |= (0x1 << 16);  //SPI_DMAREQ; Enable DMA REQ only after setting the SPIEN bit to 1.
#else
        spiDAT1_t dataconfig3_t;
        dataconfig3_t.CS_HOLD = FALSE;
        dataconfig3_t.WDEL = TRUE;
        dataconfig3_t.DFSEL = SPI_FMT_0;
        dataconfig3_t.CSNR = 0xFE;

        spiTransmitAndReceiveData(SPI_MASTER, &dataconfig3_t, D_SIZE, tx_data,rx_data);
#endif

    while(1);
/* USER CODE END */

    return 0;
}


/* USER CODE BEGIN (4) */

void dmaGroupANotification(dmaInterrupt_t inttype, uint32 channel)
{
    if (inttype == FTC)
    {
        MASTER_SPI_DMA_FTCFlag = 1;
    }
    else if (inttype == HBC)
    {
        MASTER_SPI_DMA_HBCFlag = 1;
    }
    else if (inttype == BTC)
    {
        MASTER_SPI_DMA_BTCFlag = 1;
    }
}

static void loadDataPattern(uint32 psize, uint16* pptr)
{
    int i;
    for(i=0;i<psize;i++)
    {
        pptr[i] = i;
    }
 }

#if (WITH_DMA)
static void dmaConfigCtrlTxPacket (uint32 sadd, uint32 dadd, uint16 ElmntCnt, uint16 FrameCnt)
{
    /* - configuring dma control packets   */
    g_dmaCTRLPKT_TX.SADD      = sadd;
    g_dmaCTRLPKT_TX.DADD      = dadd;
    g_dmaCTRLPKT_TX.CHCTRL    = 0;
    g_dmaCTRLPKT_TX.FRCNT     = FrameCnt;
    g_dmaCTRLPKT_TX.ELCNT     = ElmntCnt;
    g_dmaCTRLPKT_TX.ELDOFFSET = 0;
    g_dmaCTRLPKT_TX.ELSOFFSET = 0;
    g_dmaCTRLPKT_TX.FRDOFFSET = 0;
    g_dmaCTRLPKT_TX.FRSOFFSET = 0;
    g_dmaCTRLPKT_TX.PORTASGN  = PORTA_READ_PORTB_WRITE;
    g_dmaCTRLPKT_TX.RDSIZE    = ACCESS_16_BIT;
    g_dmaCTRLPKT_TX.WRSIZE    = ACCESS_16_BIT;
    g_dmaCTRLPKT_TX.TTYPE     = FRAME_TRANSFER;
    g_dmaCTRLPKT_TX.ADDMODERD = ADDR_INC1;
    g_dmaCTRLPKT_TX.ADDMODEWR = ADDR_FIXED;
    g_dmaCTRLPKT_TX.AUTOINIT  = AUTOINIT_OFF;
}

static void dmaConfigCtrlRxPacket (uint32 sadd, uint32 dadd, uint16 ElmntCnt, uint16 FrameCnt)
{
    /* - configuring dma control packets   */
    g_dmaCTRLPKT_RX.SADD      = sadd;
    g_dmaCTRLPKT_RX.DADD      = dadd;
    g_dmaCTRLPKT_RX.CHCTRL    = 0;
    g_dmaCTRLPKT_RX.FRCNT     = FrameCnt;
    g_dmaCTRLPKT_RX.ELCNT     = ElmntCnt;
    g_dmaCTRLPKT_RX.ELDOFFSET = 0;
    g_dmaCTRLPKT_RX.ELSOFFSET = 0;
    g_dmaCTRLPKT_RX.FRDOFFSET = 0;
    g_dmaCTRLPKT_RX.FRSOFFSET = 0;
    g_dmaCTRLPKT_RX.PORTASGN  = PORTB_READ_PORTA_WRITE;
    g_dmaCTRLPKT_RX.RDSIZE    = ACCESS_16_BIT;
    g_dmaCTRLPKT_RX.WRSIZE    = ACCESS_16_BIT;
    g_dmaCTRLPKT_RX.TTYPE     = FRAME_TRANSFER;
    g_dmaCTRLPKT_RX.ADDMODERD = ADDR_FIXED;
    g_dmaCTRLPKT_RX.ADDMODEWR = ADDR_INC1;
    g_dmaCTRLPKT_RX.AUTOINIT  = AUTOINIT_OFF;
}
#endif
/* USER CODE END */

1) 1)请查看上述参考并提交用于 HDK 板和外部硬件(数据密钥)之间数据交换的代码。

2) 2)如何以及在何处调整 SPI 时钟频率?

3)当我探索时钟时、我能够在探测 SPI 时钟引脚时提取50Hz 时钟频率、但我还看到 CS0、SOMI 和 SIMO 引脚上的时钟频率相同。