This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS570LS1224:TMS570 MIBSPI 从器件配置问题

Guru**** 2760505 points

Other Parts Discussed in Thread: HALCOGEN

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1164391/tms570ls1224-tms570-mibspi-slave-configuration-issue

器件型号:TMS570LS1224
主题中讨论的其他器件:HALCOGEN

大家好、

我正在处理某些需要为 SPI 从设备配置 TMS570的项目

MIBSPI1通道配置为 SPI 从器件。

MIB 缓冲区配置为128字节。  TMS570能够接收数据。

环境:主器件以500ms 的周期连续发送26字节的数据。

问题说明:

 它应该接收26个字节的数据、但它在开头仅接收10到14个字节。

一旦多缓冲器 RAM 已满、从下一次它能够接收26个字节。

我不确定为什么它会在开始正确接收26个字节后等待第一次填充整个 MIB RX 缓冲区。

在缓冲区被填满之前、每次只接收10到14个字节。  

因此、我必须等到缓冲区被填满才能获得正确的数据。 是否有人遇到与 SPI 从器件类似的问题? 请提出一些想法。

我要在此处附加 SPI 代码。 它是由 Halcogen 生成的、我对它做了一些更改。

/** @file mibspi.c
*   @brief MIBSPI Driver Implementation File
*   @date 11-Dec-2018
*   @version 04.07.01
*
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com 
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* USER CODE END */

#include "mibspi.h"
#include "sys_vim.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */

/** @fn void mibspiInit(void)
*   @brief Initializes the MIBSPI Driver
*
*   This function initializes the MIBSPI module.
*/
/* SourceId : MIBSPI_SourceId_001 */
/* DesignId : MIBSPI_DesignId_001 */
/* Requirements : HL_SR153 */
uint8 gdataspi[40];
void mibspiInit(void)
{
uint32 i ;
uint8 k;

/* USER CODE BEGIN (2) */
/* USER CODE END */


    /** @b initialize @b MIBSPI1 */

    /** bring MIBSPI out of reset */
    mibspiREG1->GCR0 = 0U;
    mibspiREG1->GCR0 = 1U;

    /** enable MIBSPI1 multibuffered mode and enable buffer RAM */
    mibspiREG1->MIBSPIE = (mibspiREG1->MIBSPIE & 0xFFFFFFFEU) | 1U;

    /** MIBSPI1 master mode and clock configuration */
    mibspiREG1->GCR1 = (mibspiREG1->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)0U << 1U)  /* CLOKMOD */
                  | 0U);  /* MASTER */

    /** MIBSPI1 enable pin configuration */
    mibspiREG1->INT0 = (mibspiREG1->INT0 & 0xFEFFFFFFU) | (uint32)((uint32)0U << 24U);  /* ENABLE HIGHZ */

    /** - Delays */
    mibspiREG1->DELAY = (uint32)((uint32)0U << 24U)  /* C2TDELAY */
                      | (uint32)((uint32)0U << 16U)  /* T2CDELAY */
                      | (uint32)((uint32)0U << 8U)   /* T2EDELAY */
                      | (uint32)((uint32)0U << 0U);  /* C2EDELAY */

    /** - Data Format 0 */
    mibspiREG1->FMT0 = (uint32)((uint32)0U << 24U)  /* wdelay */
                     | (uint32)((uint32)0U << 23U)  /* parity Polarity */
                     | (uint32)((uint32)0U << 22U)  /* parity enable */
                     | (uint32)((uint32)0U << 21U)  /* wait on enable */
                     | (uint32)((uint32)0U << 20U)  /* shift direction */
                     | (uint32)((uint32)1U << 17U)  /* clock polarity */
                     | (uint32)((uint32)0U << 16U)  /* clock phase */
                     | (uint32)((uint32)19U << 8U)  /* baudrate prescale */
                     | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 1 */
    mibspiREG1->FMT1 = (uint32)((uint32)0U << 24U)  /* wdelay */
                     | (uint32)((uint32)0U << 23U)  /* parity Polarity */
                     | (uint32)((uint32)0U << 22U)  /* parity enable */
                     | (uint32)((uint32)0U << 21U)  /* wait on enable */
                     | (uint32)((uint32)0U << 20U)  /* shift direction */
                     | (uint32)((uint32)0U << 17U)  /* clock polarity */
                     | (uint32)((uint32)1U << 16U)  /* clock phase */
                     | (uint32)((uint32)19U << 8U)  /* baudrate prescale */
                     | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 2 */
    mibspiREG1->FMT2 = (uint32)((uint32)0U << 24U)  /* wdelay */
                     | (uint32)((uint32)0U << 23U)  /* parity Polarity */
                     | (uint32)((uint32)0U << 22U)  /* parity enable */
                     | (uint32)((uint32)0U << 21U)  /* wait on enable */
                     | (uint32)((uint32)0U << 20U)  /* shift direction */
                     | (uint32)((uint32)0U << 17U)  /* clock polarity */
                     | (uint32)((uint32)0U << 16U)  /* clock phase */
                     | (uint32)((uint32)0U << 8U)  /* baudrate prescale */
                     | (uint32)((uint32)0U << 0U); /* data word length */

    /** - Data Format 3 */
    mibspiREG1->FMT3 = (uint32)((uint32)0U << 24U)  /* wdelay */
                     | (uint32)((uint32)0U << 23U)  /* parity Polarity */
                     | (uint32)((uint32)0U << 22U)  /* parity enable */
                     | (uint32)((uint32)0U << 21U)  /* wait on enable */
                     | (uint32)((uint32)0U << 20U)  /* shift direction */
                     | (uint32)((uint32)0U << 17U)  /* clock polarity */
                     | (uint32)((uint32)0U << 16U)  /* clock phase */
                     | (uint32)((uint32)0U << 8U)  /* baudrate prescale */
                     | (uint32)((uint32)0U << 0U); /* data word length */

    /** - Default Chip Select */
    mibspiREG1->DEF = (uint32)(0xFFU);

    /** - wait for buffer initialization complete before accessing MibSPI registers */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while ((mibspiREG1->FLG & 0x01000000U) != 0U)
    {
    } /* Wait */

    /** enable MIBSPI RAM Parity */
    mibspiREG1->UERRCTRL = (mibspiREG1->UERRCTRL & 0xFFFFFFF0U) | (0x00000005U);

    /** - initialize transfer groups */
    mibspiREG1->TGCTRL[0U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)0U << 8U);  /* start buffer */

    mibspiREG1->TGCTRL[1U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)128U << 8U);  /* start buffer */
#if 0
    mibspiREG1->TGCTRL[2U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)(8U+0U) << 8U);  /* start buffer */

    mibspiREG1->TGCTRL[3U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)(8U+0U+0U) << 8U);  /* start buffer */

    mibspiREG1->TGCTRL[4U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)(8U+0U+0U+0U) << 8U);  /* start buffer */

    mibspiREG1->TGCTRL[5U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)(8U+0U+0U+0U+0U) << 8U);  /* start buffer */

    mibspiREG1->TGCTRL[6U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)(8U+0U+0U+0U+0U+0U) << 8U);  /* start buffer */

    mibspiREG1->TGCTRL[7U] = (uint32)((uint32)1U << 30U)  /* oneshot */
                           | (uint32)((uint32)0U << 29U)  /* pcurrent reset */
                           | (uint32)((uint32)TRG_ALWAYS << 20U)  /* trigger event */
                           | (uint32)((uint32)TRG_DISABLED << 16U)  /* trigger source */
                           | (uint32)((uint32)(8U+0U+0U+0U+0U+0U+0U) << 8U);  /* start buffer */
#endif

    mibspiREG1->TGCTRL[1U] = (uint32)(128U+0U+0U+0U+0U+0U+0U+0U) << 8U;

    mibspiREG1->LTGPEND = (mibspiREG1->LTGPEND & 0xFFFF00FFU) | (uint32)((uint32)((128U+0U+0U+0U+0U+0U+0U+0U)-1U) << 8U);

    /** - initialize buffer ram */
    {
        i = 0U;

#if (8U > 0U)
        {

#if (8U > 1U)

            while (i < (128U-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)1U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_1)) & (uint16)0x00FFU);  /* chip select */
                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)1U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_1)) & (uint16)0x00FFU);  /* chip select */


            i++;
        }
#endif


#if (0U > 0U)
        {

#if (8U > 1U)

            while (i < ((64U+8U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)3U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)1U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)1U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)1U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
                                          /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_1)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)3U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)1U << 12U) /* chip select hold */
                                      | (uint16)((uint16)1U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
                                          /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_1)) & (uint16)0x00FFU);  /* chip select */

            i++;
        }
#endif

#if (0U > 0U)
        {

#if (0U > 1U)

            while (i < ((8U+0U+0U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)0U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_2)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)0U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_2)) & (uint16)0x00FFU);  /* chip select */

            i++;
        }
#endif

#if (0U > 0U)
        {

#if (0U > 1U)

            while (i < ((8U+0U+0U+0U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)0U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_3)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)0U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_3)) & (uint16)0x00FFU);  /* chip select */

            i++;
        }
#endif

#if (0U > 0U)
        {

#if (0U > 1U)

            while (i < ((8U+0U+0U+0U+0U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)0U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_4)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)0U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_4)) & (uint16)0x00FFU);  /* chip select */

            i++;
        }
#endif

#if (0U > 0U)
        {

#if (0U > 1U)

            while (i < ((8U+0U+0U+0U+0U+0U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)0U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_5)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)0U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_5)) & (uint16)0x00FFU);  /* chip select */

            i++;
        }
#endif

#if (0U > 0U)
        {

#if (0U > 1U)

            while (i < ((8U+0U+0U+0U+0U+0U+0U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)0U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_6)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)0U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_6)) & (uint16)0x00FFU);  /* chip select */

            i++;
        }
#endif

#if (0U > 0U)
        {

#if (0U > 1U)

            while (i < ((8U+0U+0U+0U+0U+0U+0U+0U)-1U))
            {
                mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                          | (uint16)((uint16)0U << 12U)  /* chip select hold */
                                          | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                          | (uint16)((uint16)0U << 11U)  /* lock transmission */
                                          | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                          | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_7)) & (uint16)0x00FFU);  /* chip select */

                i++;
            }
#endif
            mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U)  /* buffer mode */
                                      | (uint16)((uint16)0U << 12U) /* chip select hold */
                                      | (uint16)((uint16)0U << 10U)  /* enable WDELAY */
                                      | (uint16)((uint16)0U << 8U)  /* data format */
										  /*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
                                      | ((uint16)(~((uint16)0xFFU ^ (uint16)CS_7)) & (uint16)0x00FFU);  /* chip select */
            i++;
        }
#endif
    }

    /** - set interrupt levels */
    mibspiREG1->LVL = (uint32)((uint32)0U << 9U)  /* TXINT */
                    | (uint32)((uint32)0U << 8U)  /* RXINT */
                    | (uint32)((uint32)0U << 6U)  /* OVRNINT */
                    | (uint32)((uint32)0U << 4U)  /* BITERR */
                    | (uint32)((uint32)0U << 3U)  /* DESYNC */
                    | (uint32)((uint32)0U << 2U)  /* PARERR */
                    | (uint32)((uint32)0U << 1U)  /* TIMEOUT */
                    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** - clear any pending interrupts */
    mibspiREG1->FLG |= 0xFFFFU;

    /** - enable interrupts */
    mibspiREG1->INT0 = (mibspiREG1->INT0 & 0xFFFF0000U)
                     | (uint32)((uint32)0U << 9U)  /* TXINT */
                     | (uint32)((uint32)0U << 8U)  /* RXINT */
                     | (uint32)((uint32)0U << 6U)  /* OVRNINT */
                     | (uint32)((uint32)0U << 4U)  /* BITERR */
                     | (uint32)((uint32)0U << 3U)  /* DESYNC */
                     | (uint32)((uint32)0U << 2U)  /* PARERR */
                     | (uint32)((uint32)0U << 1U)  /* TIMEOUT */
                     | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** @b initialize @b MIBSPI1 @b Port */

    /** - MIBSPI1 Port output values */
    mibspiREG1->PC3 = (uint32)((uint32)1U << 0U)  /* SCS[0] */
                    | (uint32)((uint32)0U << 1U)  /* SCS[1] */
                    | (uint32)((uint32)1U << 2U)  /* SCS[2] */
                    | (uint32)((uint32)1U << 3U)  /* SCS[3] */
                    | (uint32)((uint32)1U << 4U)  /* SCS[4] */
                    | (uint32)((uint32)1U << 5U)  /* SCS[5] */
                    | (uint32)((uint32)0U << 8U)  /* ENA */
                    | (uint32)((uint32)0U << 9U)  /* CLK */
                    | (uint32)((uint32)0U << 10U)  /* SIMO[0] */
                    | (uint32)((uint32)0U << 11U)  /* SOMI[0] */
                    | (uint32)((uint32)0U << 17U)  /* SIMO[1] */
                    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /** - MIBSPI1 Port direction */
    mibspiREG1->PC1 = (uint32)((uint32)1U << 0U)  /* SCS[0] */
                    | (uint32)((uint32)0U << 1U)  /* SCS[1] */
                    | (uint32)((uint32)1U << 2U)  /* SCS[2] */
                    | (uint32)((uint32)1U << 3U)  /* SCS[3] */
                    | (uint32)((uint32)1U << 4U)  /* SCS[4] */
                    | (uint32)((uint32)1U << 5U)  /* SCS[5] */
                    | (uint32)((uint32)0U << 8U)  /* ENA */
                    | (uint32)((uint32)0U << 9U)  /* CLK */
                    | (uint32)((uint32)0U << 10U)  /* SIMO[0] */
                    | (uint32)((uint32)1U << 11U)  /* SOMI[0] */
                    | (uint32)((uint32)0U << 16U)  /* SIMO[1] */
                    | (uint32)((uint32)0U << 24U); /* SOMI[1] */

    /** - MIBSPI1 Port open drain enable */
    mibspiREG1->PC6 = (uint32)((uint32)1U << 0U)  /* SCS[0] */
                    | (uint32)((uint32)1U << 1U)  /* SCS[1] */
                    | (uint32)((uint32)1U << 2U)  /* SCS[2] */
                    | (uint32)((uint32)1U << 3U)  /* SCS[3] */
                    | (uint32)((uint32)1U << 4U)  /* SCS[4] */
                    | (uint32)((uint32)1U << 5U)  /* SCS[5] */
                    | (uint32)((uint32)1U << 8U)  /* ENA */
                    | (uint32)((uint32)1U << 9U)  /* CLK */
                    | (uint32)((uint32)1U << 10U)  /* SIMO[0] */
                    | (uint32)((uint32)1U << 11U)  /* SOMI[0] */
                    | (uint32)((uint32)1U << 17U)  /* SIMO[1] */
                    | (uint32)((uint32)1U << 25U); /* SOMI[1] */

    /** - MIBSPI1 Port pullup / pulldown selection */
    mibspiREG1->PC8 = (uint32)((uint32)0U << 0U)  /* SCS[0] */
                    | (uint32)((uint32)0U << 1U)  /* SCS[1] */
                    | (uint32)((uint32)0U << 2U)  /* SCS[2] */
                    | (uint32)((uint32)0U << 3U)  /* SCS[3] */
                    | (uint32)((uint32)0U << 4U)  /* SCS[4] */
                    | (uint32)((uint32)0U << 5U)  /* SCS[5] */
                    | (uint32)((uint32)0U << 8U)  /* ENA */
                    | (uint32)((uint32)0U << 9U)  /* CLK */
                    | (uint32)((uint32)0U << 10U)  /* SIMO[0] */
                    | (uint32)((uint32)0U << 11U)  /* SOMI[0] */
                    | (uint32)((uint32)0U << 17U)  /* SIMO[1] */
                    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /** - MIBSPI1 Port pullup / pulldown enable*/
    mibspiREG1->PC7 = (uint32)((uint32)0U << 0U)  /* SCS[0] */
                    | (uint32)((uint32)0U << 1U)  /* SCS[1] */
                    | (uint32)((uint32)0U << 2U)  /* SCS[2] */
                    | (uint32)((uint32)0U << 3U)  /* SCS[3] */
                    | (uint32)((uint32)0U << 4U)  /* SCS[4] */
                    | (uint32)((uint32)0U << 5U)  /* SCS[5] */
                    | (uint32)((uint32)0U << 8U)  /* ENA */
                    | (uint32)((uint32)0U << 9U)  /* CLK */
                    | (uint32)((uint32)0U << 10U)  /* SIMO[0] */
                    | (uint32)((uint32)0U << 11U)  /* SOMI[0] */
                    | (uint32)((uint32)0U << 17U)  /* SIMO[1] */
                    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /* MIBSPI1 set all pins to functional */
    mibspiREG1->PC0 = (uint32)((uint32)0U << 0U)  /* SCS[0] */
                    | (uint32)((uint32)0U << 1U)  /* SCS[1] */
                    | (uint32)((uint32)0U << 2U)  /* SCS[2] */
                    | (uint32)((uint32)0U << 3U)  /* SCS[3] */
                    | (uint32)((uint32)0U << 4U)  /* SCS[4] */
                    | (uint32)((uint32)0U << 5U)  /* SCS[5] */
                    | (uint32)((uint32)0U << 8U)  /* ENA */
                    | (uint32)((uint32)1U << 9U)  /* CLK */
                    | (uint32)((uint32)1U << 10U)  /* SIMO[0] */
                    | (uint32)((uint32)1U << 11U)  /* SOMI[0] */
                    | (uint32)((uint32)1U << 16U)  /* SIMO[1] */
                    | (uint32)((uint32)1U << 24U); /* SOMI[1] */
					
	//mibspiPmodeSet(mibspiREG1, 0, 0);

    /** - Finally start MIBSPI1 */
    mibspiREG1->GCR1 = (mibspiREG1->GCR1 & 0xFEFFFFFFU) | 0x01000000U;




/* USER CODE BEGIN (3) */
/* USER CODE END */

}


/** @fn void mibspiSetFunctional(mibspiBASE_t *mibspi, uint32 port)
*   @brief Change functional behavior of pins at runtime.
*   @param[in] mibspi   - mibspi module base address
*   @param[in] port  - Value to write to PC0 register
*
*   Change the value of the PC0 register at runtime, this allows to
*   dynamically change the functionality of the MIBSPI pins between functional
*   and GIO mode.
*/
/* SourceId : MIBSPI_SourceId_002 */
/* DesignId : MIBSPI_DesignId_002 */
/* Requirements : HL_SR154 */
void mibspiSetFunctional(mibspiBASE_t *mibspi, uint32 port)
{
/* USER CODE BEGIN (4) */
/* USER CODE END */

    mibspi->PC0 = port;

/* USER CODE BEGIN (5) */
/* USER CODE END */
}


/** @fn void mibspiSetData(mibspiBASE_t *mibspi, uint32 group, uint16 * data)
*   @brief Set Buffer Data
*   @param[in] mibspi   - Spi module base address
*   @param[in] group - Transfer group (0..7)
*   @param[in] data  - new data for transfer group
*
*   This function updates the data for the specified transfer group,
*   the length of the data must match the length of the transfer group.
*/
/* SourceId : MIBSPI_SourceId_003 */
/* DesignId : MIBSPI_DesignId_003 */
/* Requirements : HL_SR155 */
void mibspiSetData(mibspiBASE_t *mibspi, uint32 group, uint8 * data, uint8 length)
{
/* USER CODE BEGIN (6) */
/* USER CODE END */
    uint32 i ;
    uint8 j;
    mibspiRAM_t *ram    = (mibspi == mibspiREG1) ? mibspiRAM1 : ((mibspi == mibspiREG3) ? mibspiRAM3 : mibspiRAM5);
    uint32 start  = (mibspi->TGCTRL[group] >> 8U) & 0xFFU;
    uint32 end    = (group == 7U) ? (((mibspi->LTGPEND & 0x00007F00U) >> 8U) + 1U) : ((mibspi->TGCTRL[group+1U] >> 8U) & 0xFFU);
    // mibspi->TGCTRL[group] = 0x40700000U;
   // mibspi->TGCTRL[group] &= 0x7FFFFFFF;
    end = 128;

while(start < end)
{
            /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
                ram->tx[start].data = *data;
                /*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
                data++;
                start++;
}


/* USER CODE BEGIN (7) */
/* USER CODE END */
}


/** @fn void mibspiGetData(mibspiBASE_t *mibspi, uint32 group, uint16 * data)
*   @brief Retrieves Buffer Data from receive buffer
*   @param[in]  mibspi   - Spi module base address
*   @param[in]  group - Transfer group (0..7)
*   @param[out] data  - pointer to data array
*
*   @return error flags from data buffer, if there was a receive error on
*           one of the buffers this will be reflected in the return value.
*
*   This function transfers the data from the specified transfer group receive
*   buffers to the data array,  the length of the data must match the length
*   of the transfer group.
*/
/* SourceId : MIBSPI_SourceId_004 */
/* DesignId : MIBSPI_DesignId_004 */
/* Requirements : HL_SR156 */
uint16 rxcount;
uint32 mibspiGetData(mibspiBASE_t *mibspi, uint32 group, uint8 * data8, uint8 length)
{
/* USER CODE BEGIN (8) */
/* USER CODE END */
    uint16 * data;


    mibspiRAM_t *ram    = (mibspi == mibspiREG1) ? mibspiRAM1 : ((mibspi == mibspiREG3) ? mibspiRAM3 : mibspiRAM5);
    uint32 start  = (mibspi->TGCTRL[group] >> 8U) & 0xFFU;
    uint32 end    = (group == 7U) ? (((mibspi->LTGPEND & 0x00007F00U) >> 8U) + 1U) : ((mibspi->TGCTRL[group+1U] >> 8U) & 0xFFU);
    uint16 mibspiFlags  = 0U;
	uint32 ret;
	rxcount++;
    if (end == 0U) {end = 128U;}
    while (length > 0)
	{

		//while (start < end)
		{

			mibspiFlags  |= ram->rx[start].flags;
			/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
			//*data = ram->rx[start].data;
			data8[start] = (uint8) ram->rx[start].data;
			/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
			//data8[start]=(uint8)(data[start]);
			// data++;

			start++;
		}
		length--;
	}

	ret = ((uint32)mibspiFlags >> 8U) & 0x5FU;
/* USER CODE BEGIN (9) */
/* USER CODE END */

    return ret;
}


/** @fn void mibspiTransfer(mibspiBASE_t *mibspi, uint32 group)
*   @brief Transmit Transfer Group
*   @param[in] mibspi   - Spi module base address
*   @param[in] group - Transfer group (0..7)
*
*   Initiates a transfer for the specified transfer group.
*/
/* SourceId : MIBSPI_SourceId_005 */
/* DesignId : MIBSPI_DesignId_005 */
/* Requirements : HL_SR157 */
void mibspiTransfer(mibspiBASE_t *mibspi, uint32 group)
{
/* USER CODE BEGIN (10) */
/* USER CODE END */

    mibspi->TGCTRL[group] |= 0x80000000U;

/* USER CODE BEGIN (11) */
/* USER CODE END */
}


/** @fn boolean mibspiIsTransferComplete(mibspiBASE_t *mibspi, uint32 group)
*   @brief Check for Transfer Group Ready
*   @param[in] mibspi   - Spi module base address
*   @param[in] group - Transfer group (0..7)
*
*   @return TRUE is transfer complete, otherwise FALSE.
*
*   Checks to see if the transfer for the specified transfer group
*   has finished.
*/
/* SourceId : MIBSPI_SourceId_006 */
/* DesignId : MIBSPI_DesignId_006 */
/* Requirements : HL_SR158 */
boolean mibspiIsTransferComplete(mibspiBASE_t *mibspi, uint32 group)
{
    boolean status;

/* USER CODE BEGIN (12) */
/* USER CODE END */

    if(((((mibspi->TGINTFLG & 0xFFFF0000U) >> 16U)>> group) & 1U) == 1U)
    {
       mibspi->TGINTFLG = (mibspi->TGINTFLG & 0x0000FFFFU) | ((uint32)((uint32)1U << group) << 16U);
       status = TRUE;
    }
    else
    {
       status = FALSE;
    }

/* USER CODE BEGIN (13) */
/* USER CODE END */

    return (status);
}


/** @fn void mibspiEnableLoopback(mibspiBASE_t *mibspi, loopBackType_t Loopbacktype)
*   @brief Enable Loopback mode for self test
*   @param[in] mibspi        - Mibspi module base address
*   @param[in] Loopbacktype  - Digital or Analog
*
*   This function enables the Loopback mode for self test.
*/
/* SourceId : MIBSPI_SourceId_007 */
/* DesignId : MIBSPI_DesignId_009 */
/* Requirements : HL_SR161 */
void mibspiEnableLoopback(mibspiBASE_t *mibspi, loopBackType_t Loopbacktype)
{
/* USER CODE BEGIN (14) */
/* USER CODE END */

    /* Clear Loopback incase enabled already */
    mibspi->IOLPKTSTCR = 0U;

    /* Enable Loopback either in Analog or Digital Mode */
    mibspi->IOLPKTSTCR = (uint32)0x00000A00U
                       | (uint32)((uint32)Loopbacktype << 1U);

/* USER CODE BEGIN (15) */
/* USER CODE END */
}

/** @fn void mibspiDisableLoopback(mibspiBASE_t *mibspi)
*   @brief Enable Loopback mode for self test
*   @param[in] mibspi        - Mibspi module base address
*
*   This function disable the Loopback mode.
*/
/* SourceId : MIBSPI_SourceId_008 */
/* DesignId : MIBSPI_DesignId_010 */
/* Requirements : HL_SR162 */
void mibspiDisableLoopback(mibspiBASE_t *mibspi)
{
/* USER CODE BEGIN (16) */
/* USER CODE END */

    /* Disable Loopback Mode */
    mibspi->IOLPKTSTCR = 0x00000500U;

/* USER CODE BEGIN (17) */
/* USER CODE END */
}

/** @fn void mibspiPmodeSet(mibspiBASE_t *mibspi, mibspiPmode_t Pmode, mibspiDFMT_t DFMT)
*   @brief Set the Pmode for the selected Data Format register
*   @param[in] mibspi   - Mibspi module base address
*   @param[in] Pmode    - Mibspi Parellel mode
*                            PMODE_NORMAL
*                            PMODE_2_DATALINE
*                            PMODE_4_DATALINE
*                            PMODE_8_DATALINE
*   @param[in] DFMT     - Mibspi Data Format register
*                            DATA_FORMAT0
*                            DATA_FORMAT1
*                            DATA_FORMAT2
*                            DATA_FORMAT3
*
*   This function sets the Pmode for the selected Data Format register.
*/
/* SourceId : MIBSPI_SourceId_009 */
/* DesignId : MIBSPI_DesignId_011 */
/* Requirements : HL_SR524 */
void mibspiPmodeSet(mibspiBASE_t *mibspi, mibspiPmode_t Pmode, mibspiDFMT_t DFMT)
{
    uint32 pmctrl_reg;
    /* Set the Pmode for the selected Data Format register */
    pmctrl_reg     = (mibspi->PMCTRL & (~(uint32)((uint32)0xFFU << (8U * DFMT))));
    mibspi->PMCTRL = (pmctrl_reg | (uint32)((uint32)Pmode <<  ((8U * DFMT))));

}

/** @fn void mibspiEnableGroupNotification(mibspiBASE_t *mibspi, uint32 group, uint32 level)
*   @brief Enable Transfer Group interrupt
*   @param[in] mibspi   - Spi module base address
*   @param[in] group - Transfer group (0..7)
*   @param[in] level - Interrupt level
*
*   This function enables the transfer group finished interrupt.
*/
/* SourceId : MIBSPI_SourceId_010 */
/* DesignId : MIBSPI_DesignId_007 */
/* Requirements : HL_SR159 */
void mibspiEnableGroupNotification(mibspiBASE_t *mibspi, uint32 group, uint32 level)
{
/* USER CODE BEGIN (18) */
/* USER CODE END */

    if (level != 0U)
    {
        mibspi->TGITLVST = (mibspi->TGITLVST & 0x0000FFFFU) | (uint32)((uint32)((uint32)1U << group) << 16U);
    }
    else
    {
        mibspi->TGITLVCR = (mibspi->TGITLVCR & 0x0000FFFFU) | (uint32)((uint32)((uint32)1U << group) << 16U);
    }
    mibspi->TGITENST = (mibspi->TGITENST & 0x0000FFFFU) | (uint32)((uint32)((uint32)1U << group) << 16U);

/* USER CODE BEGIN (19) */
/* USER CODE END */
}


/** @fn void mibspiDisableGroupNotification(mibspiBASE_t *mibspi, uint32 group)
*   @brief Disable Transfer Group interrupt
*   @param[in] mibspi   - Spi module base address
*   @param[in] group - Transfer group (0..7)
*
*   This function disables the transfer group finished interrupt.
*/
/* SourceId : MIBSPI_SourceId_011 */
/* DesignId : MIBSPI_DesignId_008 */
/* Requirements : HL_SR160 */
void mibspiDisableGroupNotification(mibspiBASE_t *mibspi, uint32 group)
{
/* USER CODE BEGIN (20) */
/* USER CODE END */

    mibspi->TGITENCR = (mibspi->TGITENCR & 0x0000FFFFU) | (uint32)((uint32)((uint32)1U << group) << 16U);

/* USER CODE BEGIN (21) */
/* USER CODE END */
}

/** @fn void mibspi1GetConfigValue(mibspi_config_reg_t *config_reg, config_value_type_t type)
*   @brief Get the initial or current values of the configuration registers
*
*    @param[in] *config_reg: pointer to the struct to which the initial or current
*                           value of the configuration registers need to be stored
*    @param[in] type:     whether initial or current value of the configuration registers need to be stored
*                        - InitialValue: initial value of the configuration registers will be stored
*                                       in the struct pointed by config_reg
*                        - CurrentValue: initial value of the configuration registers will be stored
*                                       in the struct pointed by config_reg
*
*   This function will copy the initial or current value (depending on the parameter 'type')
*   of the configuration registers to the struct pointed by config_reg
*
*/
/* SourceId : MIBSPI_SourceId_012 */
/* DesignId : MIBSPI_DesignId_012 */
/* Requirements : HL_SR166 */
void mibspi1GetConfigValue(mibspi_config_reg_t *config_reg, config_value_type_t type)
{
    if (type == InitialValue)
    {
        config_reg->CONFIG_GCR1       = MIBSPI1_GCR1_CONFIGVALUE;
        config_reg->CONFIG_INT0       = MIBSPI1_INT0_CONFIGVALUE;
        config_reg->CONFIG_LVL        = MIBSPI1_LVL_CONFIGVALUE;
        config_reg->CONFIG_PCFUN      = MIBSPI1_PCFUN_CONFIGVALUE;
        config_reg->CONFIG_PCDIR      = MIBSPI1_PCDIR_CONFIGVALUE;
        config_reg->CONFIG_PCPDR      = MIBSPI1_PCPDR_CONFIGVALUE;
        config_reg->CONFIG_PCDIS      = MIBSPI1_PCDIS_CONFIGVALUE;
        config_reg->CONFIG_PCPSL      = MIBSPI1_PCPSL_CONFIGVALUE;
        config_reg->CONFIG_DELAY      = MIBSPI1_DELAY_CONFIGVALUE;
        config_reg->CONFIG_FMT0       = MIBSPI1_FMT0_CONFIGVALUE;
        config_reg->CONFIG_FMT1       = MIBSPI1_FMT1_CONFIGVALUE;
        config_reg->CONFIG_FMT2       = MIBSPI1_FMT2_CONFIGVALUE;
        config_reg->CONFIG_FMT3       = MIBSPI1_FMT3_CONFIGVALUE;
        config_reg->CONFIG_MIBSPIE    = MIBSPI1_MIBSPIE_CONFIGVALUE;
        config_reg->CONFIG_LTGPEND    = MIBSPI1_LTGPEND_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[0U] = MIBSPI1_TGCTRL0_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[1U] = MIBSPI1_TGCTRL1_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[2U] = MIBSPI1_TGCTRL2_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[3U] = MIBSPI1_TGCTRL3_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[4U] = MIBSPI1_TGCTRL4_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[5U] = MIBSPI1_TGCTRL5_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[6U] = MIBSPI1_TGCTRL6_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[7U] = MIBSPI1_TGCTRL7_CONFIGVALUE;
        config_reg->CONFIG_UERRCTRL   = MIBSPI1_UERRCTRL_CONFIGVALUE;
    }
    else
    {
    /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
        config_reg->CONFIG_GCR1       = mibspiREG1->GCR1;
        config_reg->CONFIG_INT0       = mibspiREG1->INT0;
        config_reg->CONFIG_LVL        = mibspiREG1->LVL;
        config_reg->CONFIG_PCFUN      = mibspiREG1->PC0;
        config_reg->CONFIG_PCDIR      = mibspiREG1->PC1;
        config_reg->CONFIG_PCPDR      = mibspiREG1->PC6;
        config_reg->CONFIG_PCDIS      = mibspiREG1->PC7;
        config_reg->CONFIG_PCPSL      = mibspiREG1->PC8;
        config_reg->CONFIG_DELAY      = mibspiREG1->DELAY;
        config_reg->CONFIG_FMT0       = mibspiREG1->FMT0;
        config_reg->CONFIG_FMT1       = mibspiREG1->FMT1;
        config_reg->CONFIG_FMT2       = mibspiREG1->FMT2;
        config_reg->CONFIG_FMT3       = mibspiREG1->FMT3;
        config_reg->CONFIG_MIBSPIE    = mibspiREG1->MIBSPIE;
        config_reg->CONFIG_LTGPEND    = mibspiREG1->LTGPEND;
        config_reg->CONFIG_TGCTRL[0U] = mibspiREG1->TGCTRL[0U];
        config_reg->CONFIG_TGCTRL[1U] = mibspiREG1->TGCTRL[1U];
        config_reg->CONFIG_TGCTRL[2U] = mibspiREG1->TGCTRL[2U];
        config_reg->CONFIG_TGCTRL[3U] = mibspiREG1->TGCTRL[3U];
        config_reg->CONFIG_TGCTRL[4U] = mibspiREG1->TGCTRL[4U];
        config_reg->CONFIG_TGCTRL[5U] = mibspiREG1->TGCTRL[5U];
        config_reg->CONFIG_TGCTRL[6U] = mibspiREG1->TGCTRL[6U];
        config_reg->CONFIG_TGCTRL[7U] = mibspiREG1->TGCTRL[7U];
        config_reg->CONFIG_UERRCTRL   = mibspiREG1->UERRCTRL;
    }
}

/** @fn void mibspi3GetConfigValue(mibspi_config_reg_t *config_reg, config_value_type_t type)
*   @brief Get the initial or current values of the configuration registers
*
*    @param[in] *config_reg: pointer to the struct to which the initial or current
*                           value of the configuration registers need to be stored
*    @param[in] type:     whether initial or current value of the configuration registers need to be stored
*                        - InitialValue: initial value of the configuration registers will be stored
*                                       in the struct pointed by config_reg
*                        - CurrentValue: initial value of the configuration registers will be stored
*                                       in the struct pointed by config_reg
*
*   This function will copy the initial or current value (depending on the parameter 'type')
*   of the configuration registers to the struct pointed by config_reg
*
*/
/* SourceId : MIBSPI_SourceId_013 */
/* DesignId : MIBSPI_DesignId_012 */
/* Requirements : HL_SR166 */
void mibspi3GetConfigValue(mibspi_config_reg_t *config_reg, config_value_type_t type)
{
    if (type == InitialValue)
    {
        config_reg->CONFIG_GCR1       = MIBSPI3_GCR1_CONFIGVALUE;
        config_reg->CONFIG_INT0       = MIBSPI3_INT0_CONFIGVALUE;
        config_reg->CONFIG_LVL        = MIBSPI3_LVL_CONFIGVALUE;
        config_reg->CONFIG_PCFUN      = MIBSPI3_PCFUN_CONFIGVALUE;
        config_reg->CONFIG_PCDIR      = MIBSPI3_PCDIR_CONFIGVALUE;
        config_reg->CONFIG_PCPDR      = MIBSPI3_PCPDR_CONFIGVALUE;
        config_reg->CONFIG_PCDIS      = MIBSPI3_PCDIS_CONFIGVALUE;
        config_reg->CONFIG_PCPSL      = MIBSPI3_PCPSL_CONFIGVALUE;
        config_reg->CONFIG_DELAY      = MIBSPI3_DELAY_CONFIGVALUE;
        config_reg->CONFIG_FMT0       = MIBSPI3_FMT0_CONFIGVALUE;
        config_reg->CONFIG_FMT1       = MIBSPI3_FMT1_CONFIGVALUE;
        config_reg->CONFIG_FMT2       = MIBSPI3_FMT2_CONFIGVALUE;
        config_reg->CONFIG_FMT3       = MIBSPI3_FMT3_CONFIGVALUE;
        config_reg->CONFIG_MIBSPIE    = MIBSPI3_MIBSPIE_CONFIGVALUE;
        config_reg->CONFIG_LTGPEND    = MIBSPI3_LTGPEND_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[0U] = MIBSPI3_TGCTRL0_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[1U] = MIBSPI3_TGCTRL1_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[2U] = MIBSPI3_TGCTRL2_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[3U] = MIBSPI3_TGCTRL3_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[4U] = MIBSPI3_TGCTRL4_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[5U] = MIBSPI3_TGCTRL5_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[6U] = MIBSPI3_TGCTRL6_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[7U] = MIBSPI3_TGCTRL7_CONFIGVALUE;
        config_reg->CONFIG_UERRCTRL   = MIBSPI3_UERRCTRL_CONFIGVALUE;
    }
    else
    {
    /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
        config_reg->CONFIG_GCR1       = mibspiREG3->GCR1;
        config_reg->CONFIG_INT0       = mibspiREG3->INT0;
        config_reg->CONFIG_LVL        = mibspiREG3->LVL;
        config_reg->CONFIG_PCFUN      = mibspiREG3->PC0;
        config_reg->CONFIG_PCDIR      = mibspiREG3->PC1;
        config_reg->CONFIG_PCPDR      = mibspiREG3->PC6;
        config_reg->CONFIG_PCDIS      = mibspiREG3->PC7;
        config_reg->CONFIG_PCPSL      = mibspiREG3->PC8;
        config_reg->CONFIG_DELAY      = mibspiREG3->DELAY;
        config_reg->CONFIG_FMT0       = mibspiREG3->FMT0;
        config_reg->CONFIG_FMT1       = mibspiREG3->FMT1;
        config_reg->CONFIG_FMT2       = mibspiREG3->FMT2;
        config_reg->CONFIG_FMT3       = mibspiREG3->FMT3;
        config_reg->CONFIG_MIBSPIE    = mibspiREG3->MIBSPIE;
        config_reg->CONFIG_LTGPEND    = mibspiREG3->LTGPEND;
        config_reg->CONFIG_TGCTRL[0U] = mibspiREG3->TGCTRL[0U];
        config_reg->CONFIG_TGCTRL[1U] = mibspiREG3->TGCTRL[1U];
        config_reg->CONFIG_TGCTRL[2U] = mibspiREG3->TGCTRL[2U];
        config_reg->CONFIG_TGCTRL[3U] = mibspiREG3->TGCTRL[3U];
        config_reg->CONFIG_TGCTRL[4U] = mibspiREG3->TGCTRL[4U];
        config_reg->CONFIG_TGCTRL[5U] = mibspiREG3->TGCTRL[5U];
        config_reg->CONFIG_TGCTRL[6U] = mibspiREG3->TGCTRL[6U];
        config_reg->CONFIG_TGCTRL[7U] = mibspiREG3->TGCTRL[7U];
        config_reg->CONFIG_UERRCTRL   = mibspiREG3->UERRCTRL;
    }
}

/** @fn void mibspi5GetConfigValue(mibspi_config_reg_t *config_reg, config_value_type_t type)
*   @brief Get the initial or current values of the configuration registers
*
*    @param[in] *config_reg: pointer to the struct to which the initial or current
*                           value of the configuration registers need to be stored
*    @param[in] type:     whether initial or current value of the configuration registers need to be stored
*                        - InitialValue: initial value of the configuration registers will be stored
*                                       in the struct pointed by config_reg
*                        - CurrentValue: initial value of the configuration registers will be stored
*                                       in the struct pointed by config_reg
*
*   This function will copy the initial or current value (depending on the parameter 'type')
*   of the configuration registers to the struct pointed by config_reg
*
*/
/* SourceId : MIBSPI_SourceId_014 */
/* DesignId : MIBSPI_DesignId_012 */
/* Requirements : HL_SR166 */
void mibspi5GetConfigValue(mibspi_config_reg_t *config_reg, config_value_type_t type)
{
    if (type == InitialValue)
    {
        config_reg->CONFIG_GCR1       = MIBSPI5_GCR1_CONFIGVALUE;
        config_reg->CONFIG_INT0       = MIBSPI5_INT0_CONFIGVALUE;
        config_reg->CONFIG_LVL        = MIBSPI5_LVL_CONFIGVALUE;
        config_reg->CONFIG_PCFUN      = MIBSPI5_PCFUN_CONFIGVALUE;
        config_reg->CONFIG_PCDIR      = MIBSPI5_PCDIR_CONFIGVALUE;
        config_reg->CONFIG_PCPDR      = MIBSPI5_PCPDR_CONFIGVALUE;
        config_reg->CONFIG_PCDIS      = MIBSPI5_PCDIS_CONFIGVALUE;
        config_reg->CONFIG_PCPSL      = MIBSPI5_PCPSL_CONFIGVALUE;
        config_reg->CONFIG_DELAY      = MIBSPI5_DELAY_CONFIGVALUE;
        config_reg->CONFIG_FMT0       = MIBSPI5_FMT0_CONFIGVALUE;
        config_reg->CONFIG_FMT1       = MIBSPI5_FMT1_CONFIGVALUE;
        config_reg->CONFIG_FMT2       = MIBSPI5_FMT2_CONFIGVALUE;
        config_reg->CONFIG_FMT3       = MIBSPI5_FMT3_CONFIGVALUE;
        config_reg->CONFIG_MIBSPIE    = MIBSPI5_MIBSPIE_CONFIGVALUE;
        config_reg->CONFIG_LTGPEND    = MIBSPI5_LTGPEND_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[0U] = MIBSPI5_TGCTRL0_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[1U] = MIBSPI5_TGCTRL1_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[2U] = MIBSPI5_TGCTRL2_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[3U] = MIBSPI5_TGCTRL3_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[4U] = MIBSPI5_TGCTRL4_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[5U] = MIBSPI5_TGCTRL5_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[6U] = MIBSPI5_TGCTRL6_CONFIGVALUE;
        config_reg->CONFIG_TGCTRL[7U] = MIBSPI5_TGCTRL7_CONFIGVALUE;
        config_reg->CONFIG_UERRCTRL   = MIBSPI5_UERRCTRL_CONFIGVALUE;
    }
    else
    {
    /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
        config_reg->CONFIG_GCR1       = mibspiREG5->GCR1;
        config_reg->CONFIG_INT0       = mibspiREG5->INT0;
        config_reg->CONFIG_LVL        = mibspiREG5->LVL;
        config_reg->CONFIG_PCFUN      = mibspiREG5->PC0;
        config_reg->CONFIG_PCDIR      = mibspiREG5->PC1;
        config_reg->CONFIG_PCPDR      = mibspiREG5->PC6;
        config_reg->CONFIG_PCDIS      = mibspiREG5->PC7;
        config_reg->CONFIG_PCPSL      = mibspiREG5->PC8;
        config_reg->CONFIG_DELAY      = mibspiREG5->DELAY;
        config_reg->CONFIG_FMT0       = mibspiREG5->FMT0;
        config_reg->CONFIG_FMT1       = mibspiREG5->FMT1;
        config_reg->CONFIG_FMT2       = mibspiREG5->FMT2;
        config_reg->CONFIG_FMT3       = mibspiREG5->FMT3;
        config_reg->CONFIG_MIBSPIE    = mibspiREG5->MIBSPIE;
        config_reg->CONFIG_LTGPEND    = mibspiREG5->LTGPEND;
        config_reg->CONFIG_TGCTRL[0U] = mibspiREG5->TGCTRL[0U];
        config_reg->CONFIG_TGCTRL[1U] = mibspiREG5->TGCTRL[1U];
        config_reg->CONFIG_TGCTRL[2U] = mibspiREG5->TGCTRL[2U];
        config_reg->CONFIG_TGCTRL[3U] = mibspiREG5->TGCTRL[3U];
        config_reg->CONFIG_TGCTRL[4U] = mibspiREG5->TGCTRL[4U];
        config_reg->CONFIG_TGCTRL[5U] = mibspiREG5->TGCTRL[5U];
        config_reg->CONFIG_TGCTRL[6U] = mibspiREG5->TGCTRL[6U];
        config_reg->CONFIG_TGCTRL[7U] = mibspiREG5->TGCTRL[7U];
        config_reg->CONFIG_UERRCTRL   = mibspiREG5->UERRCTRL;
    }
}


void mibspi1HighLevelInterrupt ()
{
	
}

void mibspi1LowLevelInterrupt ()
{
    mibspiREG1->INTVECT1 &= 0x00000000;
      mibspiGetData(mibspiREG1, 0, &gdataspi[0],10);
}




  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    要每500ms 接收26字节数据、最好将 TG 的大小配置为26字节、并使用 RX 中断来接收接收数据。

    如果 TG 大小为128个缓冲区、则在 TG 全部填满之前不会生成 RX 中断。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在多缓冲器 SPI 中、我认为我们无法配置 RX 中断。  我只能为 Tx 配置 TG 中断。

    即使 我按照长度配置 TG 大小、问题也无法解决。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您何时从 RX RAM 读取数据? 您是否不使用 DMA 将数据从 RX RAM 传输到 SRAM?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    即使我尝试使用 DMA、问题仍然存在

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    即使我尝试使用 DMA、问题仍然存在

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我读取您的代码、TG0大小为128个缓冲区。

     当 TG0已满时、RXINTFLG 标志被置位。 您可以为 TG0使用26个缓冲器吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    一个有趣的观察结果:

    调试器复位后、一切工作正常。

    问题仅在首次刷新时出现。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否尝试了 TG 大小= 26字节或26字节的字节?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Channa、

    请参阅我的示例:

    MibSPI3是主器件、使用 TG0、TG0 size=26缓冲器、字长= 16位、中断被启用、NCS 和 VCLK 之间插入6个 VLCK 周期

    MibSPI1是从器件、使用 TG0、TG0大小= 26个缓冲器、 字长= 16位、中断被启用、

    3. TX_DATA[][]被复制到 MibSPI3 RAM 中、RX_DATA[][]被从 MibSPI1 RAM 中接收数据

    4. main()比较 RX_DATA[][]和 TX_DATA[][],如果不匹配,则错误会增加。

    e2e.ti.com/.../RM46L852_5F00_MibSPI3_5F00_MibSPI1.zip