大家好、我使用的是 TM4C123GH6PM、我使用的是 QEI 模块。 使用示例代码 QEI1模块正在工作... 使用相同的代码、它不适用于 QEI0模块...任何建议...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、我使用的是 TM4C123GH6PM、我使用的是 QEI 模块。 使用示例代码 QEI1模块正在工作... 使用相同的代码、它不适用于 QEI0模块...任何建议...
FOR QEI1 MODULE TAKEN FROM THE EXAMPLE CODE OF CCS
/* ----------------------- Include Files --------------------- */
#include <stdint.h> // Library of Standard Integer Types
#include <stdbool.h> // Library of Standard Boolean Types
#include "inc/tm4c123gh6pm.h" // Definitions for interrupt and register assignments on Tiva C
#include "inc/hw_memmap.h" // Macros defining the memory map of the Tiva C Series device
#include "inc/hw_types.h" // Defines common types and macros
#include "inc/hw_gpio.h" // Defines Macros for GPIO hardware
#include "inc/hw_qei.h" // Macros used when accessing the QEI hardware
#include "driverlib/debug.h" // Macros for assisting debug of the driver library
#include "driverlib/sysctl.h" // Defines and macros for System Control API of DriverLib
#include "driverlib/interrupt.h" // Defines and macros for NVIC Controller API of DriverLib
#include "driverlib/gpio.h" // Defines and macros for GPIO API of DriverLib
#include "driverlib/qei.h" // Prototypes for the Quadrature Encoder Driver
#include "driverlib/pin_map.h" // Mapping of peripherals to pins for all parts
#include "driverlib/rom.h" // Defines and macros for ROM API of driverLib
#define VEL_INT_FREQ 10000 // Macro to store the Interrupt frequency of QEI1
#define QEI1_PPR 4000 // Macro to store the PPR of the QEI1
/* ----------------------- Global Variables --------------------- */
volatile uint32_t ui32Qei1Vel; // Variable to store the velocity of QEI1
volatile uint32_t ui32Qei1Pos; // Variable to store the position of QEI1
volatile int32_t i32Qei1Dir; // Variable to store the direction of QEI1
volatile uint16_t ui16Qei1Rpm; // Variable to store the RPM of QEI1
/* ----------------------- Function Prototypes --------------------- */
void QEI1IntHandler(void);
unsigned long int a;
/* ----------------------- Main Program --------------------- */
int main(void){
// a++;
// Set the System clock to 80MHz
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5 |SYSCTL_USE_PLL |SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ);
// Enable the clock for peripherals PortC and QEI1
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_QEI1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
// Configure the PC5, PC6 for QEI signals
ROM_GPIOPinTypeQEI(GPIO_PORTC_BASE, GPIO_PIN_5 | GPIO_PIN_6);
ROM_GPIOPinConfigure(GPIO_PC5_PHA1);
ROM_GPIOPinConfigure(GPIO_PC6_PHB1);
// Configure the QEI1 to increment for both PhA and PhB for quadrature input with "QEI1_PPR" PPR
ROM_QEIConfigure(QEI1_BASE, QEI_CONFIG_CAPTURE_A_B | QEI_CONFIG_QUADRATURE, QEI1_PPR);
// Configure the QEI1 for Velocity Calculation, Predivide by 1 at "VEL_INT_FREQ" Hz
ROM_QEIVelocityConfigure(QEI1_BASE, QEI_VELDIV_1, ROM_SysCtlClockGet() / VEL_INT_FREQ);
ROM_QEIVelocityEnable(QEI1_BASE);
// Enable the Interrupts for Velocity Timer Expiration of QEI1
void (*QEI1IntHandler_ptr)(void) = &QEI1IntHandler;
QEIIntRegister(QEI1_BASE, *QEI1IntHandler_ptr);
ROM_QEIIntEnable(QEI1_BASE, QEI_INTTIMER);
// Master interrupt enable API for all interrupts
ROM_IntMasterEnable();
// Enable the QEI1
ROM_QEIEnable(QEI1_BASE);
while (1);
}
/* ----------------------- Function Definition --------------------- */
void QEI1IntHandler(void){
// ISR for Quadrature Encoder Interface 1
// Clear the Interrupt that is generated
ROM_QEIIntClear(QEI1_BASE, ROM_QEIIntStatus(QEI1_BASE, true));
// Calculate the number of quadrature ticks in "1 / VEL_INT_FREQ" time period
ui32Qei1Vel = ROM_QEIVelocityGet(QEI1_BASE);
// Update the position reading of the encoder
ui32Qei1Pos = ROM_QEIPositionGet(QEI1_BASE);
// Update the direction reading of the encoder
i32Qei1Dir = ROM_QEIDirectionGet(QEI1_BASE);
// Calculate the velocity in RPM
ui16Qei1Rpm = ui32Qei1Vel * VEL_INT_FREQ * 60 / QEI1_PPR;
}
/* ----------------------- Include Files --------------------- */
#include <stdint.h> // Library of Standard Integer Types
#include <stdbool.h> // Library of Standard Boolean Types
#include "inc/tm4c123gh6pm.h" // Definitions for interrupt and register assignments on Tiva C
#include "inc/hw_memmap.h" // Macros defining the memory map of the Tiva C Series device
#include "inc/hw_types.h" // Defines common types and macros
#include "inc/hw_gpio.h" // Defines Macros for GPIO hardware
#include "inc/hw_qei.h" // Macros used when accessing the QEI hardware
#include "driverlib/debug.h" // Macros for assisting debug of the driver library
#include "driverlib/sysctl.h" // Defines and macros for System Control API of DriverLib
#include "driverlib/interrupt.h" // Defines and macros for NVIC Controller API of DriverLib
#include "driverlib/gpio.h" // Defines and macros for GPIO API of DriverLib
#include "driverlib/qei.h" // Prototypes for the Quadrature Encoder Driver
#include "driverlib/pin_map.h" // Mapping of peripherals to pins for all parts
#include "driverlib/rom.h" // Defines and macros for ROM API of driverLib
#define VEL_INT_FREQ 10000
#define QEI0_PPR 4000
/* ----------------------- Global Variables --------------------- */
volatile uint32_t ui32Qei0Vel;
volatile uint32_t ui32Qei0Pos;
volatile int32_t i32Qei0Dir;
volatile uint16_t ui16Qei0Rpm;
/* ----------------------- Function Prototypes --------------------- */
void QEI0IntHandler(void);
unsigned long int a;
/* ----------------------- Main Program --------------------- */
int main(void){
// Set the System clock to 80MHz
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5 |SYSCTL_USE_PLL |SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ);
// Enable the clock for peripherals PortD and QEI0
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_QEI0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
// Configure the PC5, PC6 for QEI signals
ROM_GPIOPinTypeQEI(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
ROM_GPIOPinConfigure(GPIO_PD6_PHA0);
ROM_GPIOPinConfigure(GPIO_PD7_PHB0);
// Configure the QEI1 to increment for both PhA and PhB for quadrature input with "QEI0_PPR" PPR
ROM_QEIConfigure(QEI0_BASE, QEI_CONFIG_CAPTURE_A_B | QEI_CONFIG_QUADRATURE, QEI0_PPR);
// Configure the QEI1 for Velocity Calculation, Predivide by 1 at "VEL_INT_FREQ" Hz
ROM_QEIVelocityConfigure(QEI0_BASE, QEI_VELDIV_1, ROM_SysCtlClockGet() / VEL_INT_FREQ);
ROM_QEIVelocityEnable(QEI0_BASE);
// Enable the Interrupts for Velocity Timer Expiration of QEI0
void (*QEI0IntHandler_ptr)(void) = &QEI0IntHandler;
QEIIntRegister(QEI0_BASE, *QEI0IntHandler_ptr);
ROM_QEIIntEnable(QEI0_BASE, QEI_INTTIMER);
// Master interrupt enable API for all interrupts
ROM_IntMasterEnable();
ROM_QEIEnable(QEI0_BASE);
while (1);
}
/* ----------------------- Function Definition --------------------- */
void QEI0IntHandler(void)
{
// ISR for Quadrature Encoder Interface 1
// Clear the Interrupt that is generated
ROM_QEIIntClear(QEI0_BASE, ROM_QEIIntStatus(QEI0_BASE, true));
// Calculate the number of quadrature ticks in "1 / VEL_INT_FREQ" time period
ui32Qei0Vel = ROM_QEIVelocityGet(QEI0_BASE);
// Update the position reading of the encoder
ui32Qei0Pos = ROM_QEIPositionGet(QEI0_BASE);
// Update the direction reading of the encoder
i32Qei0Dir = ROM_QEIDirectionGet(QEI0_BASE);
// Calculate the velocity in RPM
ui16Qei0Rpm = ui32Qei0Vel * VEL_INT_FREQ * 60 / QEI0_PPR;
}
该代码具有以下配置 QEI0引脚的功能、其中包含对使用端口 C 和 D 的混合引用:
// Configure the PC5, PC6 for QEI signals
ROM_GPIOPinTypeQEI(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
ROM_GPIOPinConfigure(GPIO_PD6_PHA0);
ROM_GPIOPinConfigure(GPIO_PD7_PHB0);
假设您要对 PhA0使用 PD6、对 PhB0使用 PD7、则尝试将代码更改为:
// Configure the PD6, PD7 for QEI signals
ROM_GPIOPinTypeQEI(GPIO_PORTD_BASE, GPIO_PIN_6 | GPIO_PIN_7);
ROM_GPIOPinConfigure(GPIO_PD6_PHA0);
ROM_GPIOPinConfigure(GPIO_PD7_PHB0);Anuprash、您好!
很抱歉耽误了我的假期。
您使用的 PD7是一个 NMI 引脚、默认情况下在器件上被锁定。 您将需要解锁引脚以将其配置为 QEI0操作。
有关如何操作的详细信息、请参阅以下常见问题解答: https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1020814/faq-how-to-get-locked-gpio-pins-on-tm4c123-devices-to-work
除此之外、将您的代码与 Chester 观察到 的内容与 QEI0 GPIO 配置的 GPIO_PORTC_BASE 不正确进行比较、其他所有内容似乎都与转换保持一致。 我相信、一旦您添加解锁例程、您就会有一个可用的 QEI0外设。
此致、
Ralph Jacobi