This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C129XNCZAD:启用 DMA 的 SSI

Guru**** 2930750 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1175216/tm4c129xnczad-dma-enabled-ssi

器件型号:TM4C129XNCZAD

尊敬的专家:

希望您在感恩节期间和家人度过美好时光。 最近、我正在帮助 TM4C 客户使用 TM4C129X 构建 DMA 演示代码、因为他们对成熟的项目有更严格的时序要求。 目标是向 SSI0发送/接收添加 DMA 操作。 我尝试构建启用了 DMA 的 SSI0操作代码、但发现该代码将滞留在外设 DMA 中断处理程序中、并且无法正常运行。 我使用的参考代码是 DK-TM4C129X 中的 udmademo、我使用的电路板是 DK-TM4C129X。 请帮助您查看我遗漏的内容吗? 这是由于总线的 CPU 和 DMA 竞争造成的吗? 因为我没有在代码中添加 CPU 睡眠。 BTW、从分步调试中、我发现 MCU 始终在执行 SSI 中断处理程序、但我尝试清除标志位、但不起作用。 我随附了我正在使用的代码、在此代码中、我将外设从 SSI 更改为 UART、因为我认为逻辑将相似、但我遇到了相同的故障。

Eric

-//*****************************************************************************
//
// spi_master.c - Example demonstrating how to configure SSI0 in SPI master
//                mode.
//
// Copyright (c) 2010-2020 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
//   Redistribution and use in source and binary forms, with or without
//   modification, are permitted provided that the following conditions
//   are met:
// 
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the  
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// 
// This is part of revision 2.2.0.295 of the Tiva Firmware Development Package.
//
//*****************************************************************************

#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/udma.h"
#include "driverlib/uart.h"
#include "inc/hw_ssi.h"
#include "driverlib/interrupt.h"
#include "inc/hw_ints.h"
#include "inc/hw_types.h"
#include "inc/hw_udma.h"
#include "inc/hw_uart.h"

//*****************************************************************************
//
//! \addtogroup ssi_examples_list
//! <h1>SPI Master (spi_master)</h1>
//!
//! This example shows how to configure the SSI0 as SPI Master.  The code will
//! send three characters on the master Tx then polls the receive FIFO until
//! 3 characters are received on the master Rx.
//!
//! This example uses the following peripherals and I/O signals.  You must
//! review these and change as needed for your own board:
//! - SSI0 peripheral
//! - GPIO Port A peripheral (for SSI0 pins)
//! - SSI0Clk - PA2
//! - SSI0Fss - PA3
//! - SSI0Rx (TM4C123x) / SSI0XDAT0 (TM4C129x) - PA4
//! - SSI0Tx (TM4C123x) / SSI0XDAT1 (TM4C129x) - PA5
//!
//! The following UART signals are configured only for displaying console
//! messages for this example.  These are not required for operation of SSI0.
//! - UART0 peripheral
//! - GPIO Port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//!
//! This example uses the following interrupt handlers.  To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - None.
//
//*****************************************************************************

//*****************************************************************************
//
// Number of bytes to send and receive.
//
//*****************************************************************************
#define NUM_SSI_DATA 3
#define SSI_TX 0x00000800
#define SSI_RX 0x00000400


uint32_t EEG_dataready = 0;
uint32_t g_ui32uDMAErrCount = 0;
uint8_t EEG_TXBuffer[132];
uint8_t EEG_RXBufferA[132];
uint8_t EEG_RXBufferB[132];

#pragma DATA_ALIGN(ui8ControlTable, 1024)
uint8_t ui8ControlTable[1024];

//*****************************************************************************
//
// The interrupt handler for SSI0.  This interrupt will occur when a DMA
// transfer is complete using the SSI0 uDMA channel.  It will also be
// triggered if the peripheral signals an error.
//
//*****************************************************************************
void SSI0IntHandler(void)
{
    uint32_t ui32Status;

    //
    //
     // Read the interrupt status of the SSI0.
     //

     ui32Status = HWREG(SSI0_BASE + SSI_O_MIS);

     HWREG(SSI0_BASE + SSI_O_ICR) = ui32Status;

     //
     // Clear any pending status, even though there should be none since no UART
     // interrupts were enabled.  If UART error interrupts were enabled, then
     // those interrupts could occur here and should be handled.  Since uDMA is
     // used for both the RX and TX, then neither of those interrupts should be
     // enabled.
     //
     //SSIIntClear(SSI0_BASE, ui32Status);

     ui32Status = HWREG(UDMA_CHIS);

     HWREG(UDMA_CHIS) = ui32Status;

     //
     // If the SSI0 DMA RX channel is disabled, that means the RX DMA transfer
     // is done.
     //
     //if(!uDMAChannelIsEnabled(UDMA_CHANNEL_SSI0RX))

         //
         // Notify main that EEG data is ready.
         //
     if(!uDMAChannelIsEnabled(UDMA_CHANNEL_SSI0TX))
     {
         //
         EEG_dataready = 1;
     }


}

void uDMAErrorHandler(void)
{
    uint32_t ui32Status;

    //
    // Check for uDMA error bit
    //
    ui32Status = uDMAErrorStatusGet();

    //
    // If there is a uDMA error, then clear the error and increment
    // the error counter.
    //
    if(ui32Status)
    {
        uDMAErrorStatusClear();
        g_ui32uDMAErrCount++;
    }
}


//*****************************************************************************
//
// The interrupt handler for UART0.  This interrupt will occur when a DMA
// transfer is complete using the UART0 uDMA channel.  It will also be
// triggered if the peripheral signals an error.  This interrupt handler will
// switch between receive ping-pong buffers A and B.  It will also restart a TX
// uDMA transfer if the prior transfer is complete.  This will keep the UART
// running continuously (looping TX data back to RX).
//
//*****************************************************************************
void
UART0IntHandler(void)
{
    uint32_t ui32Status;
    uint32_t ui32Mode;

    //
    // Read the interrupt status of the UART.
    //
    ui32Status = UARTIntStatus(UART0_BASE, 1);

    //
    // Clear any pending status, even though there should be none since no UART
    // interrupts were enabled.  If UART error interrupts were enabled, then
    // those interrupts could occur here and should be handled.  Since uDMA is
    // used for both the RX and TX, then neither of those interrupts should be
    // enabled.
    //
    UARTIntClear(UART0_BASE, ui32Status);

    //
    // Check the DMA control table to see if the ping-pong "A" transfer is
    // complete.  The "A" transfer uses receive buffer "A", and the primary
    // control structure.
    //
    ui32Mode = uDMAChannelModeGet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT);

    //
    // If the primary control structure indicates stop, that means the "A"
    // receive buffer is done.  The uDMA controller should still be receiving
    // data into the "B" buffer.
    //
    if(ui32Mode == UDMA_MODE_STOP)
    {

        //
        // Set up the next transfer for the "A" buffer, using the primary
        // control structure.  When the ongoing receive into the "B" buffer is
        // done, the uDMA controller will switch back to this one.  This
        // example re-uses buffer A, but a more sophisticated application could
        // use a rotating set of buffers to increase the amount of time that
        // the main thread has to process the data in the buffer before it is
        // reused.
        //
        uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART0_BASE + UART_O_DR),
                                   EEG_RXBufferA, sizeof(EEG_RXBufferA));
    }

    //
    // Check the DMA control table to see if the ping-pong "B" transfer is
    // complete.  The "B" transfer uses receive buffer "B", and the alternate
    // control structure.
    //
    ui32Mode = uDMAChannelModeGet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT);

    //
    // If the alternate control structure indicates stop, that means the "B"
    // receive buffer is done.  The uDMA controller should still be receiving
    // data into the "A" buffer.
    //
    if(ui32Mode == UDMA_MODE_STOP)
    {

        //
        // Set up the next transfer for the "B" buffer, using the alternate
        // control structure.  When the ongoing receive into the "A" buffer is
        // done, the uDMA controller will switch back to this one.  This
        // example re-uses buffer B, but a more sophisticated application could
        // use a rotating set of buffers to increase the amount of time that
        // the main thread has to process the data in the buffer before it is
        // reused.
        //
        uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART0_BASE + UART_O_DR),
                                   EEG_RXBufferB, sizeof(EEG_RXBufferA));
    }

    //
    // If the UART0 DMA TX channel is disabled, that means the TX DMA transfer
    // is done.
    //
    if(!uDMAChannelIsEnabled(UDMA_CHANNEL_UART0TX))
    {
        //
        // Start another DMA transfer to UART0 TX.
        //
        uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
                                   UDMA_MODE_BASIC, EEG_TXBuffer,
                                   (void *)(UART0_BASE + UART_O_DR),
                                   sizeof(EEG_TXBuffer));
        EEG_dataready = 1;

        //
        // The uDMA TX channel must be re-enabled.
        //
        uDMAChannelEnable(UDMA_CHANNEL_UART0TX);
    }

}

//*****************************************************************************
//
// Configure SSI0 in master Freescale (SPI) mode.  This example will send out
// 3 bytes of data, then wait for 3 bytes of data to come in.  This will all be
// done using the polling method.
//
//*****************************************************************************
int
main(void)
{
#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    uint32_t ui32SysClock;
#endif

    uint32_t pui32DataTx[NUM_SSI_DATA];
    uint32_t pui32DataRx[NUM_SSI_DATA];
    uint32_t ui32Index;

    //
    // Set the clocking to run directly from the external crystal/oscillator.
    // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
    // crystal on your board.
    //
#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                       SYSCTL_OSC_MAIN |
                                       SYSCTL_USE_OSC), 25000000);
#else
    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                   SYSCTL_XTAL_16MHZ);
#endif

    //
    // The SSI0 peripheral must be enabled for use.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

    //
    // For this example SSI0 is used with PortA[5:2].  The actual port and pins
    // used may be different on your part, consult the data sheet for more
    // information.  GPIO port A needs to be enabled so these pins can be used.
    // TODO: change this to whichever GPIO port you are using.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    //
    // Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5.
    // This step is not necessary if your part does not support pin muxing.
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
    GPIOPinConfigure(GPIO_PA3_SSI0FSS);
#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);
    GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);
#else
    GPIOPinConfigure(GPIO_PA4_SSI0RX);
    GPIOPinConfigure(GPIO_PA5_SSI0TX);
#endif

    //
    // PA0-1 are used for UART0.
    //
    GPIOPinConfigure(GPIO_PA0_U0RX);
    GPIOPinConfigure(GPIO_PA1_U0TX);
    GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    //
    // Configure the GPIO settings for the SSI pins.  This function also gives
    // control of these pins to the SSI hardware.  Consult the data sheet to
    // see which functions are allocated per pin.
    // The pins are assigned as follows:
    //      PA5 - SSI0Tx (TM4C123x) / SSI0XDAT1 (TM4C129x)
    //      PA4 - SSI0Rx (TM4C123x) / SSI0XDAT0 (TM4C129x)
    //      PA3 - SSI0Fss
    //      PA2 - SSI0CLK
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |
                   GPIO_PIN_2);

    //
    // Configure and enable the SSI port for SPI master mode.  Use SSI0,
    // system clock supply, idle clock level low and active low clock in
    // freescale SPI mode, master mode, 1MHz SSI frequency, and 8-bit data.
    // For SPI mode, you can set the polarity of the SSI clock when the SSI
    // unit is idle.  You can also configure what clock edge you want to
    // capture data on.  Please reference the datasheet for more information on
    // the different SPI modes.
    //
#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    SSIConfigSetExpClk(SSI0_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_1,
                       SSI_MODE_MASTER, 1000000, 8);
#else
    SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#endif

    UARTConfigSetExpClk(UART0_BASE, ui32SysClock, 115200,
                                UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                                UART_CONFIG_PAR_NONE);

    //
    // Enable peripherals to operate when CPU is in sleep.
    //
    SysCtlPeripheralClockGating(true);

    //
    //
    //
    // Enable the UDMA peripheral
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
    //
    // Wait for the UDMA module to be ready.
    //
    while(!SysCtlPeripheralReady(SYSCTL_PERIPH_UDMA))
    {
    }
    //
    // Enable the uDMA controller.
    //
    uDMAEnable();
    //
    // Set the base for the channel control table.
    //
    uDMAControlBaseSet(&ui8ControlTable[0]);

    //
    // Set both the TX and RX trigger thresholds to 4.  This will be used by
    // the uDMA controller to signal when more data should be transferred.  The
    // uDMA TX and RX channels will be configured so that it can transfer 4
    // bytes in a burst when the UART is ready to transfer more data.
    //
    UARTFIFOLevelSet(UART0_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

    //
    // Enable the UART for operation, and enable the uDMA interface for both TX
    // and RX channels.
    //
    UARTEnable(UART0_BASE);

    UARTDMAEnable(UART0_BASE, UART_DMA_TX | UART_DMA_RX);

    //
    // This register write will set the UART to operate in loopback mode.  Any
    // data sent on the TX output will be received on the RX input.
    //
    HWREG(UART0_BASE + UART_O_CTL) |= UART_CTL_LBE;

    //
    // Put the attributes in a known state for the uDMA UART0RX channel.  These
    // should already be disabled by default.
    //
    uDMAChannelAttributeDisable(UDMA_CHANNEL_UART0RX,
                                    UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Configure the control parameters for the primary control structure for
    // the UART RX channel.  The primary contol structure is used for the "A"
    // part of the ping-pong receive.  The transfer data size is 8 bits, the
    // source address does not increment since it will be reading from a
    // register.  The destination address increment is byte 8-bit bytes.  The
    // arbitration size is set to 4 to match the RX FIFO trigger threshold.
    // The uDMA controller will use a 4 byte burst transfer if possible.  This
    // will be somewhat more effecient that single byte transfers.
    //
    uDMAChannelControlSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Configure the control parameters for the alternate control structure for
    // the UART RX channel.  The alternate contol structure is used for the "B"
    // part of the ping-pong receive.  The configuration is identical to the
    // primary/A control structure.
    //
    uDMAChannelControlSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the UART RX primary control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "A" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART0_BASE + UART_O_DR),
                               EEG_RXBufferA, sizeof(EEG_RXBufferA));

    //
    // Set up the transfer parameters for the UART RX alternate control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "B" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART0_BASE + UART_O_DR),
                               EEG_RXBufferB, sizeof(EEG_RXBufferB));

    //
    // Put the attributes in a known state for the uDMA UART0TX channel.  These
    // should already be disabled by default.
    //
    uDMAChannelAttributeDisable(UDMA_CHANNEL_UART0TX,
                                    UDMA_ATTR_ALTSELECT |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Set the USEBURST attribute for the uDMA UART TX channel.  This will
    // force the controller to always use a burst when transferring data from
    // the TX buffer to the UART.  This is somewhat more effecient bus usage
    // than the default which allows single or burst transfers.
    //
    uDMAChannelAttributeEnable(UDMA_CHANNEL_UART0TX, UDMA_ATTR_USEBURST);

    //
    // Configure the control parameters for the UART TX.  The uDMA UART TX
    // channel is used to transfer a block of data from a buffer to the UART.
    // The data size is 8 bits.  The source address increment is 8-bit bytes
    // since the data is coming from a buffer.  The destination increment is
    // none since the data is to be written to the UART data register.  The
    // arbitration size is set to 4, which matches the UART TX FIFO trigger
    // threshold.
    //
    uDMAChannelControlSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_8 |
                              UDMA_DST_INC_NONE |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the uDMA UART TX channel.  This will
    // configure the transfer source and destination and the transfer size.
    // Basic mode is used because the peripheral is making the uDMA transfer
    // request.  The source is the TX buffer and the destination is the UART
    // data register.
    //
    uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
                               UDMA_MODE_BASIC, EEG_TXBuffer,
                               (void *)(UART0_BASE + UART_O_DR),
                               sizeof(EEG_TXBuffer));

    //
    // Now both the uDMA UART TX and RX channels are primed to start a
    // transfer.  As soon as the channels are enabled, the peripheral will
    // issue a transfer request and the data transfers will begin.
    //
    uDMAChannelEnable(UDMA_CHANNEL_UART0TX);

    uDMAChannelEnable(UDMA_CHANNEL_UART0RX);

    //
    // Enable the UART DMA TX/RX interrupts.
    //
    UARTIntEnable(UART0_BASE, UART_INT_DMATX | UART_INT_DMARX);

    //
    // Enable the UART peripheral interrupts.
    //
    IntEnable(INT_UART0);


    while(1)
    {
        if(EEG_dataready)
        {
            //
            EEG_dataready = 0;

            //SysCtlDelay(240);

            uint32_t i = 0;
            for(i = 0; i < 132; i++)
            {
                //
                EEG_TXBuffer[i] = 0x55;
                EEG_RXBufferA[i] = 0x00;
                EEG_RXBufferB[i] = 0x00;
            }

            uDMAChannelEnable(UDMA_CHANNEL_UART0TX);
            uDMAChannelEnable(UDMA_CHANNEL_UART0RX);

        }


    }

    //
    // Return no errors
    //
    return(0);
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Eric、

    我看到 UART0的 IntEnable、但看不到 SSI0的 IntEnable、因此不会对 SSI0中断提供服务、因为它在外设级别上未启用。 尝试添加以解决中断挂起问题。

    此致、

    Ralph Jacobi