请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM2634-Q1 主题中讨论的其他器件:AM2634
尊敬的香榭丽舍
您能否检查 AM2634的 RSVD T4引脚为何连接到 AM263x LP-EVM 中的1.2V VDD?
但是、建议将 RSVD_T4连接到数据表中的 GND、如下所示。
谢谢、此致、
SI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.