Other Parts Discussed in Thread: CC3100, CC2530, EK-TM4C1294XL
#ifndef __CC3200R1M1RGC__
#include
#endif
#include
#include "PubNub.h"
#include
#include
#include
#include
#include "TembooAccount.h"
#include
#include
#include
#include
#define APP_NAME "EDFT-2017_Mohamed RAHALI"
#define RF430CL330H_BoosterPack_RESET_PIN 8
#define RF430CL330H_BoosterPack_IRQ_PIN 12
RF430 NFC (RF430CL330H_BoosterPack_RESET_PIN、RF430CL330H_BoosterPack_IRQ_PIN);
//********* //
// RFID/NFC 功能 /////*********
//
void RF430CL (void){
Serial.println ("初始化 I2C-");
Wire.begin();
Serial.println ("初始化 NFC Tag-");
nfc.begin();
Serial.println ("声明 URL 对象-");
NDEF_URI tirweb ("">freeboard.io/.../yMSkFJ");
serial.println ("声明 URL 的文本说明");
NDEF_TXT tidesc ("es"、"tf_2017 reizado por Mohamed RAHALi");
serial.println ("将 URL 对象写入 NFC 收发器-");
int ndef_size;
//记录0
ndef、false = tiweb.sendTo(nfc;false = true //此消息应设置 MB,但不能设置 ME。
serial.println ("将文本对象写入 NFC 收发器"-);
//记录1
ndef_size += tidesc.sendTo(nfc、false、true); //此消息应将 MB 保留为已清除状态,但将我设置为已清除状态。
serial.println ("激活 NFC 收发器"-);
nfc.enable();
//
serial.println ("打印串行端口的 URL -");
// tidweb.printURI (串行); //测试 NDEF_URI printURI ()功能
// Serial.println ();
//
Serial.printn (“将文本说明打印到串行端口”);
// Serial.println (tidesc.getText ()));
}
//-------------------- 可变因素---------------------------- //
double andrDouble( double min、double max、int numCasas){
long _min = min * pow (10、numCasas)+ 0.1;
long _max = max * pow (10、numCasas)+ 0.1;
return (double) random (_min、_max)/pow (10、numCasas);
}
Double Freq = RandomDouble (10.71、10.79、2)+1839755.00;
double volte_1 = Randomble (0.82、0.88、2);
double temperature = RandomDouble (18.30、20.00、2);
double vol = 3.10 Double (
unsigned、3.29、2);long lastConnectionTime = 0; //上次连接到服务器时,以毫秒为单位
的布尔连接= false; //上次通过主循环
的连接状态 const unsigned long postingInterval = 0.001*1000; // ThingSpeak.com int
failedCounter = 0;
char buffer[25]; //buffer for float to string
//网络设置
字符 SSID[]="TP-link_4B41C0"; //网络名称(SSID)
字符密码[]="L@F@mii@R@h@li/10"; //网络密码
int keyIndex = 0; //网络密钥索引号(仅用于 WEP)
WiFiServer 服务器(80);
WiFiClient client_1;
WiFiClient *客户端; // WiFiClient 客户端;
//--------------- floatToString 方法------------------------------------------------------- //
字符串 floatToString (float x、byte precision = 4){
char tmp[50];
dtostrf (x、0、precision、tmp);
返回字符串(Tmp);
}
//*********
// PubNub Credencial & send 函数
//*********
const static char pubkey[]="pub-c-f00e3441-95d8-4d27-a4fb-d03fb4def8ae";
const static char 子项[]="sub-c-9d695234-13ad-11e7-894d-0619f8945a4f";const static char char subsub []="sub-9d69d695234-13dsandome(+d)+jsunchar
suntersene(=*2
;dunchemdson.json.sw);d(*2;dunchemdunchemd(*2 dunchemdunchemdong2;dunchemdunchemdunt damendere*2;damdunchunche*2;damdunchunche*tursene
双温度= RandomDouble (18.30、20.00、2);
double vol = Randomble (3.10、3.29、2);
aJson.addStringToObject (sender、"name"、 "CC3100");
aJson.addItemToObject (msg、"发件人"、发件人);
aJson.addNumberToObject (msg、 "SN"、SN);
aJson.addNumberToObject (msg、"FreqTiva"、Freq);
aJson.addNumberToObject (msg、"Voltiva"、voltive_1);
aJson.addNumberToObject (msg、"TempNodes"、 温度);
aJson.addNumberToObject (msg、"voltNodes"、vol);
sn++;
如果(SN =9999){
SN = 0;
}
返回 msg;
}
空 dumpMessage (Stream &s、aJsonObject * msg)
{
int msg_count = aJson.getArraySize (msg);
for (int j = 0;j < msg_count;j++){
aJsonObject *项、*发件人、*值;
S.print ("Msg #");
S.println (j、DEC);
item = aJson.getArrayItem (msg、j);
如果(!item){
S.println ("未获取商品");
延迟(100);
返回;
}
//下面,我们解析和转储来自同修的消息。 *
sender = aJson.getObjectItem (item、"sender");
如果(!sender){
S.println ("未获取发件人");
延迟(100);
返回;
}
S.println();
}
//*********
// WiFiConfig
//配置 Wifi 设置,连接到网络并创建 Web 服务器
void WifiSettings(void){
Serial.print("Attempting to connect to Network named:"); //尝试连接到 Wifi 网络
Serial.println (SSID); //打印网络名称(SSID)
WiFi.begin(ssid,密码); //连接到 WPA/WPA2网络。 如果在
( wife.status()!= wl_connected ){时使用开放或 WEP 网络,请更改此行
serial.print("."); //等待连接时打印点
delay (300);
}
Serial.println ("\n 您已连接到网络");
Serial.println ("正在等待 IP 地址");
while (WiFi.localIP ()== INADDR_NONE){
serial.print("."); //等待 IP 地址时打印点
delay(300);
}
Serial.println("\nip Address obtained");
printWifiStatus());
}
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// */
* 呼叫电话功能 /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
/void
callphone (void){
TembooChoreo ConfirmTextToSpeechPromptChoreo (client_1);
//设置 Temboo 帐户凭据
ConfirmTextToSpeechPromptChoreo.setAccountName(TEMBOO_ACCOUNT);
ConfirmTextToSpeechPromptChoreo.setAppKeyName(TEMBOO_APP_KEY_NAME);
ConfirmTextToSpeechPromptChoreo.setAppKey(TEMBOO_APP_KEY);
//设置 Choreo 输入
字符串 CallbackURLValue ="">http://192.168.0.105/";
ConfirmTextToValue SpeechProeToPrompto.addInput ("CallbackURL"、CallbackURLMx);"ConfirmTextToValue"
="SpeedKeyString Number7Spine.7SpinoreNumber"
;"ConfirmProSpeedKeyKeyString ("ConfirmProSpeedNumber");
字符串 ByeTextValue ="El valor actual de frecuencia Tiva es de ";
ByeTextValue = ByeTextValue +(Freq/1000000)+" MHz。 El voltaje_Tiva detectado es de "+ voltage_1;
ByeTextValue = ByeTextValue +"、la temperatura_Node1 es"+温度+"、el voltaje_Node1 es"+ vol;
ByeTextValue = ByeTextValue +"、la volatura_Node2 es"+"voltage+"、"+"nodeje"+"voltaje_voltage"。 El informe de Estado del equipo ha terminado。 hasta pron.";
ConfirmTextToSpeechPromptChoreo.addInput ("ByeText"、ByeTextValue");
String TextValue ="CC3100 Remotes Updates。 niveles dentro de rango de seguridad。";
TextValue = TextValue +"、。 Pulse uno para conocer los valores actuales de los parámetros ó n de medida。";
ConfirmTextToSpeechPromptChore.addInput ("text"、TextValue);
String FromValue ="Mohamed Rahali";
ConfirmTextValue ToSpeechPromptChore.addInput ("来自"、FromOut");
String FromValue="Mohamed Rahali";ConfirmTextValue ="7680";ConfirmToTextValue";ConfirmText165391ToText1680"; pulse uno para conocer valores medios de las últimas 24 horas";
ConfirmTextToSpeechPromptChore.addInput ("FailedText"、FailedTextSecret);
String MaxDigitsValue ="1";Value
TextToSpeechPromptChore.addInput ("MaxDigitsise"、FailedTextValue");String MaxDigitechCode.1pintrabe1
;"SecretValue1;"PrevertechobeDataCode.1pintrabeq1;"pintrabeData1;"pintrabeDataCode.q1 ConfirmTextToSpeechPromptChoreo.setChoreo("/Library/Nexmo/Voice/ConfirmTextToSpeechPrompt");
//运行 choreo
unsigned int returnCode = ConfirmTextToSpeechPromptChoreo.run();
//返回代码为零意味着在
(返回代码= 0){时所有操作都正常
while (ConfirmTextToSpeechPromptChoreo.available ()){
string name = ConfirmTextToSpeechPromptChoreo.readStringUntil ('\x1F');
name.trim ();
ConfirmTextToSpeechPromptChoreo.find ("\x1E");
}
{
*
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// */
* SMS 功能 /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
//
void SendSMSchoreo (void){
TembooChoreo SendSMSChoreo (client_1);
//调用 Temboo 客户端
SendSMSChoreo.begin();
//设置 Temboo 帐户凭据
SendSMSChoreo.setAccountName(TEMBOO_ACCOUNT);
SendSMSChoreo.setAppKeyName(TEMBOO_APP_KEY_NAME);
SendSMSChoreo.setAppKey(TEMBOO_APP_KEY);
//设置配置文件以用于执行
SendSMSChoreo.setProfile("SMStwilio");
//设置 Choreo 输入
字符串 OutTimeOut="1";
SendSMSChCallo.addInput ("IDTimeOut"
、"BackTimeOutNumber");SendSMTimeStack.AddValue ="09";"IDTimeBackNumber.TimeOut";
字符串 BodyValue ="CC3100远程更新。 Niveles dentro de rango de seguridad。 La Frecuencia Tiva detectada es de;
BodyValue = BodyValue +(Freq/1000000)+"MHz. El Voltaje_Tiva detectado es de "+volte_1;
BodyValue = Bodyvol +"V, la temperatura_Node1"+温度+"°C,el voltaje_Node1 es"+ vol;Value
= BodyValue +"V, la temperatura_Node2"+ Temperature +"°C,el Estudoes +"V。 Hasta pron.";
SendSMSChoreo.addInput ("身体"、BodyValue);
//识别 Choreo 以运行
SendSMSChoreo.setChoreo("/Library/Twilio/SMSMessages/SendSMS");
//运行 Choreo;如果结果可用,请将其打印为串行
// 901时间等待 Choreo 响应。 可根据需要进行编辑
// use_ssl 输入以告诉库使用 HTTPS
SendSMSChoreo.run(901、use_ssl);
while (SendSMSChoreo.available (){
char c = SendSMSChoreo.read();
serial.print(c);
}SendSMSchoreo.close()
;
}////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
*/
* Gmail 函数 /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
/void
SendEmail (void){
TembooChoreo SendEmailChoreo (client_1);
//调用 Temboo 客户端
SendEmailChoreo.begin();
medsimorahali@gmail.com //设置 Temboo 帐户凭据 SendEmailChoreo.setAccountName(TEMBOO_ACCOUNT); SendEmailChoreo.setAppKeyName(TEMBOO_APP_KEY_NAME); SendEmailChoreo.setAppKey(TEMBOO_APP_KEY);//设置 Choreo 输入字符串 FromAddressValue ="cc3100updates@gmail.com;SendEmailChAddresso.addInput ("FromTo3100");"SendUserNameValue"
;"SendUserName.ToName";"CC100DToName"
string MessageBodyValue ="CC3100远程更新。 Niveles dentro de rango de seguridad。 La Frecuencia Tiva detectada es de;
MessageBodyValue = MessageBodyValue +(Freq/1000000)+"MHz. El Voltaje_Tiva detectado es de "+volte_1;
MessageBodyValue = EstBodyvol +"V、la temperatura_Node1"+温度+"°
°C、el voltaje_Node1 es"+ Value;MessageValue = EstMessageMessagevol +"V、la terminatura_Node2"+"Temperature +"V、el terminature_Nodoe"+"V、"V、"+"V、"vertaje_informe"+"V、"V、"+"V、C +"V 和"V、C +"V。 hasta pron.";
SendEmailChoreo.addInput ("MessageBody "、MessageBody901);
String PasswordValue ="jnezwawthisucjqr";
SendEmailChoreo.addInput ("密码"、PasswordValue);
//识别 Choreo 以运行
SendEmailChoreo.setChoreo("/Library/Google/Gmail/SendEmail");
//运行 Choreo;当结果可用时
,等待串行响应打印/。 可根据需要进行编辑
// use_SSL 输入,以告诉库使用 HTTPS
SendEmailChoreo.run();
while (SendEmailChoreo.available (){
char c = SendEmailChoreo.read();
serial.print(c);
}SendemailChoreo.close()
;
}//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
*/
* Twitter 功能 /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
//
void Sendtweet (void){
TembooChoreo StatusesUpdateChoreo (client_1);
//调用 Temboo 客户端
StatusesUpdateChoreo.begin();
//设置 Temboo 帐户凭据
StatusesUpdateChoreo.setAccountName(TEMBOO_ACCOUNT);
StatusesUpdateChoreo.setAppKeyName(TEMBOO_APP_KEY_NAME);
StatusesUpdateChoreo.setAppKey(TEMBOO_APP_KEY);
//设置 Choreo 输入
字符串 StatusUpdateValue ="CC3100远程更新。 F-Tiva=";
StatusUpdateValue = StatusUpdateValue +(Freq/1000000)+" MHz。 V-Tiva="+ VOLTGE_1;
StatusUpdateValue = StatusUpdateValue +"V, V_Node1="+vol+"V, t_Node1="+temperature;
StatusUpdateValue = StatusUpdateValue +"°C,V_Node2="+vol+"V, t_Node2="+vol+"V,t_Node2="°C +"+vol+"+温度"。 Hasta pron.";
StatusesUpdateChore.addInput ("SecretusUpdate"、StatusUpdateValue);
字符串消耗性键值="qCeCnJi3LRIFDXc5RIPa79Ep";
StatusesConsumerUpdateChore.addInput ("SrKeyKeyKeyKeyKeyKey"、"QFN
)
;"QFN QFN QFN QFN QFN QFN QFN QFN QFN QFN QFN 1 QFN 1 QFN 1 QFN QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 QFN 1 V0QFN 1 V 1 V 1 V 1 V 1 V 1 V 1 QFN 1 QFN 1 V 1 QFN 1 QFN 1 QFN 1 V QFN 1 QFN 1 V 1 QFN 1 QFN 1 QFN 1 V 1
StatusesUpdateChoreo.setChoreo("/Library/Twitter/Tweets/StatusesUpdate");
当结果可用时、将其打印为串行
// 901时间等待 Choreo 响应。 可根据需要进行编辑
// use_ssl 输入以指示库使用 HTTPS
StatusesUpdateChoreo.run(901、use_ssl);
while (StatusUpdateChore.available (){
char c = StatusUpdateChoreo.read();
serial.print(c);
}
StatusUpdateChore.close();
}
void setup(){
Serial.begin(115200);//初始化串行通信
WifiSettings();
Serial.println ("在端口80上启动 webserver ");
server.begin(); //在端口80
Serial.println ("Webserver started!")、
PubNub.begin(pubkey 子项)、
Serial.println ("PubNub setup")、
RF430CL()、
}上启动 Web 服务器
void loop(){//
WiFiClient *CLIENT;
// Publish *//
Serial.print("publishing a message:");
aJsonObject *msg = createMessage();
char *msgStr = aJson.print(msg);
aJson.deleteItem(msg);
client = PubNub.publishing (channel、msgStr);
free(msgStr);
// if (!client){
//return;
//}
int i = 0;
WiFiClient client_1 = server.available ();//侦听传入的 Web 服务器客户端
(如果(client_1){ //如果您有一个客户端,
serial.println ("新客户端"); //从串行端口打印一条消息
char buffer[150]={
0}; //创建缓冲区来保存传入的数据 //创建缓冲区以保存传入数据(GRE_LED)
while (client_1_connected()){ //在客户端连接时循环
if (client_1_available (){ //如果有字节要从客户端读取,
char c = client_1_read(); //读取一个字节,然后
serial.write(c); //将其打印出串行监视器
如果(c ='\n'){ //如果字节是换行字符
if (strlen (buffer)=0){
client_1.println ("HTTP/1.1 200 OK");
client_1_println ("内容类型:text/html");
client_1.println ("连接:关闭");// se Cierra la conexión una vez se ha responsido a la peticion
client_1_println ("\n 刷新:5");// se brunca la página automáticamente cada 5 segundos
client_1_println();
client_1.println (" proyecto realizado en Las instalaciones de la UCLM por ");
client_1.println ("\n\n");
client_1_println (" Mohamed RAHALI <\p>");
client_1.println ("\n\n");
client_1_println();
client_1_println ("");
client_1.println ("
");//client_1.println (" <html lang='es'>");client_1.println (" <head>
<META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=utf-8" />
");client_1.println (" <meta charset='UTF-8'>");//client_1.println (" <title>");
client_1_println ("servicios multimedia para El control de Alertas");
client_1.println (" <hr>");
client_1.println (" ");="" client_1.println("rel="stylesheet" type="text/css">");="" client_1.println("href="static.tumblr.com/.../estilos.min.css">");
client_1.println ("
");
client_1.println (" 伺服系统多媒体参数 EL 控制 DE 警报
");
client_1.println ("
");
// mm cuidado H1
client_1.println (" 物联网 Web 服务器 ");
client_1.println (" ");//client_1_println (");client_1_println ("www.educachip.com"); client_1_println (");client_1_println (");client_1_println (") ");
client_1.println ("\n\n");
/-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------- //
//正文多媒体(SMS、电话呼叫)
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" 伺服 Móviles
");//client_1.println (" ");client_1.println (" ");client_1.println (" ");client_1_println ("LED Verde");client_1_println ("
");client_1.println (" ");client_1.println (" ");
client_1.println (" ");//client_1.println (" ");
client_1.println (" ");
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" ");//client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1_println();
//正文电子邮件
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" 邮件
");//client_1.println (" ");client_1.println (" ");client_1.println (" ");client_1_println ("LED Verde");client_1_println ("
");client_1.println (" ");client_1.println (" ");
//aqui Solo una de las dos、无 TODO
client_1.println (" ");//client_1.println (" ");
client_1.println (" ");
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" ");//client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1_println();
client_1.println (" ");
//社交媒体
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" 社交媒体
");//client_1.println (" ");client_1.println (" ");client_1.println (" ");client_1_println ("LED Verde");client_1_println ("
");client_1.println (" ");client_1.println (" ");
client_1.println (" ");//client_1.println (" ");
client_1.println (" ");
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" ");//client_1.println (" ");
//client_1_println ("");//client_1_println (" ");
//client_1_println ("链接按钮");
client_1.println (" ");
//client_1.println (" ");
client_1.println (" ");//client_1.println (" ");client_1.println (" ");client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1_println();
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
client_1.println (" ");
// HTTP 响应以另一行结尾:
client_1_println();
//中断 while 循环:
中断;
}
否则{ //如果有换行符,则清除缓冲区:
memset (buffer、0、150);
// memset (buffer2、0、150);
I = 0;
}
}
如果(c!='\r'){//如果您除了回车字符之外还有其他任何内容,
Buffer[i++]= c; //将其添加到 currentLine 的末尾
//buffer2[i++]= c;
}
//检查客户端请求是"get /h"还是"get /L":
if (endsWith (buffer、"get /Multimedia = 1"){
SendSMSChoreo();
serial.println ("\nSMS 已发送\n");
}
if (endsWith (buffer、"get /Multimedia = 0"){
callphone();
serial.println ("\n 电话呼叫已进行");
}
if (endsWith (buffer、"get /Mail=1"){
SendEmail();
serial.println ("\n 电子邮件已发送");
}
// if (endsWith (buffer、"get /Mail=0"){
//
//}
if (endsWith (buffer、"get /Social = 1"){
Sendtweets();
serial.println ("\nTwitter 已更新");
//
}
// if (endsWith (buffer、"get /Social = 0"){
//
//}
}
client_1_stop(); //关闭连接:
serial.println ("客户端断开连接");
}//-------
DLP-RF430CL 环路------------------------------------------------------- //
if (nFC.loop()){
if (nFC.wasRead ()){
serial.println ("NDEF 标签已读取!");
}
nfc.enable();
}
//
////检查一个数组是否以另一个数组结尾的方法
//
布尔 endsWirh (char* inString、char* compString){
int compLength = strlen (compString);
int strLength = strlen (inString);
//比较 incompI 的最后"compLength "值
;
for (i+ i);(i+ I = 0+)
char a = inString[(strLength - 1)- i];
char b = compString[(compLength - 1)- i];
如果(a!= b){
返回 false;
}
}
返回 true;
}//-----------------
printWifiStatus 函数------------------------------------------------------- //
void printWifiStatus(){
Serial.print ("SSID:"); //打印连接到的网络的 SSID:
serial.println (WiFi.ssid ());
IPAddress IP = WiFi.localIP ();//打印 WiFi IP 地址:
serial.print ("IP 地址:");
serial.println (IP);
长 RSSI = WiFi.ssi (); //打印接收到的信号强度:
serial.print ("信号强度(RSSI):");
serial.print (RSSI);
serial.println (" dBm");
serial.print ("要实际查看此页,请打开浏览器至 http://"); //在浏览器中打印转至何处:
serial.println (IP);
}
大家好、我遇到了一个小问题、下面我要处理通信协议的应用、我有 Tiva 硬件、CC2530空中模块、用于 WIFI 的 CC3100、我还可以使用 DLP-RF430CL330H。
单独运行很好、但当我将它们放在一起、在代码中安装所有 BoosterPack (一个在另一个之上)时、它对我没有任何作用、我甚至看不到串行端口被启用。 什么也不起作用。 我只需将这些片段复制并粘贴到单个代码中。
有人能告诉我问题可能是什么吗? 板是否存在一定的不兼容性? 或者它是我使用的软件(电源)吗?
我可以激活代码中不应该包含的内容吗?
我如何解决这个问题? 我需要信息或一些帮助、这很紧急。
提前感谢。
我使用 ENEGRIA IDE。V17。 我的代码是: