This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好
我不熟悉 Tm4c123、我想将端口 A 的 GPIO 设为高电平... PA5和 PA6 ...但我在这方面遇到了问题...这是我的代码...请标记问题...谢谢
int main (空)
{
ROM_FPUEnable();
ROM_FPULazyStackingEnable();
//将时钟设置为80MHz
ROM_SysCtlClockSet (SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHz|SYSCTL_SYSDIV_2_5);
ROM_SysCtlPeripheralEnable (SYSCTL_Periph_GPIOA);
GPIOPinTypeGPIOOutput (GPIO_Porta_base、GPIO_PIN_5| GPIO_PIN_6);
GPIOPinWrite (GPIO_Porta_base、GPIO_PIN_5 | GPIO_PIN_6、0x60);
}