This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP432E401Y:通过运行 bat 文件一次、可同时刷写2个不同的映像

Guru**** 2539500 points
Other Parts Discussed in Thread: UNIFLASH, MSP432E401Y

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1186228/msp432e401y-flash-2-different-images-simultaneously-by-running-bat-file-once

器件型号:MSP432E401Y
主题中讨论的其他器件:UNIFLASH

大家好,  

我生成了一个文件夹,其中包含一个 bat 文件,用于使用 Uniflash 的独立命令行将映像刷写到 msp432e401y 中。 但我的问题是,我需要一个接一个地刷新2个不同的图像,每当我运行 bat 文件一次时,任何人都能帮助我解决这个问题。

谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     请参阅 https://software-dl.ti.com/ccs/esd/uniflash/docs/v5_0/quick_start_guide/uniflash_quick_start_guide.html 上的此 Uniflash 快速入门指南。 您应该能够将这两个文件指定为参数。 请参见下面的示例。  

     dslite flash --config=ccxml-file [options] [flash-file1 flash-file2...]
     -c [ --config ] arg                Target Configuration (ccxml) file, must be
                                        supplied other than running --help. CCXML
                                        file can be generated and exported using
                                        the Uniflash GUI or Code Composer Studio.
     -n [ --core ] arg (=0)             Zero based index of core to operate on.
     -S [ --list-settings ] arg         Takes a regex and list the final values
                                        applied to the matching settings. (ie; use
                                        .* to list all available settings)
     -p [ --list-ops ]                  List the available flash operations.
     -I [ --list-device-cmds ]          List the available device commands, if
                                        any.
     -l [ --load-settings ] arg         Apply settings file generated by UniFlash
                                        GUI.
     -s [ --setting ] arg               Override a specific setting by using
                                        id=value.  Can be specified multiple
                                        times.
     -b [ --before ] arg                Operation(s) to perform before loading.
                                        Can be specified multiple times, and are
                                        performed in the order they appear on the
                                        command line. Get a list of operations by
                                        using --list-ops.
     -f [ --flash ]                     Load the file(s) specified at the end of
                                        the command line to flash.  This is
                                        assumed to be set unless verify is set.
     -v [ --verify ]                    Verify the file(s) specified at the end of
                                        the command line.
     -a [ --after ] arg                 Optional operation to perform after
                                        loading.  Can be specified multiple times,
                                        and are performed in the order they appear
                                        on the command line. Get a list of
                                        operations by using --list-ops.
     -R [ --list-resets ]               List of resets that can be done after
                                        program load and verification.
     -r [ --reset ] arg                 Set reset operation to be done after
                                        program load and verification.
     -O [ --post-flash-device-cmd ] arg Execute the given device command. Get a
                                        list of device commands by using
                                        --list-device-cmds.
     -t [ --timeout ] arg               Timeout in seconds, infinite if
                                        unspecified.
     -g [ --log ] arg                   Enable detailed logging to the specified
                                        file.
     -e [ --verbose ]                   Outputs progress messages to the console.
     -h [ --help ]                      Print this message.