This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C123GH6PZ:两个系统时钟速度的配置

Guru**** 2925690 points

Other Parts Discussed in Thread: EK-TM4C1294XL

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1224050/tm4c123gh6pz-configuration-of-two-system-clock-speed

器件型号:TM4C123GH6PZ
主题中讨论的其他器件:EK-TM4C1294XLTM4C123

如何在两个不同的系统时钟速度之间配置和切换?

例如、我需要在常规运行(主电源打开)期间使用80MHz 时钟速度、在低功耗模式和备用电池(主电源关闭)期间使用40MHz 时钟速度?

我的程序应该正常运行在80MHz、主电源打开时、它应该在检测到主电源关闭条件时切换到40MHz 的不同系统时钟速度。

请共享示例代码以执行上述任务。