This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP432E411Y:使用 UART1进行应用更新的定制 BSL

Guru**** 2874300 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1212211/msp432e411y-custom-bsl-using-uart1-for-app-updating

器件型号:MSP432E411Y

您好!  

我们的 HW 包括 USB 转 UART 桥接器(FT234XD)。 我们希望将桥的 UART 输出连接到 MSP43241152的 UART1端口,并通过桥执行应用更新。 显然、需要在闪存中对使用 UART1的自定义引导加载程序进行编程。 除此之外,这项计划的可行性和容易程度如何?

此致、Magda

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     我建议您首先在 C:\ti\simplelink_msp432e4_sdk_4_20_00_12\examples\nortos\MSP_EXP432E401Y\boot_loader\boot_serial_uart_flash 处尝试基于闪存的串行 UART 引导加载程序示例。 本示例使用 UART0。 但在 bl_config.h 文件中、您可以指定 UART1等其他 UART 实例作为引导加载端口。 您需要将 bl_config.h 中定义的宏从 UART0更改为 UART1。 有关 UART0的内容、请参见下文。

    //*****************************************************************************
    //
    // Selects the baud rate to be used for the UART.
    //
    // Depends on: UART_ENABLE_UPDATE, CRYSTAL_FREQ
    // Exclusive of: UART_AUTOBAUD
    // Requires: None
    //
    //*****************************************************************************
    #define UART_FIXED_BAUDRATE     115200
    
    //*****************************************************************************
    //
    // Selects the clock enable for the UART peripheral module
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UARTx
    //
    //*****************************************************************************
    #define UART_CLOCK_ENABLE     SYSCTL_RCGCUART_R0
    
    //*****************************************************************************
    //
    // Selects the base address of the UART peripheral module
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_CLOCK_ENABLE
    //
    //*****************************************************************************
    #define UARTx                 UART0
    
    //*****************************************************************************
    //
    // Selects the clock enable for the GPIO corresponding to UART RX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_RXPIN_BASE, UART_RXPIN_PCTL and UART_RXPIN_POS
    //
    //*****************************************************************************
    #define UART_RXPIN_CLOCK_ENABLE  SYSCTL_RCGCGPIO_R0
    
    //*****************************************************************************
    //
    // Selects the base address for the GPIO corresponding to UART RX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_RXPIN_CLOCK_ENABLE, UART_RXPIN_PCTL and UART_RXPIN_POS
    //
    //*****************************************************************************
    #define UART_RXPIN_BASE          GPIOA
    
    //*****************************************************************************
    //
    // Selects the port control value for the GPIO corresponding to UART RX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_RXPIN_CLOCK_ENABLE, UART_RXPIN_BASE and UART_RXPIN_POS
    //
    //*****************************************************************************
    #define UART_RXPIN_PCTL          0x1
    
    //*****************************************************************************
    //
    // Selects the pin number for the GPIO corresponding to UART RX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_RXPIN_CLOCK_ENABLE, UART_RXPIN_BASE and UART_RXPIN_PCTL
    //
    //*****************************************************************************
    #define UART_RXPIN_POS           0
    
    //*****************************************************************************
    //
    // Selects the clock enable for the GPIO corresponding to UART TX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_TXPIN_BASE, UART_TXPIN_PCTL and UART_TXPIN_POS
    //
    //*****************************************************************************
    #define UART_TXPIN_CLOCK_ENABLE  SYSCTL_RCGCGPIO_R0
    
    //*****************************************************************************
    //
    // Selects the base address for the GPIO corresponding to UART TX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_TXPIN_CLOCK_ENABLE, UART_TXPIN_PCTL and UART_TXPIN_POS
    //
    //*****************************************************************************
    #define UART_TXPIN_BASE          GPIOA
    
    //*****************************************************************************
    //
    // Selects the port control value for the GPIO corresponding to UART TX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_TXPIN_CLOCK_ENABLE, UART_TXPIN_BASE and UART_TXPIN_POS
    //
    //*****************************************************************************
    #define UART_TXPIN_PCTL          0x1
    
    //*****************************************************************************
    //
    // Selects the pin number for the GPIO corresponding to UART TX pin
    //
    // Depends on: UART_ENABLE_UPDATE
    // Exclusive of: None
    // Requires: UART_TXPIN_CLOCK_ENABLE, UART_TXPIN_BASE and UART_TXPIN_PCTL
    //
    //*****************************************************************************
    #define UART_TXPIN_POS           1