This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1290NCPDT:模拟输入序列发生器不会返回所有通道

Guru**** 2943400 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1247893/tm4c1290ncpdt-analog-input-sequencer-is-not-returning-all-channels

器件型号:TM4C1290NCPDT

下面是我们针对模拟输入序列发生器的源代码实现。 在处理器启动时调用初始化函数、而 Read_local_inputs 函数被定期调用以获取 ADC 数据。 Low_Voltage_Detection_Entry 和 Nominal _Voltage_Detection_Entry 是用于 ADC0序列0和 ADC1序列0上比较器的函数。 我们观察到+24V、+15V 和驱动温度具有错误的读数。 我们已使用电压探头检查硬件、且处理器获取这些引脚的预期电压、因此我们排除了任何硬件问题。

我们希望您输入可能导致读取错误的内容、或者我们可以采取哪些步骤来解决此问题。

void Analog_Task::Initialize()
{
    Error_Block adc0ss0_eb;
    Error_Block adc1ss0_eb;
#ifndef TEST_HARNESS
    Hwi_Params adc0ss0_hwi_params;
    Hwi_Params adc1ss0_hwi_params;
#endif

    //  Enable ADC0 peripheral
    SysCtlPeripheralEnable( SYSCTL_PERIPH_ADC0 );

    //  Enable ADC1 peripheral
    SysCtlPeripheralEnable( SYSCTL_PERIPH_ADC1 );

    //  Configure trigger sequence to trigger on a processor request
    /*
     * ADC 0 Sequence 0:
     *      -   ADC0AIN1    +24V reference
     *      -   ADC0AIN0    -15V reference
     *      -   ADC0AIN2    +15V reference
     *
     * ADC 0 Sequence 1:
     *      -   ADC0AIN3    +5V reference
     *      -   ADC0AIN13   Drive temperature
     *
     * ADC 1 Sequence 0:
     *      -   ADC1AIN1    +24V reference
     */
    ADCSequenceConfigure( ADC0_BASE, 0, ADC_TRIGGER_PROCESSOR, 0 );
    ADCSequenceConfigure( ADC0_BASE, 1, ADC_TRIGGER_PROCESSOR, 1 );
    ADCSequenceConfigure( ADC1_BASE, 0, ADC_TRIGGER_ALWAYS, 0 );

    //  Setup the ADC0 read sequence 0
    ADCSequenceStepConfigure( ADC0_BASE, 0, 0, ADC_CTL_CH1 | ADC_CTL_CMP0 );
    ADCSequenceStepConfigure( ADC0_BASE, 0, 1, ADC_CTL_CH1 | ADC_CTL_CMP0 );
    ADCSequenceStepConfigure( ADC0_BASE, 0, 2, ADC_CTL_CH0 );
    ADCSequenceStepConfigure( ADC0_BASE, 0, 3, ADC_CTL_CH0 );
    ADCSequenceStepConfigure( ADC0_BASE, 0, 4, ADC_CTL_CH2 );
    ADCSequenceStepConfigure( ADC0_BASE, 0, 5, ADC_CTL_CH2 | ADC_CTL_IE | ADC_CTL_END );

    //  Setup the ADC0 read sequence 1
    ADCSequenceStepConfigure( ADC0_BASE, 1, 0, ADC_CTL_CH3 );
    ADCSequenceStepConfigure( ADC0_BASE, 1, 1, ADC_CTL_CH3 );
    ADCSequenceStepConfigure( ADC0_BASE, 1, 2, ADC_CTL_CH13 );
    ADCSequenceStepConfigure( ADC0_BASE, 1, 3, ADC_CTL_CH13 | ADC_CTL_IE | ADC_CTL_END );

    //  Setup the ADC1 read sequence 0
    ADCSequenceStepConfigure( ADC1_BASE, 0, 0, ADC_CTL_CH1 | ADC_CTL_CMP0 | ADC_CTL_END );

    //  Setup the 24V comparator low voltage trigger
    ADCComparatorConfigure( ADC0_BASE, 0, ADC_COMP_INT_LOW_HONCE );
    ADCComparatorRegionSet( ADC0_BASE, 0, LOW_TRIGGER_ADC_COUNTS, NOMINAL_TRIGGER_ADC_COUNTS );

    //  Setup the 24V comparator recovery trigger
    ADCComparatorConfigure( ADC1_BASE, 0, ADC_COMP_INT_HIGH_HONCE );
    ADCComparatorRegionSet( ADC1_BASE, 0, LOW_TRIGGER_ADC_COUNTS, NOMINAL_TRIGGER_ADC_COUNTS );

    //  Clear the comparator data
    ADCComparatorReset( ADC0_BASE, 0, true, true );
    ADCComparatorReset( ADC1_BASE, 0, true, true );

    //  Create a Hwi for ADC0 sequence 0
    Error_init( &adc0ss0_eb );
    Hwi_Params_init( &adc0ss0_hwi_params );
    Hwi_construct( &( adc0ss0_hwi_struct ),
                   INT_ADC0SS0,
                   Analog_Task::Low_Voltage_Detection_Entry,
                   &adc0ss0_hwi_params,
                   &adc0ss0_eb );

    //  Create a Hwi for ADC1 sequence 0
    Error_init( &adc1ss0_eb );
    Hwi_Params_init( &adc1ss0_hwi_params );

    //  Set the low voltage interrupt to the highest priority (0)
    adc1ss0_hwi_params.priority = 0;
    Hwi_construct( &( adc1ss0_hwi_struct ),
                   INT_ADC1SS0,
                   Analog_Task::Nominal_Voltage_Detection_Entry,
                   &adc1ss0_hwi_params,
                   &adc1ss0_eb );

    //  Enable the comparator interrupts
    ADCComparatorIntEnable( ADC0_BASE, 0 );
    ADCComparatorIntEnable( ADC1_BASE, 0 );

    //  Clear any pending interrupts
    ADCIntClear( ADC0_BASE, 0 );
    ADCIntClear( ADC1_BASE, 0 );

    //  Enable the sequences
    ADCSequenceEnable( ADC0_BASE, 0 );
    ADCSequenceEnable( ADC0_BASE, 1 );
    ADCSequenceEnable( ADC1_BASE, 0 );

    //  Enable the comparator interrupt sources
    ADCIntEnableEx( ADC0_BASE, ADC_INT_DCON_SS0 );
    ADCIntEnableEx( ADC1_BASE, ADC_INT_DCON_SS0 );

    //  Enable the comparator interrupts
    ADCIntEnable( ADC1_BASE, 0 );
    ADCIntEnable( ADC1_BASE, 0 );

    //  Enable the ADC0 sequence 0 interrupt
    IntEnable( INT_ADC0SS0 );

    //  Enable the ADC1 sequence 0 interrupt
    IntEnable( INT_ADC1SS0 );
    //  Assert the low power detection pin to notify DSP nominal voltage is detected
    GPIO_Out_HI( LOW_POWER_DET );
}

void Analog_Task::Read_Local_Inputs()
{
    //  Clear the interrupt mask
    ADCIntClear( ADC0_BASE, 0 );
    ADCIntClear( ADC0_BASE, 1 );

    //  Trigger the analog read
    ADCProcessorTrigger( ADC0_BASE, 0 );
    ADCProcessorTrigger( ADC0_BASE, 1 );

    //  Wait for reads to complete
    while ( !ADCIntStatus( ADC0_BASE, 0, false ) )
    {
    }
    while ( !ADCIntStatus( ADC0_BASE, 1, false ) )
    {
    }
    //  Grab the latest input readings
    ADCSequenceDataGet( ADC0_BASE, 0, m_adc0_seq0 );
    ADCSequenceDataGet( ADC0_BASE, 1, m_adc0_seq1 );
}

void Analog_Task::Low_Voltage_Detection_Entry( UArg )
{
    uint32_t adc_comparator_status;

    //  Get the interrupt status
    adc_comparator_status = ADCComparatorIntStatus( ADC0_BASE );

    //  Clear the asserted interrupts
    ADCComparatorIntClear( ADC0_BASE, adc_comparator_status );

    //  Inactivate the warehouse task
    //  TODO - Need to add back in once on production board
    //Task_setPri( g_wh_task_handle, -1 );

    //  De-assert the low power detection pin to notify DSP low voltage is detected
    GPIO_Out_LO( LOW_POWER_DET );
}

void Analog_Task::Nominal_Voltage_Detection_Entry( UArg )
{
    uint32_t adc_comparator_status;

    //  Get the interrupt status
    adc_comparator_status = ADCComparatorIntStatus( ADC1_BASE );

    //  Clear the asserted interrupts
    ADCComparatorIntClear( ADC1_BASE, adc_comparator_status );

    //  Activate the warehouse task
    //  TODO - Need to add back in once on production board
    //Task_setPri( g_wh_task_handle, WAREHOUSE_TASK_PRIORITY );

    //  Assert the low power detection pin to notify DSP nominal voltage is detected
    GPIO_Out_HI( LOW_POWER_DET );
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     您能详细说明什么是错误读数吗? 您读过什么、预期读数是多少?

     在读取第35和36行的代码时、我不明白您为什么要同时为 COMP0分配步骤0和1。 在这里、您要指定序列发生器0中的样本0和1以供数字比较器单元0进行比较。  

     另请注意、当您为比较器使用步骤0和1 (采样0和1)时、该值不会保存到 FIFO 中。 如果希望将样本0和1的 ADC 对话值保存在 FIFO Toso 中、则可稍后在比较该值的同时读出、但不会发生这种情况。

    最后,请参阅勘误表 ADC#14,看看它是否适用于您的观察结果。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    抱歉、第36行应该是比较器1、不知道在我们发送的版本中它是如何更改为0的。 如果 FIFO 中不存在使用比较器的阶跃、是否可以访问比较器中断中的值? 这也适用于带有 ADC_CTL_IE 的步骤吗?

    谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Bryan:

    如果使用比较器的步骤在 FIFO 中不可用,是否有办法访问比较器中断中的值?

     请参阅以下描述。 当通道发送到比较器时、其转换值不保存到 FIFO 中。 您可以尝试 对 具有 ADC_CTL_CMP0 标志的比较器使用一个步骤、同时为没有标志的同一通道专用另一个步骤。 这样、 ADC_CTL_CH1转换值仍会保存 到 FIFO 中。  

    这是否也适用于带有 ADC_CTL_IE 的步骤?

    否、不适用于 ADC_CTL_IE。 ADC_CTL_IE 仅表示相应通道转换完成时产生中断。 在上述代码中、转换步骤5后将生成中断。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    抱歉线36应该是比较器1

    还有一点、与每个比较器单元相关联、您可以设置上下键合值。 请参阅以下说明。 无需使用两个不同的比较器单元来设置上限和下限。 您似乎是打算使用两个不同的比较器单元来设置两个不同的界限值。