主题中讨论的其他器件: UNIFLASH、 SEGGER、MSPM0G3507
我有一个 LP-MSPM0G3507板、我尝试使用 CCS 构建的 MSPM0 SDK 示例中的二进制文件进行刷写。
不幸的是、我无法访问内核。
XDS110 USB 调试探针
当尝试从 CSS 刷新时、我收到以下消息:
Error connecting to the target: (Error -614 @ 0x0) The target indicates there is an error condition from a previous SWD request. Clear the error the condition, and try the SWD request again.
J-Link Ultra+调试探针
当我从 J101断开 SWD 并将 J-Link Ultra+连接到 J103、启动 J-Link Commander 并尝试进行连接时、我得到:
AP[0]: Stopped AP scan as end of AP map seems to be reached Iterating through AP map to find AHB-AP to use Attach to CPU failed. Executing connect under reset. DPIDR: 0x6BA02477 CoreSight SoC-400 or earlier Scanning AP map to find all available APs AP[0]: Stopped AP scan as end of AP map has been reached Iterating through AP map to find AHB-AP to use Could not find core in Coresight setup Cannot connect to target.
在我看来、器件似乎是以某种方式锁定了或处于不再接受 SWD 命令的状态。
有任何提示/想法、我可以做些什么来让它恢复运行?