This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] EK-TM4C1294XL:基于 ARM 的微控制器论坛

Guru**** 2425610 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1323076/ek-tm4c1294xl-arm-based-microcontrollers-forum

器件型号:EK-TM4C1294XL

您好!

我们将 CCS 项目配置为执行单元测试(使用寄生软件)。

同时生成测试适合和测试用例.

/resized-image/__size/1200x426/__key/communityserver-discussions-components-files/908/2273.ERROR.png

下面是链接器脚本:-

/*
 * Copyright (c) 2013, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */
/*
 *  ======== DK_TM4C129X.cmd ========
 *  Define the memory block start/length for the TM4C129XNCZAD
 */

/* The starting address of the application.  Normally the interrupt vectors  */
/* must be located at the beginning of the application.                      */
#define APP_BASE 0x00004000
#define RAM_BASE 0x20000000
#define SDRAM_BASE 0x60100000

MEMORY
{
    FLASH (RX) : origin = APP_BASE, length = 0x000FC000

	/* For EVT Board */
    SRAM (RWX) : origin = 0x20000000, length = 0x00040000
	/* For EDT Board  comment above line and uncomment below line */
	//SRAM (RWX) : origin = 0x20000000, length = 0x00020000
	SDRAM (RW): origin = SDRAM_BASE, length = 0x100000
}

/* The following command line options are set as part of the CCS project.    */
/* If you are building using the command line, or for some reason want to    */
/* define them here, you can uncomment and modify these lines as needed.     */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone.              */
/*                                                                           */
/* --heap_size=0                                                             */
/* --stack_size=256                                                          */
/* --library=rtsv7M4_T_le_eabi.lib                                           */

/* Section allocation in memory */

SECTIONS
{
    .intvecs:   > APP_BASE
    .text   :   > FLASH
    .const  :   > FLASH
    .cinit  :   > FLASH
    .pinit  :   > FLASH
    .init_array : > FLASH

    .vtable :   > RAM_BASE
    .data   :   > SRAM
    .bss    :   > SRAM
    .sysmem :   > SRAM
    .stack  :   > SRAM
    .sdram  :   > SDRAM

    .sdram{
      // rechargeIcons.obj(.const)
      // disinfectionIcons.obj(.const)
    } > SDRAM
}

__STACK_TOP = __stack + 512;

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     从链接器文件的角度来看、我唯一看到缺少的 er 文件是 --retain=g_pfnVectors。 除此之外、我不会注意到链接器文件有问题。 我认为 这个问题与 您的应用程序有关、因为该错误抱怨.const 需要0x2c12b 字节、而内存中只有0x281b8字节的闪存。 您的.text (您的应用程序)太大、因此.const 没有剩余空间。 请注意、器件中只有1MB 闪存。