Other Parts Discussed in Thread: MSPM0G3507, TCAN1042DEVM
主题中讨论的其他器件:MSPM0G3507、 TCAN1042DEVM
您好、TI 团队:
我遇到了在 CRO 上进行 CAN 传输信号检测的问题。
我正在使用 MSPM0G3507 Launchpad 中"mspm0_SDK_1_20_01_06"的"mcan_multi_message_tx"示例代码。 在此代码中、我注释了微控制器等待开关按压的部分。
我 没有 适用于 CAN 的 TCAN1042DEVM 板。 我只是检查 CRO 上 PA12引脚上的 CAN 发送信号。 但是、 将探头连接到 CAN TX 引脚 PA12时、CRO 上不会显示数据/波形。
是否可以在不使用 TCAN1042DEVM 板的情况下获得 CRO 上的数据/波形? 请帮助我解决此问题。
以下是我使用的代码
/*
* Copyright (c) 2021, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
#include "ti_msp_dl_config.h"
#define LED0_STATUS_ON ((uint8_t) 0x01)
#define LED0_STATUS_OFF ((uint8_t) 0x00)
#define LED1_STATUS_ON ((uint8_t) 0x01)
#define LED1_STATUS_OFF ((uint8_t) 0x00)
volatile bool gTXMsg;
volatile bool error;
int main(void)
{
DL_MCAN_TxBufElement txMsg0;
DL_MCAN_TxBufElement txMsg1;
SYSCFG_DL_init();
/* Initialize message0 to transmit. */
/* Identifier Value. */
txMsg0.id = ((uint32_t)(0x4)) << 18U;
/* Transmit data frame. */
txMsg0.rtr = 0U;
/* 11-bit standard identifier. */
txMsg0.xtd = 0U;
/* ESI bit in CAN FD format depends only on error passive flag. */
txMsg0.esi = 0U;
/* Transmitting 4 bytes. */
txMsg0.dlc = 1U;
/* CAN FD frames transmitted with bit rate switching. */
txMsg0.brs = 1U;
/* Frame transmitted in CAN FD format. */
txMsg0.fdf = 1U;
/* Store Tx events. */
txMsg0.efc = 1U;
/* Message Marker. */
txMsg0.mm = 0xAAU;
/* Data bytes. */
txMsg0.data[0] = LED0_STATUS_ON;
/* Initialize message1 to transmit. */
/* Identifier Value. */
txMsg1.id = ((uint32_t)(0x3)) << 18U;
/* Transmit data frame. */
txMsg1.rtr = 0U;
/* 11-bit standard identifier. */
txMsg1.xtd = 0U;
/* ESI bit in CAN FD format depends only on error passive flag. */
txMsg1.esi = 0U;
/* Transmitting 4 bytes. */
txMsg1.dlc = 1U;
/* CAN FD frames transmitted with bit rate switching. */
txMsg1.brs = 1U;
/* Frame transmitted in CAN FD format. */
txMsg1.fdf = 1U;
/* Store Tx events. */
txMsg1.efc = 1U;
/* Message Marker. */
txMsg1.mm = 0xAAU;
/* Data bytes. */
txMsg1.data[0] = LED1_STATUS_ON;
//NVIC_EnableIRQ(GPIO_SWITCHES_INT_IRQN);
while (DL_MCAN_OPERATION_MODE_NORMAL != DL_MCAN_getOpMode(MCAN0_INST))
;
while (1) {
/* Waits until button is pressed to send the message*/
/*
while (gTXMsg == false) {
__WFE();
}
gTXMsg = false;
if (txMsg0.data[0] == LED0_STATUS_ON) {
txMsg0.data[0] = LED0_STATUS_OFF;
} else {
txMsg0.data[0] = LED0_STATUS_ON;
}
if (txMsg1.data[0] == LED1_STATUS_ON) {
txMsg1.data[0] = LED1_STATUS_OFF;
} else {
txMsg1.data[0] = LED1_STATUS_ON;
}
*/
/* Write Tx Message to the Message RAM. */
DL_MCAN_writeMsgRam(MCAN0_INST, DL_MCAN_MEM_TYPE_BUF, 0, &txMsg0);
/* Write Tx Message to the Message RAM. */
DL_MCAN_writeMsgRam(MCAN0_INST, DL_MCAN_MEM_TYPE_BUF, 1, &txMsg1);
/* Add request for transmission. */
DL_MCAN_TXBufAddReq(MCAN0_INST, 0);
/* Add request for transmission. */
DL_MCAN_TXBufAddReq(MCAN0_INST, 1);
}
}
void GROUP1_IRQHandler(void)
{
switch (DL_Interrupt_getPendingGroup(DL_INTERRUPT_GROUP_1)) {
case GPIO_SWITCHES_INT_IIDX:
switch (DL_GPIO_getPendingInterrupt(GPIO_SWITCHES_PORT)) {
case DL_GPIO_IIDX_DIO21:
gTXMsg = true;
break;
default:
break;
}
break;
default:
break;
}
}
感谢您发送
迪帕克