This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM2632:提供符合安全标准的支持套件

Guru**** 2763595 points

Other Parts Discussed in Thread: HALCOGEN, AM2632

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1276679/am2632-safety-compliant-support-package-availability

器件型号:AM2632
主题中讨论的其他器件:HALCOGEN

您好!

我浏览了 适用于 TMS570系列的 SafeTI HALCoGen 合规性支持包、以符合 IEC 61508和 ISO 26262等功能安全标准。

AM2632系列是否有任何此类支持? 是否有关于将 AM2632系列用于 SIL4系统设计的任何具体建议/意见?