This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1294KCPDT:TM4C1294 EVK

Guru**** 2803255 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1252586/tm4c1294kcpdt-tm4c1294-evk

器件型号:TM4C1294KCPDT

大家好、

IAM 尝试在 TM4C1294 EVK (免费 RTOS + LWIP)中进行以太网通信、以便使用演示代码  Enet_tcpecho_client_lwip (无免费 RTOS)、  

所以、我曾尝试将免费 RTOS 与以太网接收 和发送任务集成在一起、但在连接建立阶段我的代码却受到了冲击。

我只需要一个演示项目(免费 RTOS + LWIP + TM4C1294 EVK +以太网 客户端发送 和接收 任务),这样我就可以尝试确定 API 步骤并尝试解决问题

当前 IAM 使用以下工程、但不含免费 RTOS 的演示工程

采取必要措施解决问题

 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    Unknown 说:
    我只需要一个演示项目(免费 RTOS + LWIP + TM4C1294 EVK +以太网 客户端发送 和接收 任务),这样我就可以尝试确定 API 步骤并尝试解决问题[/报价]

    抱歉、我们没有免费 RTOS + LWIP + TM4C1294 EVK +以太网 客户端    TM4C129的发送和接收任务这样的项目。 非 RTOS RAW  Enet_tcpecho_client_lwip 是我们针对 lwIP 提供的唯一客户端示例。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    团队成员

    您能给我们提供 TM4C1294 EVK 的 I2C 代码吗,因为我们 在我们的代码中看不到任何时钟初始化, 如果 需要在我们的代码中进行任何更改,请更正我们。
    请尽快返回。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    //============================================================================
    // Name        : i2cAPI.c
    // Author      :
    // Version     :
    // Copyright   : Your copyright notice
    // Description : Tiva i2c in C++, Ansi-style
    //============================================================================
    /*
     * i2cAPI.c
     * Implementation of a i2c interface
     *
     * Copyright
     *
     * Redistribution and use in source and binary forms, with or without modification,
     * are permitted provided that the following conditions are met:
     * 1. Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     * 2. Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * THIS SOFTWARE IS PROVIDED ''AS IS'' AND ANY EXPRESS OR IMPLIED WARRANTIES,
     * INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY
     * AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL I
     * BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
     * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE
     * GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
     * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
     * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
     * SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    
    #include <stdint.h>
    #include <stdio.h>
    #include <stdbool.h>
    #include "i2cAPI.h"
    #include "driverlib/inc/tm4c1294kcpdt.h"
    #include "driverlib/inc/hw_i2c.h"
    #include "driverlib/inc/hw_memmap.h"
    #include "driverlib/inc/hw_types.h"
    #include "driverlib/inc/hw_gpio.h"
    #include "driverlib/i2c.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/rom_map.h"
    #include "utils/uartstdio.h"
    
    uint32_t i2c_init(uint32_t g_ui32SysClock)
    {
    	//This function is for eewiki and is to be updated to handle any port
        //  Enable peripherals in use. Also reset I2C2 at the end to allow calling
            //  this function at any point in order to reset I2C interface.
            MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
    
            MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C8);
    
    
            // Enable I2C communication interface, SCL, SDA lines
            MAP_GPIOPinConfigure(GPIO_PD2_I2C8SCL);
            MAP_GPIOPinConfigure(GPIO_PD3_I2C8SDA);
    
            MAP_GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_2);
            MAP_GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_3);
    
            //  Enable I2C master interface
            MAP_I2CMasterEnable(I2C8_BASE);
    
            // Run I2C bus in high-speed mode, 400kHz speed
            MAP_I2CMasterInitExpClk(I2C8_BASE, g_ui32SysClock, true);
    
    
    
    
    	/*//enable GPIO peripheral that contains I2C
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
    
    	while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOD))
        {
            UARTprintf("I2c master busy Init\r\n");
            break;
        }
    
    	// Configure the pin muxing for I2C0 functions on port B2 and B3.
    	GPIOPinConfigure(GPIO_PD2_I2C8SCL);
    	GPIOPinConfigure(GPIO_PD3_I2C8SDA);
    
    	// Select the I2C function for these pins.
    	GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_2);
    	GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_3);
    	//I2CMasterEnable( I2C8_BASE );
    	// Enable and initialize the I2C0 master module.  Use the system clock for
    	// the I2C0 module.  The last parameter sets the I2C data transfer rate.
    	// If false the data rate is set to 100kbps and if true the data rate will
    	// be set to 400kbps.
    	//I2CMasterInitExpClk(I2C8_BASE, SysCtlClockGet(), false);
    	SysCtlPeripheralDisable(SYSCTL_PERIPH_I2C8);
    	SysCtlPeripheralReset(SYSCTL_PERIPH_I2C8);
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C8);
    
    	while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOD))
        {
            UARTprintf("I2c master busy Init_1\r\n");
            break;
        }
    
    	I2CMasterInitExpClk(I2C8_BASE, g_ui32SysClock, true);
    */
    
    	//clear I2C FIFOs
    	/*HWREG(I2C8_BASE + I2C_O_FIFOCTL) = 80008000;*/
    }
    
    void i2c_read_byte(uint16_t device_address, uint16_t device_register, uint8_t *pui32DataRx)
    {
        i2c_read_multi(device_address,device_register,pui32DataRx,1);
    }
    
    void i2c_write_byte(uint16_t device_address, uint16_t device_register, uint8_t pui32DataTx)
    {
        uint8_t ui8DataTx = pui32DataTx;
        i2c_write_multi(device_address,device_register,&ui8DataTx,1);
    }
    
    void i2c_read_multi(uint16_t device_address, uint16_t device_register, uint8_t *pui32DataRx,uint8_t nNumbytes)
    {
        uint32_t I2cbaseregAddr = I2C0_BASE;
    	//specify that we want to communicate to device address with an intended write to bus
    	I2CMasterSlaveAddrSet(I2cbaseregAddr, device_address, false);
    
    	//the register to be read
    	I2CMasterDataPut(I2cbaseregAddr, device_register);
    
    	//send control byte and register address byte to slave device
    	I2CMasterControl(I2cbaseregAddr, I2C_MASTER_CMD_SINGLE_SEND);
    
    	//wait for MCU to complete send transaction
    	while(I2CMasterBusy(I2cbaseregAddr))
        {
    	    UARTprintf("I2c master busy\r\n");
        }
    
    	//read from the specified slave device
    	I2CMasterSlaveAddrSet(I2cbaseregAddr, device_address, true);
    
    	//send control byte and read from the register from the MCU
    	I2CMasterControl(I2cbaseregAddr, I2C_MASTER_CMD_SINGLE_RECEIVE);
    
    	//wait while checking for MCU to complete the transaction
    	while(I2CMasterBusy(I2cbaseregAddr))
    	{
    	    UARTprintf("I2c master busy\r\n");
    	}
    
    
        // Dummy acknowledge and wait for the receive request from the master.
        // This is done to clear any flags that should not be set.
        //
        while(!(I2CSlaveStatus(I2cbaseregAddr) & I2C_SLAVE_ACT_TREQ))
        {
        }
    
    	if(nNumbytes == 1)
    	{
    	    pui32DataRx[nNumbytes] = I2CMasterDataGet(I2cbaseregAddr);
    	}
    	else if(nNumbytes > 1)
    	{
    	    for(ui32Index = 0; ui32Index < nNumbytes; ui32Index++)
            {
                //
                // Read the data from the master.
                //
                pui32DataRx[ui32Index] = I2CMasterDataGet(I2cbaseregAddr);
    
                //
                // Display the data that the slave has received.
                //
                //UARTprintf("Received: '%c'\n", pui32DataRx[ui32Index]);
            }
    
    	}
    }
    
    void i2c_write_multi(uint16_t device_address, uint16_t device_register, uint8_t* pui32DataTx,uint8_t nNumbytes)  //uint32_t pui32DataTx[NUM_I2C_DATA];
    {
        uint32_t I2cbaseregAddr = I2C0_BASE;
    	//specify that we want to communicate to device address with an intended write to bus
    	I2CMasterSlaveAddrSet(I2cbaseregAddr, device_address, false);
    
    	//register to be read
    	I2CMasterDataPut(I2cbaseregAddr, device_register);
    
    	//send control byte and register address byte to slave device
    	I2CMasterControl(I2cbaseregAddr, I2C_MASTER_CMD_BURST_SEND_START);
    
    	//wait for MCU to finish transaction
    	while(I2CMasterBusy(I2cbaseregAddr));
    
    	I2CMasterSlaveAddrSet(I2cbaseregAddr, device_address, true);
    
    	//specify data to be written to the above mentioned device_register
    	while(nNumbytes--)
    	{
            //
            // Place the data to be sent in the data register
            //
    	    I2CMasterDataPut(I2cbaseregAddr, pui32DataTx);
    	    UARTprintf("  Sending: '%c'  . . .  ", pui32DataTx);
            //
            // Initiate send of data from the master.  Since the loopback
            // mode is enabled, the master and slave units are connected
            // allowing us to receive the same data that we sent out.
            //
    	    I2CMasterControl(I2cbaseregAddr, I2C_MASTER_CMD_SINGLE_SEND);
    
    	    //
    	    // Wait until the slave has received and acknowledged the data.
    	    //
    	    while(!(I2CSlaveStatus(I2cbaseregAddr) & I2C_SLAVE_ACT_RREQ))
            {
    	       UARTprintf("I2c NACK\r\n");
            }
    
    	    pui32DataTx++;
    	}
    	//wait while checking for MCU to complete the transaction
    	I2CMasterControl(I2cbaseregAddr, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
    
    	//wait for MCU & device to complete transaction
    	while(I2CMasterBusy(I2cbaseregAddr));
    	{
    	    UARTprintf("I2c master busy\r\n");
    	}
    
    }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    几个问题:

     -在第52-71行之间,你初始化 I2C8。 但在76-108之间、您可以再次初始化 I2C8。 为什么要这样做?  

     -在你的128和188行,你硬编码 I2C0。 我想在 i2c_init()中启动 I2C8时使用 I2C8。 如果要使用 I2C0、I2C0的初始化在哪里? 这就是它不起作用的原因。  

     -确保您电路板上的 SDA 和 SDL 具有正确的上拉电阻,用于您要使用的 I2C 总线(例如 I2C8SDA 和 I2C8SCL)。  

     BTW、如果您对 I2C 有新问题、则应打开新主题进行讨论。 您不仅仅拒绝了我两周前关于以太网的回答。