工具与软件:
您好!
Im 尝试通过 SPI 刷写微控制器(从连接的外部存储器)。
使用提供的应用手册:
适用于 Hercules TMS570LS31X MCU 的 SPI 引导加载程序(TI.com)
我演示了此函数、通过外部存储器中的数据存储器进行刷写、而不是通过 SPI 接收的数据包。
但是我有一个问题的功能 Fapi_Block。
该程序在这条线被卡住了
"while (FAPI_GET_FSM_STATUS!= Fapi_Status_Success);"
如果您愿意、我可以提供所有代码。
bl_spi.c
//*****************************************************************************
//
// bl_spi.c - Functions used to transfer data via the SPI port.
// Author : QJ Wang. qjwang@ti.com
// Date : 9-19-2012
//
// Copyright (c) 2006-2011 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
//*****************************************************************************
#include "bl_config.h"
#include "bl_commands.h"
#include "bl_spi_packet.h"
#include "bl_spi.h"
#include "Registers_FMC_LE.h"
#include "system.h"
#include "bl_flash.h"
#include "hw_spi.h"
#include "sci_common.h"
#include "bl_led_demo.h"
uint8_t g_ucStatus;
extern uint32_t transferAddress;
extern uint32_t transferSize;
extern uint32_t g_ulUpdateStatusAddr;
extern uint32_t g_ulUpdateBufferSize; //32 bytes or 8 32-bit words
extern uint32_t g_pulUpdateSuccess[8];
#include "fram.h"
#include "general_def.h"
#define PAGE_LENGTH 16
void readPageFromExtMem(uint8_t FRAM, uint32_t packetNr, uint32_t dataDir, uint8_t *returnDir);
uint16_t rExtMem(uint32_t address, uint8_t cs, bool delay);
void cast8to32(uint8_t *dataIn, uint32_t *dataOut){
uint8_t littleEndian = 0;
if (littleEndian)
*dataOut = ((uint32_t)dataIn[3] << 24) | ((uint32_t)dataIn[2] << 16) | ((uint32_t)dataIn[1] << 8) | ((uint32_t)dataIn[0]);
else
*dataOut = ((uint32_t)dataIn[0] << 24) | ((uint32_t)dataIn[1] << 16) | ((uint32_t)dataIn[2] << 8) | ((uint32_t)dataIn[3]);
}
#define UPD_STATUS_BANK 0
#define UPD_BANK 1
enum STATUS {
Success = 1,
Fail = 0
};
void UpdaterSPI(spiBASE_t *node) {
uint32_t dataDir = APP_BANK_B;
uint32_t dataInMem_32[PAGE_LENGTH*2];
uint8_t dataInMem_8[PAGE_LENGTH*8];
uint16_t NrPages, statusOk;
uint32_t FLASH_FIRST_SECTOR_SIZE;
uint8_t i;
uint8_t ulSize = PAGE_LENGTH*2;
transferAddress = APP_START_ADDRESS;
uExtMem(FRAM1);
NrPages = rExtMem(APP_BANK_B_LEN, FRAM1, true);
sExtMem(FRAM1);
transferSize = ulSize*NrPages;
FLASH_FIRST_SECTOR_SIZE = BLInternalFlashFirstSectorSizeGet();
if(transferSize > FLASH_FIRST_SECTOR_SIZE) {
sciSend(scilinREG, 22, "\n\rProgram Flash failed");
sciSend(scilinREG, 18, "\n\r\tFile to large\n\r");
return;
}
sciSend(scilinREG, 17, "\n\rNr of pages: 0x");
sciDisplayData(scilinREG, (uint8 *) &NrPages, 2);
sciSend(scilinREG, 2, "\n\r");
while(transferSize) {
sciSend(scilinREG, 18, "\n\rPackets left: 0x");
sciDisplayData(scilinREG, (uint8 *) &transferSize, 4);
readPageFromExtMem(FRAM1, PAGE_LENGTH, dataDir, dataInMem_8);
for(i = 0; i < PAGE_LENGTH*2; i++){
cast8to32(dataInMem_8+(i*4), dataInMem_32+i);
}
statusOk = !Fapi_BlockProgram(UPD_BANK, transferAddress, (uint32_t)dataInMem_32, ulSize);
//the program does not move beyond this point
if (!statusOk) {
sciSend(scilinREG, 22, "\n\rProgram Flash failed");
return;
}
dataDir += ulSize*4;
transferAddress += ulSize;
transferSize -= ulSize;
}
sciSend(scilinREG, 36, "\n\r\n\rApplication load was successful!");
statusOk = !Fapi_UpdateStatusProgram(UPD_STATUS_BANK, g_ulUpdateStatusAddr, (uint32_t)&g_pulUpdateSuccess[0], g_ulUpdateBufferSize);
if (statusOk) {
sciSend(scilinREG, 17, "\n\r\n\rReseting...\n\r");
systemREG1->SYSECR = (0x10) << 14;
// The microcontroller should have reset, so this should never be reached.
while(1){}
}
}
...............