器件型号:LP-AM243x
工具与软件:
您好!
我将按照"CC33XX RTOS MCU 用户指南"中的"入门"指南来设置 AM243x 和 CC33XX。 我已到达第4步、但遇到错误:
D:\ti\cc33xx_mcu_package_R4\tools\programing>python uart_uniflash.py -p COM32 --cfg=only_wifi_fw.cfg Parsing config file ... Parsing config file ... SUCCESS. Found 6 command(s) !!! Executing command 1 of 6 ... Found flash writer ... sending ./sbl_uart_uniflash.release.tiimage Sent flashwriter ./sbl_uart_uniflash.release.tiimage of size 294775 bytes in 27.1s. Executing command 2 of 6 ... Command arguments : --operation=flash-phy-tuning-data Sending flash-phy-tuning-data_command: 0%| | 0/32 [00:00<?, ?bytes/s]send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'2' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'0' send error: expected NAK, CRC, EOT or CAN; got b'1' send error: expected NAK, CRC, EOT or CAN; got b'1' send error: error_count reached 10, aborting. Sending flash-phy-tuning-data_command: 6%|██▌ | 2/32 [00:01<00:59, 2.00s/bytes] [ERROR] XMODEM send failed, no response OR incorrect response from EVM OR cancelled by user, Power cycle EVM and run this script again !!!
-完成了 AM243x MCU+ SDK 的"入门"指南。
-已使用 UniFlash 成功刷写 default_sbl_null.cfg。
-我已经确认 SW4开关位于正确的位置。
-在尝试刷写过程之前、可以在 UART 串行控制台上看到"C"字符。
-我已经 对 EVM 下电上电并运行此脚本 多次、但错误仍然存在。
-我尝试了命令提示符,有和没有管理员权限。
-我已尝试在编程之前断开 BP-33X1连接
环境:
-mcu_plus_sdk_am243x_08_05_00_24、 mcu_plus_sdk_am243x_09_02_00_50
-cc33xx_mcu_package_R4
-CCS 12.7.1.
-SysConfig 1.18.1、1.12.0、1.21.0
-TI_Clang 2.1.0 LTS、1.3.0 LTS
Windows 10
-ASSY:PROC109A (001)
如果您在排除此 XMODEM 发送故障方面有任何帮助、我们将不胜感激!