This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] RM48L540:刷写 RM48L540芯片时出现问题:"CortexR4:不能运行目标 CPU"错误

Guru**** 2526700 points
Other Parts Discussed in Thread: RM48L540

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1435570/rm48l540-issue-flashing-rm48l540-chip-cortexr4-can-t-run-target-cpu-error

器件型号:RM48L540

工具与软件:

您好!

我在尝试在我设计的定制电路板上刷写 RM48L540芯片时遇到问题。 电路板已经过测试、我以前没有遇到任何问题。 但是、我现在收到以下错误:

CortexR4: Can't Run Target CPU: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 9.3.0.00058) CortexR4: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g., lower TCLK). (Emulation package 9.3.0.00058) CortexR4: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g., lower TCLK). (Emulation package 9.3.0.00058)

我唯一能执行的操作就是访问闪存映射、但我无法写入。

是否有人遇到类似的问题、或者您是否可以建议任何其他故障排除步骤? 如果有任何见解、将不胜感激。

谢谢!

Leandro