This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1294NCPDT:TM4C1294NCPDT -以太网引导加载程序

Guru**** 2606725 points
Other Parts Discussed in Thread: TM4C1294NCPDT

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1451957/tm4c1294ncpdt-tm4c1294ncpdt---ethernet-bootloader

器件型号:TM4C1294NCPDT

工具与软件:

AEDHi 团队、

我正在使用 BOOT_EMAC_FLASH 进行固件升级、我目前的要求是在通过 EPI 模块下载到外部 RAM 之前对二进制文件进行解密、

我集成了代码、但是如何以及在何处 在 BL_STARTUP_CCS.s 文件中添加 AES 128位解密和 EPI0模块引脚中断以启用它  

您能否建议如何在 bl_startup_ccs.s 文件中添加这些中断

;;*****************************************************************************
;;
;; This portion of the file goes into interrupt vectors section
;;
;;*****************************************************************************
    .sect ".intvecs"

;;*****************************************************************************
;;
;; The minimal vector table for a Cortex-M3 processor.
;;
;;*****************************************************************************
Vectors:
    .ref    __STACK_TOP
    .word   __STACK_TOP                     ;; Offset 00: Initial stack pointer
    .word   ResetISR - 0x20000000           ;; Offset 04: Reset handler
    .word   NmiSR - 0x20000000              ;; Offset 08: NMI handler
    .word   FaultISR - 0x20000000           ;; Offset 0C: Hard fault handler
    .word   IntDefaultHandler               ;; Offset 10: MPU fault handler
    .word   IntDefaultHandler               ;; Offset 14: Bus fault handler
    .word   IntDefaultHandler               ;; Offset 18: Usage fault handler
    .word   0                               ;; Offset 1C: Reserved
    .word   0                               ;; Offset 20: Reserved
    .word   0                               ;; Offset 24: Reserved
    .word   0                               ;; Offset 28: Reserved
    .word   UpdateHandler - 0x20000000      ;; Offset 2C: SVCall handler
    .word   IntDefaultHandler               ;; Offset 30: Debug monitor handler
    .word   0                               ;; Offset 34: Reserved
    .word   IntDefaultHandler               ;; Offset 38: PendSV handler
 .if $$defined(ENET_ENABLE_UPDATE)
    .ref    SysTickIntHandler
    .word   SysTickIntHandler               ;; Offset 3C: SysTick handler
 .else
    .word   IntDefaultHandler               ;; Offset 3C: SysTick handler
 .endif
 .if $$defined(UART_ENABLE_UPDATE) & $$defined(UART_AUTOBAUD)
    .ref    GPIOIntHandler
    .word   GPIOIntHandler                  ;; Offset 40: GPIO port A handler
 .else
    .word   IntDefaultHandler               ;; Offset 40: GPIO port A handler
 .endif
 .if ($$defined(USB_ENABLE_UPDATE) | (APP_START_ADDRESS != VTABLE_START_ADDRESS))
    .word   IntDefaultHandler               ;; Offset 44: GPIO Port B
    .word   IntDefaultHandler               ;; Offset 48: GPIO Port C
    .word   IntDefaultHandler               ;; Offset 4C: GPIO Port D
    .word   IntDefaultHandler               ;; Offset 50: GPIO Port E
    .word   IntDefaultHandler               ;; Offset 54: UART0 Rx and Tx
    .word   IntDefaultHandler               ;; Offset 58: UART1 Rx and Tx
    .word   IntDefaultHandler               ;; Offset 5C: SSI0 Rx and Tx
    .word   IntDefaultHandler               ;; Offset 60: I2C0 Master and Slave
    .word   IntDefaultHandler               ;; Offset 64: PWM Fault
    .word   IntDefaultHandler               ;; Offset 68: PWM Generator 0
    .word   IntDefaultHandler               ;; Offset 6C: PWM Generator 1
    .word   IntDefaultHandler               ;; Offset 70: PWM Generator 2
    .word   IntDefaultHandler               ;; Offset 74: Quadrature Encoder 0
    .word   IntDefaultHandler               ;; Offset 78: ADC Sequence 0
    .word   IntDefaultHandler               ;; Offset 7C: ADC Sequence 1
    .word   IntDefaultHandler               ;; Offset 80: ADC Sequence 2
    .word   IntDefaultHandler               ;; Offset 84: ADC Sequence 3
    .word   IntDefaultHandler               ;; Offset 88: Watchdog timer
    .word   IntDefaultHandler               ;; Offset 8C: Timer 0 subtimer A
    .word   IntDefaultHandler               ;; Offset 90: Timer 0 subtimer B
    .word   IntDefaultHandler               ;; Offset 94: Timer 1 subtimer A
    .word   IntDefaultHandler               ;; Offset 98: Timer 1 subtimer B
    .word   IntDefaultHandler               ;; Offset 9C: Timer 2 subtimer A
    .word   IntDefaultHandler               ;; Offset A0: Timer 2 subtimer B
    .word   IntDefaultHandler               ;; Offset A4: Analog Comparator 0
    .word   IntDefaultHandler               ;; Offset A8: Analog Comparator 1
    .word   IntDefaultHandler               ;; Offset AC: Analog Comparator 2
    .word   IntDefaultHandler               ;; Offset B0: System Control
    .word   IntDefaultHandler               ;; Offset B4: FLASH Control
 .endif
 .if ($$defined(USB_ENABLE_UPDATE) | (APP_START_ADDRESS != VTABLE_START_ADDRESS))
    .word   IntDefaultHandler               ;; Offset B8: GPIO Port F
    .word   IntDefaultHandler               ;; Offset BC: GPIO Port G
    .word   IntDefaultHandler               ;; Offset C0: GPIO Port H
    .word   IntDefaultHandler               ;; Offset C4: UART2 Rx and Tx
    .word   IntDefaultHandler               ;; Offset C8: SSI1 Rx and Tx
    .word   IntDefaultHandler               ;; Offset CC: Timer 3 subtimer A
    .word   IntDefaultHandler               ;; Offset D0: Timer 3 subtimer B
    .word   IntDefaultHandler               ;; Offset D4: I2C1 Master and Slave
 .if ($$defined(TARGET_IS_TM4C129_RA0) | $$defined(TARGET_IS_TM4C129_RA1) | $$defined(TARGET_IS_TM4C129_RA2))
    .word   IntDefaultHandler               ;; Offset D8: CAN0
    .word   IntDefaultHandler               ;; Offset DC: CAN1
    .word   IntDefaultHandler               ;; Offset E0: Ethernet
    .word   IntDefaultHandler               ;; Offset E4: Hibernation module
 .if $$defined(USB_ENABLE_UPDATE)
    .ref    USB0DeviceIntHandler
    .word   USB0DeviceIntHandler            ;; Offset E8: USB 0 Controller
 .else
    .word   IntDefaultHandler               ;; Offset E8: USB 0 Controller
 .endif
    .word   IntDefaultHandler               ;; Offset EC: PWM Generator 3
    .word   IntDefaultHandler               ;; Offset F0: uDMA 0 Software
 .else
    .word   IntDefaultHandler               ;; Offset D8: Quadrature Encoder 1
    .word   IntDefaultHandler               ;; Offset DC: CAN0
    .word   IntDefaultHandler               ;; Offset E0: CAN1
    .word   IntDefaultHandler               ;; Offset E4: CAN2
    .word   IntDefaultHandler               ;; Offset E8: Ethernet
    .word   IntDefaultHandler               ;; Offset EC: Hibernation module
 .if $$defined(USB_ENABLE_UPDATE)
    .ref    USB0DeviceIntHandler
    .word   USB0DeviceIntHandler            ;; Offset F0: USB 0 Controller
 .else
    .word   IntDefaultHandler               ;; Offset F0: USB 0 Controller
 .endif
 .endif
 .endif

;;*****************************************************************************

请帮助我添加这些中断


另外、我对如何配置这个 EPI0模块及其工作文档集有疑问

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     我目前正在度假一整周。 我会在今天稍后时间答复你的质询。 请预计会延迟响应。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [报价 userid="524025" url="~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1451957/tm4c1294ncpdt-tm4c1294ncpdt---ethernet-bootloader "]

    我集成了代码、但是如何以及在何处 在 BL_STARTUP_CCS.s 文件中添加 AES 128位解密和 EPI0模块引脚中断以启用它  

    您能否建议如何在 bl_startup_ccs.s 文件中添加这些中断

    [报价]

    您好!

     请记住、TM4C1294NCPDT 没有 AES 功能。  请参阅 TM4C 产品选型指南 以了解支持 AES 的器件型号。 请参见下文。  

    假设您使用的器件型号支持 AES。 在这种情况下、AES 中断将映射到矢量编号111。 请参见下文。