This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV320AIC3104:使用 tinyplay 播放 WAV 文件时没有声音。

Guru**** 2587345 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1510435/tlv320aic3104-there-is-no-sound-when-using-tinyplay-to-play-a-wav-file

器件型号:TLV320AIC3104

工具/软件:

尊敬的 TI 团队:

使用 tinyplay 播放 WAV 文件时没有声音。

编解码器 DIN 上有一个数据信号。 MCLK 的频率为11.36 MHz、BCLK 的频率为14.14 MHz。

i2cdump 信息如下所示:

tinymix 配置:

Number of controls: 114
ctl	type	num	name                                    	device	value
0	INT	1	Left Line Mixer Line2R Bypass Volume    	0118 (range 0->118)
1	INT	1	Right Line Mixer Line2L Bypass Volume   	0111 (range 0->118)
2	INT	1	Left HP Mixer Line2R Bypass Volume      	0118 (range 0->118)
3	INT	1	Right HP Mixer Line2L Bypass Volume     	0111 (range 0->118)
4	INT	1	Left HPCOM Mixer Line2R Bypass Volume   	0118 (range 0->118)
5	INT	1	Right HPCOM Mixer Line2L Bypass Volume  	0111 (range 0->118)
6	INT	2	Line Line2 Bypass Volume                	0111, 71 (range 0->118)
7	INT	2	HP Line2 Bypass Volume                  	0111, 71 (range 0->118)
8	INT	2	HPCOM Line2 Bypass Volume               	0111, 71 (range 0->118)
9	INT	2	Mono Line2 Bypass Volume                	0111, 71 (range 0->118)
10	INT	2	Mono PGA Bypass Volume                  	071, 71 (range 0->118)
11	INT	2	Mono DAC Playback Volume                	071, 71 (range 0->118)
12	BOOL	1	Mono Playback Switch                    	0Off
13	INT	1	Mono Playback Volume                    	08 (range 0->9)
14	INT	2	PCM Playback Volume                     	0118, 118 (range 0->127)
15	INT	1	Left Line Mixer PGAR Bypass Volume      	0118 (range 0->118)
16	INT	1	Left Line Mixer DACR1 Playback Volume   	0118 (range 0->118)
17	INT	1	Right Line Mixer PGAL Bypass Volume     	0111 (range 0->118)
18	INT	1	Right Line Mixer DACL1 Playback Volume  	0111 (range 0->118)
19	INT	1	Left HP Mixer PGAR Bypass Volume        	0118 (range 0->118)
20	INT	1	Left HP Mixer DACR1 Playback Volume     	0118 (range 0->118)
21	INT	1	Right HP Mixer PGAL Bypass Volume       	0118 (range 0->118)
22	INT	1	Right HP Mixer DACL1 Playback Volume    	0118 (range 0->118)
23	INT	1	Left HPCOM Mixer PGAR Bypass Volume     	0118 (range 0->118)
24	INT	1	Left HPCOM Mixer DACR1 Playback Volume  	0118 (range 0->118)
25	INT	1	Right HPCOM Mixer PGAL Bypass Volume    	0118 (range 0->118)
26	INT	1	Right HPCOM Mixer DACL1 Playback Volume 	0118 (range 0->118)
27	INT	2	Line PGA Bypass Volume                  	0111, 71 (range 0->118)
28	INT	2	Line DAC Playback Volume                	0111, 71 (range 0->118)
29	INT	2	HP PGA Bypass Volume                    	0111, 71 (range 0->118)
30	INT	2	HP DAC Playback Volume                  	0111, 71 (range 0->118)
31	INT	2	HPCOM PGA Bypass Volume                 	071, 71 (range 0->118)
32	INT	2	HPCOM DAC Playback Volume               	071, 71 (range 0->118)
33	INT	2	Line Playback Volume                    	08, 8 (range 0->9)
34	BOOL	2	Line Playback Switch                    	0Off, Off
35	INT	2	HP Playback Volume                      	08, 8 (range 0->9)
36	BOOL	2	HP Playback Switch                      	0Off, Off
37	INT	2	HPCOM Playback Volume                   	08, 8 (range 0->9)
38	BOOL	2	HPCOM Playback Switch                   	0Off, Off
39	BOOL	2	AGC Switch                              	0Off, Off
40	ENUM	1	Left AGC Target level                   	0> -5.5dB, -8dB, -10dB, -12dB, -14dB, -17dB, -20dB, -24dB, 
41	ENUM	1	Right AGC Target level                  	0> -5.5dB, -8dB, -10dB, -12dB, -14dB, -17dB, -20dB, -24dB, 
42	ENUM	1	Left AGC Attack time                    	0> 8ms, 11ms, 16ms, 20ms, 
43	ENUM	1	Right AGC Attack time                   	0> 8ms, 11ms, 16ms, 20ms, 
44	ENUM	1	Left AGC Decay time                     	0> 100ms, 200ms, 400ms, 500ms, 
45	ENUM	1	Right AGC Decay time                    	0> 100ms, 200ms, 400ms, 500ms, 
46	BOOL	2	De-emphasis Switch                      	0On, On
47	INT	2	PGA Capture Volume                      	032, 32 (range 0->119)
48	BOOL	2	PGA Capture Switch                      	0On, On
49	ENUM	2	ADC HPF Cut-off                         	0Disabled, 0.0045xFs, > 0.0125xFs, 0.025xFs, , Disabled, 0.0045xFs, > 0.0125xFs, 0.025xFs, 
50	ENUM	1	Output Driver Power-On time             	0> 0us, 10us, 100us, 1ms, 10ms, 50ms, 100ms, 200ms, 400ms, 800ms, 2s, 4s, 
51	ENUM	1	Output Driver Ramp-up step              	0> 0ms, 1ms, 2ms, 4ms, 
52	ENUM	1	Left DAC Mux                            	0> DAC_L1, DAC_L3, DAC_L2, 
53	ENUM	1	Left HPCOM Mux                          	0> differential of HPLOUT, constant VCM, single-ended, 
54	ENUM	1	Right DAC Mux                           	0> DAC_R1, DAC_R3, DAC_R2, 
55	ENUM	1	Right HPCOM Mux                         	0> differential of HPROUT, constant VCM, single-ended, differential of HPLCOM, external feedback, 
56	ENUM	1	Left Line1L Mux                         	0single-ended, > differential, 
57	ENUM	1	Left Line1R Mux                         	0> single-ended, differential, 
58	ENUM	1	Right Line1L Mux                        	0> single-ended, differential, 
59	ENUM	1	Right Line1R Mux                        	0single-ended, > differential, 
60	BOOL	1	Left PGA Mixer Line1L Switch            	0On
61	BOOL	1	Left PGA Mixer Line1R Switch            	0Off
62	BOOL	1	Left PGA Mixer Line2L Switch            	0On
63	BOOL	1	Left PGA Mixer Mic3L Switch             	0Off
64	BOOL	1	Left PGA Mixer Mic3R Switch             	0Off
65	ENUM	1	Left Line2L Mux                         	0single-ended, > differential, 
66	BOOL	1	Right PGA Mixer Line1R Switch           	0On
67	BOOL	1	Right PGA Mixer Line1L Switch           	0Off
68	BOOL	1	Right PGA Mixer Line2R Switch           	0On
69	BOOL	1	Right PGA Mixer Mic3L Switch            	0Off
70	BOOL	1	Right PGA Mixer Mic3R Switch            	0Off
71	ENUM	1	Right Line2R Mux                        	0single-ended, > differential, 
72	BOOL	1	Left Line Mixer PGAL Bypass Switch      	0On
73	BOOL	1	Left Line Mixer DACL1 Switch            	0On
74	BOOL	1	Left Line Mixer PGAR Bypass Switch      	0Off
75	BOOL	1	Left Line Mixer DACR1 Switch            	0Off
76	BOOL	1	Left Line Mixer Line2L Bypass Switch    	0On
77	BOOL	1	Left Line Mixer Line2R Bypass Switch    	0Off
78	BOOL	1	Right Line Mixer PGAL Bypass Switch     	0On
79	BOOL	1	Right Line Mixer DACL1 Switch           	0On
80	BOOL	1	Right Line Mixer PGAR Bypass Switch     	0Off
81	BOOL	1	Right Line Mixer DACR1 Switch           	0On
82	BOOL	1	Right Line Mixer Line2L Bypass Switch   	0On
83	BOOL	1	Right Line Mixer Line2R Bypass Switch   	0Off
84	BOOL	1	Left HP Mixer PGAL Bypass Switch        	0On
85	BOOL	1	Left HP Mixer DACL1 Switch              	0On
86	BOOL	1	Left HP Mixer PGAR Bypass Switch        	0Off
87	BOOL	1	Left HP Mixer DACR1 Switch              	0Off
88	BOOL	1	Left HP Mixer Line2L Bypass Switch      	0On
89	BOOL	1	Left HP Mixer Line2R Bypass Switch      	0Off
90	BOOL	1	Right HP Mixer PGAL Bypass Switch       	0Off
91	BOOL	1	Right HP Mixer DACL1 Switch             	0Off
92	BOOL	1	Right HP Mixer PGAR Bypass Switch       	0Off
93	BOOL	1	Right HP Mixer DACR1 Switch             	0On
94	BOOL	1	Right HP Mixer Line2L Bypass Switch     	0On
95	BOOL	1	Right HP Mixer Line2R Bypass Switch     	0Off
96	BOOL	1	Left HPCOM Mixer PGAL Bypass Switch     	0Off
97	BOOL	1	Left HPCOM Mixer DACL1 Switch           	0On
98	BOOL	1	Left HPCOM Mixer PGAR Bypass Switch     	0Off
99	BOOL	1	Left HPCOM Mixer DACR1 Switch           	0Off
100	BOOL	1	Left HPCOM Mixer Line2L Bypass Switch   	0On
101	BOOL	1	Left HPCOM Mixer Line2R Bypass Switch   	0Off
102	BOOL	1	Right HPCOM Mixer PGAL Bypass Switch    	0Off
103	BOOL	1	Right HPCOM Mixer DACL1 Switch          	0Off
104	BOOL	1	Right HPCOM Mixer PGAR Bypass Switch    	0Off
105	BOOL	1	Right HPCOM Mixer DACR1 Switch          	0On
106	BOOL	1	Right HPCOM Mixer Line2L Bypass Switch  	0On
107	BOOL	1	Right HPCOM Mixer Line2R Bypass Switch  	0Off
108	BOOL	1	Mono Mixer Line2L Bypass Switch         	0On
109	BOOL	1	Mono Mixer PGAL Bypass Switch           	0Off
110	BOOL	1	Mono Mixer DACL1 Switch                 	0On
111	BOOL	1	Mono Mixer Line2R Bypass Switch         	0Off
112	BOOL	1	Mono Mixer PGAR Bypass Switch           	0Off
113	BOOL	1	Mono Mixer DACR1 Switch                 	0On

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    您的预期采样率是多少? 是否也为器件提供了 FSYNC?

    谢谢、
    Jeff McPherson

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    采样率为44.1kHz。  主器件的 FSYNC 连接到编解码器

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    声音需要输出到 LEFT_LOP/M 如何配置 reg 或 kcontrol?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    我建议在这里使用 AIC310x EVM GUI 来配置 I2C 脚本、但我在这里得到了默认的输出脚本、并添加了注释以说明 DAC 和线路输出的配置方式。 但是、需要注意的一点是、BCLK/MCLK 似乎不是44.1k 的倍数、因此 DAC 无法按预期工作。 根据数据表中的时钟树、CODEC_CLK 需要为256*fs、对于44.1k 作为 FS (ref)、需要为11.29MHz。 CODEC_CLK 可以通过 CLKDIV_IN 进行设置、因此只需确保 MCLK 或 BCLK 为11.2896MHz、然后在寄存器0x66中将该时钟设置为 CLKDIV_IN。 如果您只是尝试以16位进行立体声 I2S、则 BCLK 不必如此高、例如、BCLK 至少需要为44.1kHz * 16 * 2 = 1.4112MHz。 但是、一般经验法则是、BCLK 应始终是 WCLK/采样速率的整数倍、理想情况下为2*16、20、24或32的因子、因为这些是标准音频位深度。  

    # example script from the GUI
    # stereo line out playback
    w 30 07 8A #44.1k, left dac plays left channel, right dac plays right channel
    w 30 66 A0 #clkdiv_in uses bclk, pllclk_in uses bclk -> PLL is disabled by default so this is fine
    w 30 25 C0 #l+r dac powered up
    w 30 29 02 #volume control is same between left and right
    w 30 2B 00 #left dac not muted, gain =0db
    w 30 52 80 #dac_l1 routed to left_lop/m, gain=0db
    w 30 5C 80 #dac_r1 routed to right_lop/m, gain=0db
    w 30 56 09 #output level=0db gain, left_lop/m is NOT muted, left_lop/m fully powered up
    w 30 5D 09 #same for right line out
    

    如果您对时钟或配置有更多问题、敬请告知。

    此致、
    Mir