请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:PGA2311 大家好,我正在尝试使用PGA2311 ,但我的系统从单个(USB接口) 5VDC电源获得电源,
但在VOUTR中,无论VINR中是否存在信号,我都获得了稳定的600mV直流...
有什么想法吗? 我必须使用双电源并将VA-连接至-5VDC?? 即使我的信号是p-p 300mV且电压为2.5VDC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.