This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV320AIC3204:无音频输出

Guru**** 2914610 points

Other Parts Discussed in Thread: TLV320AIC3204

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/612783/tlv320aic3204-no-audio-output

部件号:TLV320AIC3204

我正在尝试将TLV320AIC3204用作I2S主控制器,MCLK=12MHz。  

我似乎有数据来自编解码器,我正在发送数据,但在耳机或线路输出上没有听到任何提示音。  

所附为I2S总线的波形,此处为寄存器设置。 有人知道我错过了什么吗?

顺便说一下,数据表和应用程序注释对于此零件来说是坏的,其中也没有提到寄存器11和12与13和14之间的差异,这让我花了一段时间才明白。  

lv320aic3204.cpp 65:第0页:
tlv320aic3204.cpp 69:1 (0x01)=0 (0x00)
tlv320aic3204.cpp 69:2 (0x02)=96 (0x60)
tlv320aic3204.cpp 69:3 (0x03)=0 (0x00)
tlv320aic3204.cpp 69:4 (0x04)=3 (0x03)
tlv320aic3204.cpp 69:5 (0x05)=145 (0x91)
tlv320aic3204.cpp 69:6 (0x06)=8 (0x08)
tlv320aic3204.cpp 69:7 (0x07)= 7 (0x07)
tlv320aic3204.cpp 69:8 (0x08)= 128 (0x80)
tlv320aic3204.cpp 69:9 (0x09)=0 (0x00)
tlv320aic3204.cpp 69:10 (0x0A)=0 (0x00)
tlv320aic3204.cpp 69:11 (0x0B)=136 (0x88)
tlv320aic3204.cpp 69:12(0x0C)=130(0x82)
tlv320aic3204.cpp 69:13(0x0D)=3(0x03)
tlv320aic3204.cpp 69:14 (0x0E)=0 (0x00)
tlv320aic3204.cpp 69:15 (0x0F)=2 (0x02)
tlv320aic3204.cpp 69:16 (0x10)=0 (0x00)
tlv320aic3204.cpp 69:17 (0x11)=8 (0x08)
tlv320aic3204.cpp 69:18(0x12)=136(0x88)
tlv320aic3204.cpp 69:19 (0x13)= 140 (0x8C)
tlv320aic3204.cpp 69:20 (0x14)=128 (0x80)
tlv320aic3204.cpp 69:21 (0x15)= 1 (0x01)
tlv320aic3204.cpp 69:22(0x16)=0(0x00)
tlv320aic3204.cpp 69:23(0x17)=4(0x04)
tlv320aic3204.cpp 69:24 (0x18)= 0 (0x00)
tlv320aic3204.cpp 69:25 (0x19)=0 (0x00)
tlv320aic3204.cpp 69:26 (0x1A)= 1 (0x01)
tlv320aic3204.cpp 69:27 (0x1B)= 12 (0x0C)
tlv320aic3204.cpp 69:28 (0x1C)=0 (0x00)
tlv320aic3204.cpp 69:29(0x1D)=0(0x00)
tlv320aic3204.cpp 69:30(0x1E)=176(0xB0)
tlv320aic3204.cpp 69:31 (0x1F)=0 (0x00)
tlv320aic3204.cpp 69:32(0x20)=0(0x00)
tlv320aic3204.cpp 69:33 (0x21)= 0 (0x00)
tlv320aic3204.cpp 69:34(0x22)=0(0x00)
tlv320aic3204.cpp 69:35 (0x23)= 0 (0x00)
tlv320aic3204.cpp 69:36(0x24)=204(0xCC)
tlv320aic3204.cpp 69:37 (0x25)=238 (0xEE)
tlv320aic3204.cpp 69:38 (0x26)= 17 (0x11)
tlv320aic3204.cpp 69:39 (0x27)= 0 (0x00)
tlv320aic3204.cpp 69:40 (0x28)= 0 (0x00)
tlv320aic3204.cpp 69:41 (0x29)= 0 (0x00)
tlv320aic3204.cpp 69:42 (0x2A)= 0 (0x00)
tlv320aic3204.cpp 69:43 (0x2B)= 0 (0x00)
tlv320aic3204.cpp 69:44 (0x2C)=192 (0xC0)
tlv320aic3204.cpp 69:45 (0x2D)=0 (0x00)
tlv320aic3204.cpp 69:46 (0x2E)= 0 (0x00)
tlv320aic3204.cpp 69:47 (0x2F)=0 (0x00)
tlv320aic3204.cpp 69:48 (0x30)= 0 (0x00)
tlv320aic3204.cpp 69:49 (0x31)= 0 (0x00)
tlv320aic3204.cpp 69:50 (0x32)=0 (0x00)
tlv320aic3204.cpp 69:51(0x33)=0(0x00)
tlv320aic3204.cpp 69:52 (0x34)= 0 (0x00)
tlv320aic3204.cpp 69:53 (0x35)= 18 (0x12)
tlv320aic3204.cpp 69:54 (0x36)=2 (0x02)
tlv320aic3204.cpp 69:55 (0x37)=2 (0x02)
tlv320aic3204.cpp 69:56(0x38)=2(0x02)
tlv320aic3204.cpp 69:57 (0x39)= 0 (0x00)
tlv320aic3204.cpp 69:58 (0x3A)= 0 (0x00)
tlv320aic3204.cpp 69:59 (0x3B)= 0 (0x00)
tlv320aic3204.cpp 69:60 (0x3C)= 1 (0x01)
tlv320aic3204.cpp 69:61 (0x3D)= 7 (0x07)
tlv320aic3204.cpp 69:62 (0x3E)= 0 (0x00)
tlv320aic3204.cpp 69:63(0x3F)=212(0xD4)
tlv320aic3204.cpp 69:64(0x40)=2(0x02)
tlv320aic3204.cpp 69:65 (0x41)= 0 (0x00)
tlv320aic3204.cpp 69:66 (0x42)= 0 (0x00)
tlv320aic3204.cpp 69:67 (0x43)= 0 (0x00)
tlv320aic3204.cpp 69:68 (0x44)=111 (0x6f)
tlv320aic3204.cpp 69:69(0x45)=56(0x38)
tlv320aic3204.cpp 69:70 (0x46)= 0 (0x00)
tlv320aic3204.cpp 69:71(0x47)=0(0x00)
tlv320aic3204.cpp 69:72(0x48)=0(0x00)
tlv320aic3204.cpp 69:73 (0x49)= 0 (0x00)
tlv320aic3204.cpp 69:74 (0x4A)= 0 (0x00)
tlv320aic3204.cpp 69:75 (0x4B)=238 (0xEE)
tlv320aic3204.cpp 69:76(0x4C)=16(0x10)
tlv320aic3204.cpp 69:77 (0x4D)=216 (0xD8)
tlv320aic3204.cpp 69:78 (0x4E)=126 (0x7E)
tlv320aic3204.cpp 69:79 (0x4F)=227 (0xE3)
tlv320aic3204.cpp 69:80 (0x50)=0 (0x00)
tlv320aic3204.cpp 69:81 (0x51)=192 (0xC0)
tlv320aic3204.cpp 69:82(0x52)=0(0x00)
tlv320aic3204.cpp 69:83(0x53)=0(0x00)
tlv320aic3204.cpp 69:84 (0x54)= 0 (0x00)
tlv320aic3204.cpp 69:85(0x55)=0(0x00)
tlv320aic3204.cpp 69:86 (0x56)= 0 (0x00)
tlv320aic3204.cpp 69:87 (0x57)=0 (0x00)
tlv320aic3204.cpp 69:88 (0x58)= 127 (0x7F)
tlv320aic3204.cpp 69:89(0x59)=0(0x00)
tlv320aic3204.cpp 69:90 (0x5A)= 0 (0x00)
tlv320aic3204.cpp 69:91 (0x5B)=0 (0x00)
tlv320aic3204.cpp 69:92 (0x5C)=0 (0x00)
tlv320aic3204.cpp 69:93 (0x5D)= 0 (0x00)
tlv320aic3204.cpp 69:94(0x5E)=0(0x00)
tlv320aic3204.cpp 69:95(0x5F)=0(0x00)
tlv320aic3204.cpp 69:96 (0x60)= 127 (0x7F)
tlv320aic3204.cpp 69:97 (0x61)= 0 (0x00)
tlv320aic3204.cpp 69:98(0x62)=0(0x00)
tlv320aic3204.cpp 69:99 (0x63)= 0 (0x00)
tlv320aic3204.cpp 69:100(0x64)=0(0x00)
tlv320aic3204.cpp 69:101 (0x65)=0 (0x00)
tlv320aic3204.cpp 69:102 (0x66)=0 (0x00)
tlv320aic3204.cpp 69:103 (0x67)= 0 (0x00)
tlv320aic3204.cpp 69:104 (0x68)= 0 (0x00)
tlv320aic3204.cpp 69:105(0x69)=0(0x00)
tlv320aic3204.cpp 69:106 (0x6A)=0 (0x00)
tlv320aic3204.cpp 69:107 (0x6B)= 0 (0x00)
tlv320aic3204.cpp 69:108 (0x6C)=0 (0x00)
tlv320aic3204.cpp 72:第1页:
tlv320aic3204.cpp 22:将页面设置为1
tlv320aic3204.cpp 76:1 (0x01)= 8 (0x08)
tlv320aic3204.cpp 76:2 (0x02)= 1 (0x01)
tlv320aic3204.cpp 76:3 (0x03)=8 (0x08)
tlv320aic3204.cpp 76:4 (0x04)= 8 (0x08)
tlv320aic3204.cpp 76:5 (0x05)=0 (0x00)
tlv320aic3204.cpp 76:6 (0x06)=0 (0x00)
tlv320aic3204.cpp 76:7 (0x07)= 0 (0x00)
tlv320aic3204.cpp 76:8 (0x08)= 0 (0x00)
tlv320aic3204.cpp 76:9 (0x09)= 63 (0x3F)
tlv320aic3204.cpp 76:10 (0x0A)=64 (0x40)
tlv320aic3204.cpp 76:11 (0x0B)=16 (0x10)
tlv320aic3204.cpp 76:12 (0x0C)=8 (0x08)
tlv320aic3204.cpp 76:13 (0x0D)=8 (0x08)
tlv320aic3204.cpp 76:14 (0x0E)=8 (0x08)
tlv320aic3204.cpp 76:15 (0x0F)=8 (0x08)
tlv320aic3204.cpp 76:16 (0x10)= 0 (0x00)
tlv320aic3204.cpp 76:17 (0x11)= 0 (0x00)
tlv320aic3204.cpp 76:18(0x12)=64(0x40)
tlv320aic3204.cpp 76:19 (0x13)= 64 (0x40)
tlv320aic3204.cpp 76:20 (0x14)= 0 (0x00)
tlv320aic3204.cpp 76:21 (0x15)= 0 (0x00)
tlv320aic3204.cpp 76:22(0x16)=0(0x00)
tlv320aic3204.cpp 76:23 (0x17)=0 (0x00)
tlv320aic3204.cpp 76:24 (0x18)= 0 (0x00)
tlv320aic3204.cpp 76:25 (0x19)= 0 (0x00)
tlv320aic3204.cpp 76:26 (0x1A)= 0 (0x00)
tlv320aic3204.cpp 76:27 (0x1B)= 0 (0x00)
tlv320aic3204.cpp 76:28 (0x1C)=0 (0x00)
tlv320aic3204.cpp 76:29(0x1D)=0(0x00)
tlv320aic3204.cpp 76:30(0x1E)=0(0x00)
tlv320aic3204.cpp 76:31 (0x1F)= 0 (0x00)
tlv320aic3204.cpp 76:32 (0x20)= 0 (0x00)
tlv320aic3204.cpp 76:33 (0x21)= 0 (0x00)
tlv320aic3204.cpp 76:34 (0x22)= 0 (0x00)
tlv320aic3204.cpp 76:35 (0x23)= 0 (0x00)
tlv320aic3204.cpp 76:36 (0x24)= 0 (0x00)
tlv320aic3204.cpp 76:37 (0x25)= 0 (0x00)
tlv320aic3204.cpp 76:38 (0x26)= 0 (0x00)
tlv320aic3204.cpp 76:39 (0x27)= 0 (0x00)
tlv320aic3204.cpp 76:40 (0x28)= 0 (0x00)
tlv320aic3204.cpp 76:41 (0x29)= 0 (0x00)
tlv320aic3204.cpp 76:42 (0x2A)= 0 (0x00)
tlv320aic3204.cpp 76:43 (0x2B)= 0 (0x00)
tlv320aic3204.cpp 76:44 (0x2C)= 0 (0x00)
tlv320aic3204.cpp 76:45 (0x2D)= 0 (0x00)
tlv320aic3204.cpp 76:46 (0x2E)= 0 (0x00)
tlv320aic3204.cpp 76:47 (0x2F)= 0 (0x00)
tlv320aic3204.cpp 76:48 (0x30)= 0 (0x00)
tlv320aic3204.cpp 76:49 (0x31)= 0 (0x00)
tlv320aic3204.cpp 76:50 (0x32)= 0 (0x00)
tlv320aic3204.cpp 76:51 (0x33)= 0 (0x00)
tlv320aic3204.cpp 76:52 (0x34)= 128 (0x80)
tlv320aic3204.cpp 76:53 (0x35)= 0 (0x00)
tlv320aic3204.cpp 76:54 (0x36)= 128 (0x80)
tlv320aic3204.cpp 76:55 (0x37)= 128 (0x80)
tlv320aic3204.cpp 76:56 (0x38)= 0 (0x00)
tlv320aic3204.cpp 76:57 (0x39)= 128 (0x80)
tlv320aic3204.cpp 76:58 (0x3A)= 0 (0x00)
tlv320aic3204.cpp 76:59 (0x3B)= 12 (0x0C)
tlv320aic3204.cpp 76:60 (0x3C)= 12 (0x0C)
tlv320aic3204.cpp 76:61 (0x3D)=255 (0xFF)
tlv320aic3204.cpp 76:62(0x3E)=3(0x03)
tlv320aic3204.cpp 76:63 (0x3F)= 192 (0xC0)
tlv320aic3204.cpp 76:64 (0x40)= 0 (0x00)
tlv320aic3204.cpp 76:65 (0x41)= 0 (0x00)
tlv320aic3204.cpp 76:66 (0x42)= 0 (0x00)
tlv320aic3204.cpp 76:67 (0x43)= 0 (0x00)
tlv320aic3204.cpp 76:68 (0x44)= 0 (0x00)
tlv320aic3204.cpp 76:69 (0x45)= 0 (0x00)
tlv320aic3204.cpp 76:70 (0x46)= 0 (0x00)
tlv320aic3204.cpp 76:71(0x47)=50(0x32)
tlv320aic3204.cpp 76:72 (0x48)= 0 (0x00)
tlv320aic3204.cpp 76:73 (0x49)= 0 (0x00)
tlv320aic3204.cpp 76:74 (0x4A)= 0 (0x00)
tlv320aic3204.cpp 76:75 (0x4B)= 0 (0x00)
tlv320aic3204.cpp 76:76 (0x4C)= 0 (0x00)
tlv320aic3204.cpp 76:77 (0x4D)=0 (0x00)
tlv320aic3204.cpp 76:78 (0x4E)= 0 (0x00)
tlv320aic3204.cpp 76:79 (0x4F)= 0 (0x00)
tlv320aic3204.cpp 76:80 (0x50)=0 (0x00)
tlv320aic3204.cpp 76:81 (0x51)= 0 (0x00)
tlv320aic3204.cpp 76:82 (0x52)= 0 (0x00)
tlv320aic3204.cpp 76:83 (0x53)= 0 (0x00)
tlv320aic3204.cpp 76:84 (0x54)= 0 (0x00)
tlv320aic3204.cpp 76:85(0x55)=0(0x00)
tlv320aic3204.cpp 76:86 (0x56)= 0 (0x00)
tlv320aic3204.cpp 76:87 (0x57)= 0 (0x00)
tlv320aic3204.cpp 76:88 (0x58)= 0 (0x00)
tlv320aic3204.cpp 76:89(0x59)=0(0x00)
tlv320aic3204.cpp 76:90 (0x5A)= 0 (0x00)
tlv320aic3204.cpp 76:91 (0x5B)=0 (0x00)
tlv320aic3204.cpp 76:92 (0x5C)=0 (0x00)
tlv320aic3204.cpp 76:93 (0x5D)= 0 (0x00)
tlv320aic3204.cpp 76:94(0x5E)=0(0x00)
tlv320aic3204.cpp 76:95 (0x5F)=0 (0x00)
tlv320aic3204.cpp 76:96 (0x60)= 0 (0x00)
tlv320aic3204.cpp 76:97 (0x61)= 0 (0x00)
tlv320aic3204.cpp 76:98 (0x62)= 0 (0x00)
tlv320aic3204.cpp 76:99 (0x63)= 0 (0x00)
tlv320aic3204.cpp 76:100 (0x64)= 0 (0x00)
tlv320aic3204.cpp 76:101 (0x65)= 0 (0x00)
tlv320aic3204.cpp 76:102 (0x66)= 0 (0x00)
tlv320aic3204.cpp 76:103 (0x67)= 0 (0x00)
tlv320aic3204.cpp 76:104 (0x68)= 0 (0x00)
tlv320aic3204.cpp 76:105 (0x69)= 0 (0x00)
tlv320aic3204.cpp 76:106 (0x6A)=0 (0x00)
tlv320aic3204.cpp 76:107 (0x6B)= 0 (0x00)
tlv320aic3204.cpp 76:108 (0x6C)=0 (0x00)
tlv320aic3204.cpp 76:109 (0x6D)= 0 (0x00)
tlv320aic3204.cpp 76:110 (0x6E)= 0 (0x00)
tlv320aic3204.cpp 76:111 (0x6f)=0 (0x00)
tlv320aic3204.cpp 76:112 (0x70)= 0 (0x00)
tlv320aic3204.cpp 76:113 (0x71)= 0 (0x00)
tlv320aic3204.cpp 76:114 (0x72)= 0 (0x00)
tlv320aic3204.cpp 76:115 (0x73)= 0 (0x00)
tlv320aic3204.cpp 76:116 (0x74)= 0 (0x00)
tlv320aic3204.cpp 76:117 (0x75)= 0 (0x00)
tlv320aic3204.cpp 76:118 (0x76)= 0 (0x00)
tlv320aic3204.cpp 76:119 (0x77)= 0 (0x00)
tlv320aic3204.cpp 76:120 (0x78)= 0 (0x00)
tlv320aic3204.cpp 76:121 (0x79)= 0 (0x00)
tlv320aic3204.cpp 76:122 (0x7A)= 0 (0x00)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Trampas,

    总的来说,根据您共享的设置,设备的播放配置是正确的。 能否检查设备输出时您得到的是什么?您应该会得到共模电压。 另外,您是否尝试过使用环回将ADC输出直接路由到DAC输入以放弃n ü I²S输入数据的任何问题?这是通过将'1'写入寄存器29第0页的位D4来实现的。 另一个尝试是将NDAC,MDAC和DOSR分频器配置为与ADC分频器(AOSR,NADC和mAdc)具有相同的值。

    此致,

     -Diego Mel é ndez López ñ a
      音频应用工程师